imx8dx usb2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8dx usb2

2,731件の閲覧回数
songhongliang
Contributor II

HI 

I want to use the second usb of imx8dx, but I don't know how to configure it. Is there a patch or help me complete the function together.

thanks!

0 件の賞賛
返信
5 返答(返信)

2,716件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

imx8dx use usbotg3 for usb2, try to change the source code about usbotg3 in the In fsl-imx8dxp.dtsi and fsl-imx8dxp.dtsi, you need to change according to your HW, I don't have such example for you

 

 

 

0 件の賞賛
返信

2,714件の閲覧回数
songhongliang
Contributor II

hi 

The usb2 of imx8dx is usb2.0, the hardware is the same as the official reference schematic diagram, as shown in the picture, there are not too many other components.

thanks

0 件の賞賛
返信

2,704件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

sorry I missed this picture before, for usb_otg2, I got information:

"imx8dx has two USB ports (one for chipidea, one for cdns3), and both are enabled, see arch/arm64/boot/dts/freescale/imx8x-mek.dtsi detail please."

0 件の賞賛
返信

2,698件の閲覧回数
songhongliang
Contributor II

HI

Is it possible to use cdns3 for USB2.0? The second USB2.0 port of imx8dx, according to the device tree configuration of cdns3, the second USB cannot be used. My USB only has DP DN. There are no other auxiliary devices. I haven't found a suitable modification method yet. If there is a good modification method, please tell me in time.

thanks

タグ(1)
0 件の賞賛
返信

2,690件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

.MX8QX/DX there are two USB controllers:

- One is USB2 compatible and the IP comes from ChipIdea (the same USB IP used on mx5/mx6/mx7)

- One is USB3 compatible and the IP comes from Cadence.

0 件の賞賛
返信