imx8dx usb2

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx8dx usb2

2,564 次查看
songhongliang
Contributor II

HI 

I want to use the second usb of imx8dx, but I don't know how to configure it. Is there a patch or help me complete the function together.

thanks!

0 项奖励
回复
5 回复数

2,549 次查看
joanxie
NXP TechSupport
NXP TechSupport

imx8dx use usbotg3 for usb2, try to change the source code about usbotg3 in the In fsl-imx8dxp.dtsi and fsl-imx8dxp.dtsi, you need to change according to your HW, I don't have such example for you

 

 

 

0 项奖励
回复

2,547 次查看
songhongliang
Contributor II

hi 

The usb2 of imx8dx is usb2.0, the hardware is the same as the official reference schematic diagram, as shown in the picture, there are not too many other components.

thanks

0 项奖励
回复

2,537 次查看
joanxie
NXP TechSupport
NXP TechSupport

sorry I missed this picture before, for usb_otg2, I got information:

"imx8dx has two USB ports (one for chipidea, one for cdns3), and both are enabled, see arch/arm64/boot/dts/freescale/imx8x-mek.dtsi detail please."

0 项奖励
回复

2,531 次查看
songhongliang
Contributor II

HI

Is it possible to use cdns3 for USB2.0? The second USB2.0 port of imx8dx, according to the device tree configuration of cdns3, the second USB cannot be used. My USB only has DP DN. There are no other auxiliary devices. I haven't found a suitable modification method yet. If there is a good modification method, please tell me in time.

thanks

标记 (1)
0 项奖励
回复

2,523 次查看
joanxie
NXP TechSupport
NXP TechSupport

.MX8QX/DX there are two USB controllers:

- One is USB2 compatible and the IP comes from ChipIdea (the same USB IP used on mx5/mx6/mx7)

- One is USB3 compatible and the IP comes from Cadence.

0 项奖励
回复