imx8 running Linux not able to recognize USB ACM device

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8 running Linux not able to recognize USB ACM device

Jump to solution
1,450 Views
Mojosound
Contributor I

I am working on a project where we are changing from an older imx6 architecture (not NXP) to an NXP based imx8 based system.  The imx6 system was running a stock Debian and included support for the usb_acm driver.  I cannot find support for the usb_acm driver in the github repository.  The board I am testing on is not recognizing the device.  This is a key peripheral to our system and a show stopper if not supported.  The device being connected has a STM32 processor and should come up as a comm port.  I did a search but could not find an answer to this.  If I missed it, please provide the link.  Otherwise, how can I resolve this?  Thanks.

https://github.com/nxp-imx/linux-imx/tree/lf-5.15.y/

 

Evaluation board used is 8MPLUSLPD4-EVK.

 

Tags (3)
0 Kudos
Reply
1 Solution
1,426 Views
Mojosound
Contributor I

The driver name is different in github.  Instead of usb_acm the driver is cdc-acm.

View solution in original post

0 Kudos
Reply
2 Replies
1,427 Views
Mojosound
Contributor I

The driver name is different in github.  Instead of usb_acm the driver is cdc-acm.

0 Kudos
Reply
1,422 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

(y)

0 Kudos
Reply