imx8: pyeiq facial detection & face eye detection not working with live camera(v4l2, ov5640)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8: pyeiq facial detection & face eye detection not working with live camera(v4l2, ov5640)

4,317 Views
vsuneja63
Contributor III

pyeiq facial detection & face eye detection working fine with USB cam but same is not working on nxp ov5640 camera on imx8mq evk (5.4.24 bsp) target. Streaming is fine but false detection happening with wrong marking and that is also random. Its fps is around 17. What could be the issue for such behavior.

3 Replies

4,185 Views
vsuneja63
Contributor III

Hi,

Thanks!

Any update on the issue, looking forward for your response.

0 Kudos
Reply

4,185 Views
diego_dorta
NXP Employee
NXP Employee

Hi Suneja,

I have a suggestion for you, I think this question would be better if asked on the eIQ community, with that we can track it better.

Thanks,

Diego

0 Kudos
Reply

4,185 Views
vsuneja63
Contributor III

Hi Diego,

Thanks!

Did the same as you said.