Hi all,
I am playing maaxboard-mini, it can not automatically mount USB disk after booting. I need to add mount command in my boot script. but before I played maaxboard sumo, it can.
so I want to know which systems service to do it ? why missed it?
It seems to need automount.rules, I find it in recipes,
how to add it in local.conf ??
./poky/meta/recipes-core/udev/udev-extraconf/automount.rules
Thank you very much.
解決済! 解決策の投稿を見る。
Thank you very much.
I have found the solution.
I add the below line in local.conf
IMAGE_INSTALL_append += " udev udev-extraconf"
Hello jin1,
one can check usb power supplies: VDD_USB_3P3, VDD_USB_1P8, VDD_USB_0P8
and connections of USB1_TXRTUNE,USB1_VBUS using Table 8. USB recommendation of the hardware guide.
Pre built binary L5.4.70-2.3.0 boots all the way to login prompt..
if prebuilt (Demo) image works fine on custom board, one can try to build
image without additional modifications, use i.MX Yocto Project User’s Guide
Regards
Regards
Thank you very much.
I have found the solution.
I add the below line in local.conf
IMAGE_INSTALL_append += " udev udev-extraconf"