imx8: kirkstone yocto source image xen-minimal-image failing at do_rootfs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8: kirkstone yocto source image xen-minimal-image failing at do_rootfs

1,251 Views
vsuneja63
Contributor III

Hi,

Thanks!

I am building xen-image-minimal on yocto kirkstone sources for imx8 EVK but its failing at rootfs with below error:

ERROR: xen-image-minimal-1.0-r0 do_rootfs: The postinstall intercept hook 'update_gtk_icon_cache' failed

Host machine: ubuntu 20.04

Any suggestion on this issue will be really helpful.

0 Kudos
Reply
2 Replies

1,237 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

XEN only work on MX8QX and MX8QM, i think you are using MX8MQ.

 

Regards

 

0 Kudos
Reply

1,233 Views
vsuneja63
Contributor III

Hi,

Thanks!

I am building for imx8qm only, but this error doesn't seems to be specific to machine or EVK. Any suggestion on this issue?

Regards,

Vipul Kumar

 

0 Kudos
Reply