imx8 bitbake myir-image-full error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8 bitbake myir-image-full error

Jump to solution
1,166 Views
Yuto-A
Contributor I

Hi !

I am a beginner in yocto, i.mx and Ubuntu.

I am building myir-image-full on yocto zeus sources for imx8 EVK but its failing at rootfs with below error:

ERROR: myir-image-minimal-1.0-r0 do_rootfs: The postinstall intercept hook 'update_gtk_immodule_cache' failed 

 

 

What is a good solution?

 

ENV : Ubuntu 18.04.6 LTS

EVK : MYS-8MMQ6-V2-8E2D-160-I

 

Any suggestion on this issue will be really helpful.

Thank you.

 

 

Labels (1)
0 Kudos
Reply
1 Solution
1,146 Views
Yuto-A
Contributor I

I had resolved.

This error was reason is SDK update( gtk software package )

I reference this link

immodules.cache': No such file or directory (xilinx.com)

 

Thank you for view !

View solution in original post

0 Kudos
Reply
2 Replies
1,147 Views
Yuto-A
Contributor I

I had resolved.

This error was reason is SDK update( gtk software package )

I reference this link

immodules.cache': No such file or directory (xilinx.com)

 

Thank you for view !

0 Kudos
Reply
1,009 Views
J_h__
Contributor I

I have also encountered such a mistake, may I ask how you specifically solve it?

0 Kudos
Reply