imx8 android support mobile network

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8 android support mobile network

7,618件の閲覧回数
fu_qiang
Contributor II

hi all:

Now want to imx8 android9.0 use ec20 module, modify the ril related parts as well as the kernel, wanted to test whether can be normal use, found no mobile network on the upper interface of the set, now is the need to device/FSL imx8m/evk_8mq/overlay/frameworks/base/core/res/res/values/config. The XML related to modify this file, Whether someone has made the relevant modification, give some advice for reference, thank you

So here's the log associated with grabbing the radio

evk_8mq:/ # logcat -b radio -v time
01-01 00:00:14.661 D/RILD ( 3098): **RIL Daemon Started**
01-01 00:00:14.661 D/RILD ( 3098): **RILd param count=3**
01-01 00:00:14.736 D/RILD ( 3098): RIL_Init argc = 3 clientId = 0
01-01 00:00:14.748 D/use-Rlog/RLOG-RIL RILC( 3098): Quectel RIL Version: Quectel_Android_RIL_Driver_V2.9.9
01-01 00:00:14.748 D/use-Rlog/RLOG-RIL RILC( 3098): libquectel-ril build info: On branch master Your branch is up to date with 'origin/master'. ae4e66815e5934311cd560e77be34cfbf8a283cf 04/09/20_11:29:42
01-01 00:00:14.748 D/use-Rlog/RLOG-RIL RILC( 3098): Compiled date: Apr 9 2020 time: 11:29:46
01-01 00:00:14.767 E/use-Rlog/RLOG-RIL RILC( 3098): '/vendor/manifest.xml' not exist.
01-01 00:00:14.769 D/use-Rlog/RLOG-RIL RILC( 3098): t-prop_value is 1
01-01 00:00:14.769 D/use-Rlog/RLOG-RIL RILC( 3098): before_dot is 9
01-01 00:00:14.769 D/use-Rlog/RLOG-RIL RILC( 3098): [ro.build.version.release]: [9.0]
01-01 00:00:14.769 D/use-Rlog/RLOG-RIL RILC( 3098): Android Version: 90, RIL_VERSION: 12 / 12
01-01 00:00:14.769 D/use-Rlog/RLOG-RIL RILC( 3098): [ro.build.description]: [evk_8mq-userdebug 9 V002IMX8_20200421 eng.fq.20200421.100616 dev-keys]
01-01 00:00:14.769 D/use-Rlog/RLOG-RIL RILC( 3098): [ro.hardware]: [freescale]
01-01 00:00:14.769 D/use-Rlog/RLOG-RIL RILC( 3098): selinux maybe set Enforcing mode, use command getenforce to check
01-01 00:00:14.769 D/use-Rlog/RLOG-RIL RILC( 3098): selinux maybe set Enforcing mode, use command "setenforce 0" to disable
01-01 00:00:14.769 I/use-Rlog/RLOG-RIL RILC( 3098): clientID = 0
01-01 00:00:14.769 I/use-Rlog/RLOG-RIL RILC( 3098): mainLoop Start
01-01 00:00:14.770 D/use-Rlog/RLOG-RIL RILU( 3098): find quectel module /sys/bus/usb/devices/1-1.3 idVendor=2c7c idProduct=0125
01-01 00:00:15.771 D/use-Rlog/RLOG-RIL RILU( 3098): find /sys/bus/usb/devices/1-1.3:1.2/ttyUSB2
01-01 00:00:15.771 D/use-Rlog/RLOG-RIL RILU( 3098): ttyAT = ttyUSB2
01-01 00:00:15.771 D/use-Rlog/RLOG-RIL RILU( 3098): find /sys/bus/usb/devices/1-1.3:1.3/ttyUSB3
01-01 00:00:15.771 D/use-Rlog/RLOG-RIL RILU( 3098): ttyPPP = ttyUSB3
01-01 00:00:15.771 D/use-Rlog/RLOG-RIL RILU( 3098): find /sys/bus/usb/devices/1-1.3:1.0/ttyUSB0
01-01 00:00:15.772 D/use-Rlog/RLOG-RIL RILU( 3098): ttyDM = ttyUSB0
01-01 00:00:15.772 D/use-Rlog/RLOG-RIL RILU( 3098): find /sys/bus/usb/devices/1-1.3:1.1/ttyUSB1
01-01 00:00:15.772 D/use-Rlog/RLOG-RIL RILU( 3098): ttyGPS = ttyUSB1
01-01 00:00:15.772 D/use-Rlog/RLOG-RIL RILC( 3098): quectel at port is /dev/ttyUSB2
01-01 00:00:15.967 D/use-Rlog/RLOG-RIL RILC( 3098): open device /dev/ttyUSB2 correctly
01-01 00:00:15.968 E/use-Rlog/RLOG-RIL ATC( 3098): at_open s_tild_reader = 263568481072368
01-01 00:00:15.968 D/use-Rlog/RLOG-RIL ATC( 3098): AT> ATE0Q0V1
01-01 00:00:15.977 D/use-Rlog/RLOG-RIL ATC( 3098): AT< ATE0Q0V1
01-01 00:00:16.000 D/use-Rlog/RLOG-RIL ATC( 3098): AT< OK
01-01 00:00:16.500 D/use-Rlog/RLOG-RIL ATC( 3098): AT> ATI
01-01 00:00:16.501 D/use-Rlog/RLOG-RIL ATC( 3098): AT< Quectel
01-01 00:00:16.501 D/use-Rlog/RLOG-RIL ATC( 3098): AT< EC20F
01-01 00:00:16.501 D/use-Rlog/RLOG-RIL ATC( 3098): AT< Revision: EC20CEHCLGR06A01M1G_AUD
01-01 00:00:16.501 D/use-Rlog/RLOG-RIL ATC( 3098): AT< OK
01-01 00:00:16.501 D/use-Rlog/RLOG-RIL RILC( 3098): ql_product_version is EC20CEHCLGR06A01M1G_AUD
01-01 00:00:16.501 D/use-Rlog/RLOG-RIL RILC( 3098): Quectel Product Revision: EC20CEHCLGR06A01M1G_AUD
01-01 00:00:16.501 D/use-Rlog/RLOG-RIL RILC( 3098): 9X07 EC20F
01-01 00:00:16.501 D/use-Rlog/RLOG-RIL ATC( 3098): AT> AT+CSUB;+CVERSION
01-01 00:00:16.503 D/use-Rlog/RLOG-RIL ATC( 3098): AT< SubEdition: V02
01-01 00:00:16.503 D/use-Rlog/RLOG-RIL ATC( 3098): AT< VERSION: EC20CEHCLGR06A01M1G_AUD
01-01 00:00:16.503 D/use-Rlog/RLOG-RIL ATC( 3098): AT< Dec 10 2018 19:34:25
01-01 00:00:16.503 D/use-Rlog/RLOG-RIL ATC( 3098): AT< Authors: QCT
01-01 00:00:16.503 D/use-Rlog/RLOG-RIL ATC( 3098): AT< OK
01-01 00:00:16.503 D/use-Rlog/RLOG-RIL ATC( 3098): AT> ATE0Q0V1
01-01 00:00:16.504 D/use-Rlog/RLOG-RIL ATC( 3098): AT< OK
01-01 00:00:16.504 D/use-Rlog/RLOG-RIL ATC( 3098): AT> ATS0=0
01-01 00:00:16.505 D/use-Rlog/RLOG-RIL ATC( 3098): AT< OK
01-01 00:00:16.505 D/use-Rlog/RLOG-RIL ATC( 3098): AT> AT+QURCCFG="URCPORT","usbat"
01-01 00:00:16.507 D/use-Rlog/RLOG-RIL ATC( 3098): AT< OK
01-01 00:00:16.507 D/use-Rlog/RLOG-RIL ATC( 3098): AT> AT&D2
01-01 00:00:16.509 D/use-Rlog/RLOG-RIL ATC( 3098): AT< OK
01-01 00:00:16.509 D/use-Rlog/RLOG-RIL ATC( 3098): AT> AT+CMEE=1
01-01 00:00:16.510 D/use-Rlog/RLOG-RIL ATC( 3098): AT< OK
01-01 00:00:16.510 D/use-Rlog/RLOG-RIL ATC( 3098): AT> AT+CREG=2
01-01 00:00:16.511 D/use-Rlog/RLOG-RIL ATC( 3098): AT< OK
01-01 00:00:16.511 D/use-Rlog/RLOG-RIL ATC( 3098): AT> AT+CGREG=2
01-01 00:00:16.512 D/use-Rlog/RLOG-RIL ATC( 3098): AT< OK
01-01 00:00:16.512 D/use-Rlog/RLOG-RIL ATC( 3098): AT> AT^DSCI=1
01-01 00:00:16.513 D/use-Rlog/RLOG-RIL ATC( 3098): AT< ERROR
01-01 00:00:16.513 D/use-Rlog/RLOG-RIL ATC( 3098): AT> at+qdai=5
01-01 00:00:16.538 D/use-Rlog/RLOG-RIL ATC( 3098): AT< OK
01-01 00:00:16.538 D/use-Rlog/RLOG-RIL ATC( 3098): AT> AT+CFUN?
01-01 00:00:16.540 D/use-Rlog/RLOG-RIL ATC( 3098): AT< +CFUN: 1
01-01 00:00:16.540 D/use-Rlog/RLOG-RIL ATC( 3098): AT< OK
01-01 00:00:16.540 D/use-Rlog/RLOG-RIL ATC( 3098): AT> AT+CPIN?
01-01 00:00:16.543 D/use-Rlog/RLOG-RIL ATC( 3098): AT< +CME ERROR: 10
01-01 00:00:17.178 D/TelephonyManager( 3063): No /proc/cmdline exception=java.io.FileNotFoundException: /proc/cmdline (Permission denied)
01-01 00:00:17.178 D/TelephonyManager( 3063): /proc/cmdline=
01-01 00:00:17.543 D/use-Rlog/RLOG-RIL ATC( 3098): AT> AT+CFUN?
01-01 00:00:17.545 D/use-Rlog/RLOG-RIL ATC( 3098): AT< +CFUN: 1
01-01 00:00:17.545 D/use-Rlog/RLOG-RIL ATC( 3098): AT< OK
01-01 00:00:17.545 I/use-Rlog/RLOG-RIL RILC( 3098): [setRadioState]:oldState=1, newState=2
01-01 00:00:17.546 W/RILC ( 3098): RIL_onUnsolicitedResponse called before RIL_register
01-01 00:00:17.546 D/RILD ( 3098): RIL_Init rilInit completed
01-01 00:00:17.546 D/use-Rlog/RLOG-RIL ATC( 3098): AT> AT+CPIN?
01-01 00:00:17.546 I/RILC ( 3098): SIM_COUNT: 1
01-01 00:00:17.546 E/RILC ( 3098): RIL_register: RIL version 12
01-01 00:00:17.546 I/RILC ( 3098): s_registerCalled flag set, 1
01-01 00:00:17.546 D/RILC ( 3098): registerService: starting android::hardware::radio::V1_1::IRadio slot1
01-01 00:00:17.548 I/RILC ( 3098): RILHIDL called registerService
01-01 00:00:17.548 D/RILD ( 3098): RIL_Init RIL_register completed
01-01 00:00:17.548 D/RILD ( 3098): RIL_register_socket started
01-01 00:00:17.548 D/RIL_UIM_SOCKET( 3098): Adding socket with id: 0
01-01 00:00:17.548 I/RILC ( 3098): RIL_register_socket: calling registerService
01-01 00:00:17.548 D/RIL_SAP ( 3098): registerService: starting ISap slot1 for slotId 0
01-01 00:00:17.549 D/RIL_SAP ( 3098): registerService: started ISap slot1 status 0
01-01 00:00:17.549 D/RILD ( 3098): RIL_register_socket completed
01-01 00:00:17.549 D/RILD ( 3098): RIL_Init starting sleep loop
01-01 00:00:17.549 D/use-Rlog/RLOG-RIL ATC( 3098): AT< +CME ERROR: 10
01-01 00:00:17.549 I/use-Rlog/RLOG-RIL RILC( 3098): [setRadioState]:oldState=2, newState=3
01-01 00:00:17.578 E/RILC ( 3098): radioStateChangedInd: radioService[0]->mRadioIndication == NULL
01-01 00:00:17.578 D/use-Rlog/RLOG-RIL ATC( 3098): AT> AT+CSQ
01-01 00:00:17.579 D/use-Rlog/RLOG-RIL ATC( 3098): AT< +CSQ: 23,99
01-01 00:00:17.579 D/use-Rlog/RLOG-RIL ATC( 3098): AT< OK
01-01 00:00:17.579 E/RILC ( 3098): currentSignalStrengthInd: radioService[0]->mRadioIndication == NULL
01-01 00:00:17.579 D/use-Rlog/RLOG-RIL ATC( 3098): AT> AT+CGREG?
01-01 00:00:17.580 D/use-Rlog/RLOG-RIL ATC( 3098): AT< +CGREG: 2,2
01-01 00:00:17.580 D/use-Rlog/RLOG-RIL ATC( 3098): AT< OK
01-01 00:00:17.580 E/RILC ( 3098): networkStateChangedInd: radioService[0]->mRadioIndication == NULL
04-21 11:32:30.286 E/TelephonyManager( 3241): IMSI error: Subscriber Info is null
04-21 11:32:30.423 D/TelephonyManager( 3064): No /proc/cmdline exception=java.io.FileNotFoundException: /proc/cmdline (Permission denied)
04-21 11:32:30.423 D/TelephonyManager( 3064): /proc/cmdline=
04-21 11:32:31.490 D/TelephonyRegistry( 3241): listen oscl: hasNotifySubscriptionInfoChangedOccurred==false no callback
04-21 11:32:31.540 D/TelephonyRegistry( 3241): systemRunning register for intents
04-21 11:32:31.849 D/TelephonyRegistry( 3241): listen oscl: hasNotifySubscriptionInfoChangedOccurred==false no callback
04-21 11:32:32.173 D/TelephonyRegistry( 3241): notifyCellLocationForSubscriber: subId=0 cellLocation=Bundle[{}]
04-21 11:32:32.184 D/TDC ( 3648): updateOrInsert: inserting: Modem { uuid=modem, state=0, rilModel=0, rat={}, maxActiveVoiceCall=1, maxActiveDataCall=1, maxStandby=1 }
04-21 11:32:32.184 D/TDC ( 3648): updateOrInsert: inserting: Sim { uuid=sim, modemUuid=modem, state=0 }
04-21 11:32:32.187 D/CdmaSSM ( 3648): subscriptionSource from settings: 0
04-21 11:32:32.187 I/PhoneFactory( 3648): Cdma Subscription set to 0
04-21 11:32:32.187 I/PhoneFactory( 3648): ImsResolver: defaultImsPackage:
04-21 11:32:32.188 I/PhoneFactory( 3648): Network Mode set to 0
04-21 11:32:32.188 D/RILJ ( 3648): RIL: init preferredNetworkType=0 cdmaSubscription=0)
04-21 11:32:32.199 I/PhoneFactory( 3648): Creating SubscriptionController
04-21 11:32:32.202 D/SubscriptionController( 3648): [SubscriptionController] init by Context
04-21 11:32:32.208 D/UiccController( 3648): Creating UiccController
04-21 11:32:32.208 D/UiccController( 3648): config_num_physical_slots = 1
04-21 11:32:32.215 D/TelephonyTester( 3648): register for intent action=com.android.internal.telephony.action_detached
04-21 11:32:32.215 D/TelephonyTester( 3648): register for intent action=com.android.internal.telephony.action_attached
04-21 11:32:32.215 D/TelephonyTester( 3648): register for intent action=com.android.internal.telephony.TestServiceState
04-21 11:32:32.224 D/Phone ( 3648): mDoesRilSendMultipleCallRing=true
04-21 11:32:32.224 D/Phone ( 3648): mCallRingDelay=3000
04-21 11:32:32.238 D/SmsDispatchersController( 3648): SmsDispatchersController created
04-21 11:32:32.241 I/ImsManager( 3648): Creating ImsService
04-21 11:32:32.241 W/MmTelFeatureConnection( 3648): create: binder is null! Slot Id: 0
04-21 11:32:32.241 E/ImsSmsDispacher( 3648): Failed to get sms format. Error: getSmsFormat()
04-21 11:32:32.241 D/SMSDispatcher( 3648): SMSDispatcher: ctor mSmsCapable=true format=unknown mSmsSendDisabled=false
04-21 11:32:32.242 D/SMSDispatcher( 3648): SMSDispatcher: ctor mSmsCapable=true format=3gpp2 mSmsSendDisabled=false
04-21 11:32:32.242 D/CdmaSMSDispatcher( 3648): CdmaSMSDispatcher created
04-21 11:32:32.261 D/GsmInboundSmsHandler( 3648): created InboundSmsHandler
04-21 11:32:32.263 D/GsmInboundSmsHandler( 3648): entering Startup state
04-21 11:32:32.278 D/CdmaInboundSmsHandler( 3648): created InboundSmsHandler
04-21 11:32:32.285 D/CdmaInboundSmsHandler( 3648): entering Startup state
04-21 11:32:32.286 D/SMSDispatcher( 3648): SMSDispatcher: ctor mSmsCapable=true format=3gpp mSmsSendDisabled=false
04-21 11:32:32.286 D/GsmSMSDispatcher( 3648): GsmSMSDispatcher created
04-21 11:32:32.297 D/CdmaInboundSmsHandler( 3648): StartupState.processMessage:6
04-21 11:32:32.298 D/CdmaInboundSmsHandler( 3648): entering Idle state
04-21 11:32:32.298 D/CdmaInboundSmsHandler( 3648): IdleState.processMessage:5
04-21 11:32:32.298 D/CdmaInboundSmsHandler( 3648): Idle state processing message type 5
04-21 11:32:32.298 D/CdmaInboundSmsHandler( 3648): mWakeLock released
04-21 11:32:32.298 D/GsmInboundSmsHandler( 3648): StartupState.processMessage:6
04-21 11:32:32.298 D/GsmInboundSmsHandler( 3648): entering Idle state
04-21 11:32:32.298 D/GsmInboundSmsHandler( 3648): IdleState.processMessage:5
04-21 11:32:32.298 D/GsmInboundSmsHandler( 3648): Idle state processing message type 5
04-21 11:32:32.299 D/GsmInboundSmsHandler( 3648): mWakeLock released
04-21 11:32:32.299 D/CdmaSSM ( 3648): subscriptionSource from settings: 0
04-21 11:32:32.299 D/CdmaSSM ( 3648): cdmaSSM constructor: 0
04-21 11:32:32.301 D/GsmCdmaPhone( 3648): [0] Precise phone type 1
04-21 11:32:32.302 D/RILJ ( 3648): setPhoneType=1 old value=0 [SUB0]
04-21 11:32:32.305 D/CarrierActionAgent( 3648): [0]Creating CarrierActionAgent
04-21 11:32:32.306 W/CarrierConfigManager( 3648): Error getting config for subId -1 ICarrierConfigLoader is null
04-21 11:32:32.308 W/CarrierConfigManager( 3648): Error getting config for subId -1 ICarrierConfigLoader is null
04-21 11:32:32.309 D/TelephonyRegistry( 3241): listen oscl: hasNotifySubscriptionInfoChangedOccurred==false no callback
04-21 11:32:32.309 W/CarrierConfigManager( 3648): Error getting config for subId -2 ICarrierConfigLoader is null
04-21 11:32:32.309 D/NetworkRegistrationManager( 3648): Binding to packageName com.android.phone for transport type1
04-21 11:32:32.311 D/NetworkRegistrationManager( 3648): registerForNetworkRegistrationStateChanged
04-21 11:32:32.317 D/SST ( 3648): handleNetworkUnavailable
04-21 11:32:32.318 D/SST ( 3648): [0] notifyDataRegStateRilRadioTechnologyChanged: drs=1 rat=0
04-21 11:32:32.320 D/TelephonyRegistry( 3241): listen oscl: hasNotifySubscriptionInfoChangedOccurred==false no callback
04-21 11:32:32.320 D/DCT ( 3648): [0]DCT.constructor
04-21 11:32:32.321 W/CarrierConfigManager( 3648): Error getting config for subId -2 ICarrierConfigLoader is null
04-21 11:32:32.322 I/chatty ( 3648): uid=1001(radio) com.android.phone identical 1 line
04-21 11:32:32.322 W/CarrierConfigManager( 3648): Error getting config for subId -2 ICarrierConfigLoader is null
04-21 11:32:32.329 D/TelephonyRegistry( 3241): listen oscl: hasNotifySubscriptionInfoChangedOccurred==false no callback
04-21 11:32:32.330 D/Dcc ( 3648): E ctor
04-21 11:32:32.330 D/Dcc ( 3648): X ctor
04-21 11:32:32.333 D/DcTesterDeacativateAll( 3648): register for intent action=com.android.internal.telephony.dataconnection.action_deactivate_all
04-21 11:32:32.333 D/DcTesterDeacativateAll( 3648): register for intent action=com.android.internal.telephony.action_detached
04-21 11:32:32.335 D/SubscriptionController( 3648): [getPhoneId] asked for default subId=-1
04-21 11:32:32.336 D/DcTesterFailBrinupAll( 3648): register for intent action=com.android.internal.telephony.dataconnection.action_fail_bringup
04-21 11:32:32.336 D/DcTesterFailBrinupAll( 3648): register for intent action=com.android.internal.telephony.action_detached
04-21 11:32:32.336 D/DcTesterFailBrinupAll( 3648): register for intent action=com.android.internal.telephony.action_attached
04-21 11:32:32.337 D/SST ( 3648): [0] notifyDataRegStateRilRadioTechnologyChanged: drs=1 rat=0
04-21 11:32:32.338 D/DCT ( 3648): [0]update sub = -2
04-21 11:32:32.338 D/DCT ( 3648): [0]update(): Active DDS, register for all events now!
04-21 11:32:32.338 D/GsmCdmaPhone( 3648): [0] updateCurrentCarrierInProvider: mSubId = -2 currentDds = -1 operatorNumeric = null
04-21 11:32:32.339 D/DCT ( 3648): [0]initApnContexts: E
04-21 11:32:32.339 D/DCT ( 3648): [0]initApnContexts: skipping unknown type=1
04-21 11:32:32.339 D/DCT ( 3648): [0]initApnContexts: skipping unknown type=7
04-21 11:32:32.339 D/DCT ( 3648): [0]initApnContexts: skipping unknown type=9
04-21 11:32:32.342 W/CarrierConfigManager( 3461): Error getting config for subId -1 ICarrierConfigLoader is null
04-21 11:32:32.346 D/CarrierIdentifier( 3648): Creating CarrierIdentifier[0]
04-21 11:32:32.351 D/TelephonyRegistry( 3241): listen oscl: hasNotifySubscriptionInfoChangedOccurred==false no callback
04-21 11:32:32.354 D/GsmCdmaPhone( 3648): [0] GsmCdmaPhone: constructor: sub = 0
04-21 11:32:32.354 I/PhoneFactory( 3648): Creating Phone with type = 1 sub = 0
04-21 11:32:32.357 I/PhoneFactory( 3648): defaultSmsApplication: NONE
04-21 11:32:32.358 I/PhoneFactory( 3648): Creating SubInfoRecordUpdater
04-21 11:32:32.359 D/SubscriptionInfoUpdater( 3648): Constructor invoked
04-21 11:32:32.360 D/TelephonyRegistry( 3241): listen oscl: hasNotifySubscriptionInfoChangedOccurred==false no callback
04-21 11:32:32.361 D/SubscriptionController( 3648): [getActiveSubInfoList] Sub Controller not ready
04-21 11:32:32.365 D/SubscriptionController( 3648): [getPhoneId] asked for default subId=-1
04-21 11:32:32.390 I/ImsManager( 3648): Creating ImsService
04-21 11:32:32.391 W/MmTelFeatureConnection( 3648): create: binder is null! Slot Id: 0
04-21 11:32:32.391 I/ImsManager( 3648): Creating ImsService
04-21 11:32:32.392 W/MmTelFeatureConnection( 3648): create: binder is null! Slot Id: 0
04-21 11:32:32.392 D/TelephonyRegistry( 3241): listen oscl: hasNotifySubscriptionInfoChangedOccurred==false no callback
04-21 11:32:32.393 D/TelephonyRegistry( 3241): listen oscl: hasNotifySubscriptionInfoChangedOccurred==false no callback
04-21 11:32:32.394 D/PhoneSwitcher( 3648): PhoneSwitcher started
04-21 11:32:32.394 D/ProxyController( 3648): Constructor - Enter
04-21 11:32:32.395 D/ProxyController( 3648): clearTransaction
04-21 11:32:32.395 D/ProxyController( 3648): clearTransaction: phoneId=0 status=IDLE
04-21 11:32:32.395 D/ProxyController( 3648): Constructor - Exit
04-21 11:32:32.398 D/TelephonyNetworkFactory[0]( 3648): Registering NetworkFactory
04-21 11:32:32.402 D/CallManager( 3648): registerPhone(GSM Handler (com.android.internal.telephony.GsmCdmaPhone) {24363a2})
04-21 11:32:32.416 D/TelephonyRegistry( 3241): listen oscl: hasNotifySubscriptionInfoChangedOccurred==false no callback
04-21 11:32:32.416 D/CallManager( 3648): registerForMmiComplete
04-21 11:32:32.426 D/TelephonyRegistry( 3241): listen oscl: hasNotifySubscriptionInfoChangedOccurred==false no callback
04-21 11:32:32.427 D/SubscriptionController( 3648): [getPhoneId] asked for default subId=-1
04-21 11:32:32.429 D/SubscriptionManager( 3648): [getSubId]- fail
04-21 11:32:32.432 D/UiccController( 3648): EVENT_RADIO_UNAVAILABLE, dispose card
04-21 11:32:32.432 D/Phone ( 3648): config LCE service failed: com.android.internal.telephony.CommandException: RADIO_NOT_AVAILABLE
04-21 11:32:32.432 D/ImsManager( 3648): Connector: getImsService
04-21 11:32:32.432 I/ImsManager( 3648): Creating ImsService
04-21 11:32:32.433 W/MmTelFeatureConnection( 3648): create: binder is null! Slot Id: 0
04-21 11:32:32.433 E/ImsManager( 3648): Connector: Retrying getting ImsService...
04-21 11:32:32.433 D/GsmSMSDispatcher( 3648): GsmSMSDispatcher: subId = -2 slotId = 0
04-21 11:32:32.433 D/GsmCdmaPhone( 3648): [0] Event EVENT_RADIO_OFF_OR_NOT_AVAILABLE Received
04-21 11:32:32.435 D/NetworkService( 3648): network service created
04-21 11:32:32.436 D/SST ( 3648): [0] mDeviceShuttingDown=false, mDesiredPowerState=true, getRadioState=RADIO_UNAVAILABLE, mPowerOffDelayNeed=true, mAlarmSwitch=false, mRadioDisabledByCarrier=false
04-21 11:32:32.436 D/SST ( 3648): [0] pollState: modemTriggered=true
04-21 11:32:32.436 D/SST ( 3648): handleNetworkUnavailable
04-21 11:32:32.436 D/SST ( 3648): [0] useDataRegStateForDataOnlyDevice: VoiceRegState=1 DataRegState=1
04-21 11:32:32.436 D/SST ( 3648): [0] Poll ServiceState done: oldSS=[{mVoiceRegState=1(OUT_OF_SERVICE), mDataRegState=1(OUT_OF_SERVICE), mChannelNumber=0, duplexMode()=0, mCellBandwidths=[], mVoiceRoamingType=home, mDataRoamingType=home, mVoiceOperatorAlphaLong=null, mVoiceOperatorAlphaShort=null, mDataOperatorAlphaLong=null, mDataOperatorAlphaShort=null, isManualNetworkSelection=false(automatic), mRilVoiceRadioTechnology=0(Unknown), mRilDataRadioTechnology=0(Unknown), mCssIndicator=unsupported, mNetworkId=0, mSystemId=0, mCdmaRoamingIndicator=0, mCdmaDefaultRoamingIndicator=0, mIsEmergencyOnly=false, mIsDataRoamingFromRegistration=false, mIsUsingCarrierAggregation=false, mLteEarfcnRsrpBoost=0, mNetworkRegistrationStates=[]}] newSS=[{mVoiceRegState=1(OUT_OF_SERVICE), mDataRegState=1(OUT_OF_SERVICE), mChannelNumber=-1, duplexMode()=0, mCellBandwidths=[], mVoiceRoamingType=home, mDataRoamingType=home, mVoiceOperatorAlphaLong=null, mVoiceOperatorAlphaShort=null, mDataOperatorAlphaLong=null, mDataOperatorAlphaShort=null, isManualNetworkSelection=false(automatic), mRilVoiceRadioTechnology=0(Unknown), mRilDataRadioTechnology=0(Unknown), mCssIndicator=unsupported, mNetworkId=-1, mSystemId=-1, mCdmaRoamingIndicator=-1, mCdmaDefaultRoamingIndicator=-1, mIsEmergencyOnly=false, mIsDataRoamingFromRegistration=false, mIsUsingCarrierAggregation=false, mLteEarfcnRsrpBoost=0, mNetworkRegistrationStates=[]}] oldMaxDataCalls=1 mNewMaxDataCalls=1 oldReasonDataDenied=-1 mNewReasonDataDenied=-1
04-21 11:32:32.436 D/SST ( 3648): [0] pollStateDone: hasRegistered=false hasDeregistered=false hasDataAttached=false hasDataDetached=false hasDataRegStateChanged=false hasRilVoiceRadioTechnologyChanged= false hasRilDataRadioTechnologyChanged=false hasChanged=true hasVoiceRoamingOn=false hasVoiceRoamingOff=false hasDataRoamingOn=false hasDataRoamingOff=false hasLocationChanged=false has4gHandoff = false hasMultiApnSupport=false hasLostMultiApnSupport=false hasCssIndicatorChanged=false
04-21 11:32:32.436 D/SST ( 3648): [0] updateSpnDisplay: radio is on but out of service, set plmn='No service'
04-21 11:32:32.437 D/SST ( 3648): [0] updateSpnDisplay: changed sending intent rule=0 showPlmn='true' plmn='No service' showSpn='false' spn='' dataSpn='' subId='-2'
04-21 11:32:32.439 D/SubscriptionController( 3648): [setPlmnSpn] No valid subscription to store info
04-21 11:32:32.439 D/SubscriptionController( 3648): notifySubscriptionInfoChanged:
04-21 11:32:32.439 D/TelephonyRegistry( 3241): notifySubscriptionInfoChanged: first invocation mRecords.size=16
04-21 11:32:32.441 D/SubscriptionController( 3648): [getPhoneId]- no sims, returning default phoneId=2147483647
04-21 11:32:32.442 D/SubscriptionController( 3648): [getSlotIndex]- subId invalid
04-21 11:32:32.442 D/SubscriptionController( 3648): [getSubId]- invalid slotIndex=-1
04-21 11:32:32.443 D/SST ( 3648): [0] operatorNumeric null is invalid
04-21 11:32:32.443 D/LocaleTracker( 3648): updateOperatorNumericAsync. mcc/mnc=
04-21 11:32:32.443 D/SST ( 3648): handleNetworkUnavailable
04-21 11:32:32.443 D/LocaleTracker( 3648): updateOperatorNumericSync. mcc/mnc=
04-21 11:32:32.443 D/LocaleTracker( 3648): Operator numeric changes to
04-21 11:32:32.443 D/LocaleTracker( 3648): Operator numeric unavailable. Get latest cell info from the modem.
04-21 11:32:32.443 D/SST ( 3648): [0] SST.getAllCellInfo(): not implemented
04-21 11:32:32.443 D/SST ( 3648): [0] SST.getAllCellInfo(): X size=0 list=null
04-21 11:32:32.443 D/LocaleTracker( 3648): getCellInfo: cell info=null
04-21 11:32:32.443 D/LocaleTracker( 3648): Can't get cell info. Try again in 2 secs.
04-21 11:32:32.443 D/LocaleTracker( 3648): updateLocale: mcc = null, country =
04-21 11:32:32.443 D/SST ( 3648): [0] Broadcasting ServiceState : {mVoiceRegState=1(OUT_OF_SERVICE), mDataRegState=1(OUT_OF_SERVICE), mChannelNumber=-1, duplexMode()=0, mCellBandwidths=[], mVoiceRoamingType=home, mDataRoamingType=home, mVoiceOperatorAlphaLong=null, mVoiceOperatorAlphaShort=null, mDataOperatorAlphaLong=null, mDataOperatorAlphaShort=null, isManualNetworkSelection=false(automatic), mRilVoiceRadioTechnology=0(Unknown), mRilDataRadioTechnology=0(Unknown), mCssIndicator=unsupported, mNetworkId=-1, mSystemId=-1, mCdmaRoamingIndicator=-1, mCdmaDefaultRoamingIndicator=-1, mIsEmergencyOnly=false, mIsDataRoamingFromRegistration=false, mIsUsingCarrierAggregation=false, mLteEarfcnRsrpBoost=0, mNetworkRegistrationStates=[]}
04-21 11:32:32.443 D/LocaleTracker( 3648): updateLocale: Change the current country to
04-21 11:32:32.445 D/SubscriptionController( 3648): [getActiveSubInfoList] Sub Controller not ready
04-21 11:32:32.447 D/SST ( 3648): [0] mDeviceShuttingDown=false, mDesiredPowerState=true, getRadioState=RADIO_UNAVAILABLE, mPowerOffDelayNeed=true, mAlarmSwitch=false, mRadioDisabledByCarrier=false
04-21 11:32:32.447 D/SST ( 3648): [0] pollState: modemTriggered=true
04-21 11:32:32.447 D/SST ( 3648): handleNetworkUnavailable
04-21 11:32:32.447 D/SST ( 3648): [0] useDataRegStateForDataOnlyDevice: VoiceRegState=1 DataRegState=1
04-21 11:32:32.447 D/SST ( 3648): [0] Poll ServiceState done: oldSS=[{mVoiceRegState=1(OUT_OF_SERVICE), mDataRegState=1(OUT_OF_SERVICE), mChannelNumber=-1, duplexMode()=0, mCellBandwidths=[], mVoiceRoamingType=home, mDataRoamingType=home, mVoiceOperatorAlphaLong=null, mVoiceOperatorAlphaShort=null, mDataOperatorAlphaLong=null, mDataOperatorAlphaShort=null, isManualNetworkSelection=false(automatic), mRilVoiceRadioTechnology=0(Unknown), mRilDataRadioTechnology=0(Unknown), mCssIndicator=unsupported, mNetworkId=-1, mSystemId=-1, mCdmaRoamingIndicator=-1, mCdmaDefaultRoamingIndicator=-1, mIsEmergencyOnly=false, mIsDataRoamingFromRegistration=false, mIsUsingCarrierAggregation=false, mLteEarfcnRsrpBoost=0, mNetworkRegistrationStates=[]}] newSS=[{mVoiceRegState=1(OUT_OF_SERVICE), mDataRegState=1(OUT_OF_SERVICE), mChannelNumber=-1, duplexMode()=0, mCellBandwidths=[], mVoiceRoamingType=home, mDataRoamingType=home, mVoiceOperatorAlphaLong=null, mVoiceOperatorAlphaShort=null, mDataOperatorAlphaLong=null, mDataOperatorAlphaShort=null, isManualNetworkSelection=false(automatic), mRilVoiceRadioTechnology=0(Unknown), mRilDataRadioTechnology=0(Unknown), mCssIndicator=unsupported, mNetworkId=-1, mSystemId=-1, mCdmaRoamingIndicator=-1, mCdmaDefaultRoamingIndicator=-1, mIsEmergencyOnly=false, mIsDataRoamingFromRegistration=false, mIsUsingCarrierAggregation=false, mLteEarfcnRsrpBoost=0, mNetworkRegistrationStates=[]}] oldMaxDataCalls=1 mNewMaxDataCalls=1 oldReasonDataDenied=-1 mNewReasonDataDenied=-1
04-21 11:32:32.447 D/SST ( 3648): [0] pollStateDone: hasRegistered=false hasDeregistered=false hasDataAttached=false hasDataDetached=false hasDataRegStateChanged=false hasRilVoiceRadioTechnologyChanged= false hasRilDataRadioTechnologyChanged=false hasChanged=false hasVoiceRoamingOn=false hasVoiceRoamingOff=false hasDataRoamingOn=false hasDataRoamingOff=false hasLocationChanged=false has4gHandoff = false hasMultiApnSupport=false hasLostMultiApnSupport=false hasCssIndicatorChanged=false
04-21 11:32:32.448 I/CSST ( 3648): PrefNetworkNotification: sendMessage() w/values: ,false,-1,false,false
04-21 11:32:32.448 I/CSST ( 3648): canceling notifications: 1000
04-21 11:32:32.448 D/Phone ( 3648): isWifiCallingEnabled =false
04-21 11:32:32.448 D/CSST ( 3648): isPhoneRegisteredForWifiCalling: false
04-21 11:32:32.448 D/Phone ( 3648): isWifiCallingEnabled =false
04-21 11:32:32.448 I/CSST ( 3648): EmergencyNetworkNotification: sendMessage() w/values: ,false,-1,false,false
04-21 11:32:32.448 I/CSST ( 3648): canceling notifications: 1001
04-21 11:32:32.449 I/CSST ( 3648): PrefNetworkNotification: sendMessage() w/values: ,false,-1,false,false
04-21 11:32:32.449 I/CSST ( 3648): canceling notifications: 1000
04-21 11:32:32.449 D/Phone ( 3648): isWifiCallingEnabled =false
04-21 11:32:32.449 D/CSST ( 3648): isPhoneRegisteredForWifiCalling: false
04-21 11:32:32.449 D/Phone ( 3648): isWifiCallingEnabled =false
04-21 11:32:32.449 I/CSST ( 3648): EmergencyNetworkNotification: sendMessage() w/values: ,false,-1,false,false
04-21 11:32:32.449 I/CSST ( 3648): canceling notifications: 1001
04-21 11:32:32.454 D/DataService( 3648): Data service created
04-21 11:32:32.454 D/DCT ( 3648): [0]onRadioOffOrNotAvailable: is off and clean up all connections
04-21 11:32:32.454 D/DCT ( 3648): [0]cleanUpAllConnections: tearDown=false reason=radioTurnedOff
04-21 11:32:32.454 D/DCT ( 3648): [0]stopNetStatPoll
04-21 11:32:32.455 D/DCT ( 3648): [0]cleanUpConnection: mDisconnectPendingCount = 0
04-21 11:32:32.455 D/DCT ( 3648): [0]onDataConnectionDetached: stop polling and notify detached
04-21 11:32:32.455 D/DCT ( 3648): [0]stopNetStatPoll
04-21 11:32:32.455 D/DCT ( 3648): [0]notifyDataConnection: reason=dataDetached
04-21 11:32:32.455 D/DCT ( 3648): [0]onDataRoamingOff
04-21 11:32:32.456 D/DCT ( 3648): [0]setInitialApn: E mPreferredApn=null
04-21 11:32:32.456 D/DCT ( 3648): [0]setInitialAttachApn: X There in no available apn
04-21 11:32:32.456 D/DCT ( 3648): [0]setDataProfilesAsNeeded
04-21 11:32:32.456 D/DCT ( 3648): [0]setupDataOnConnectableApns: roamingOff
04-21 11:32:32.456 D/TelephonyNetworkFactory[0]( 3648): onSubIdChange -1->-2
04-21 11:32:32.456 D/TelephonyNetworkFactory[0]( 3648): got request NetworkRequest [ BACKGROUND_REQUEST id=2, [ Transports: CELLULAR Capabilities: INTERNET&NOT_RESTRICTED&TRUSTED&NOT_VPN Unwanted: ] ] with score 0
04-21 11:32:32.456 D/TelephonyNetworkFactory[0]( 3648): got request NetworkRequest [ TRACK_DEFAULT id=8, [ Capabilities: INTERNET&NOT_RESTRICTED&TRUSTED Unwanted: Uid: 10029] ] with score 0
04-21 11:32:32.456 D/TelephonyNetworkFactory[0]( 3648): got request NetworkRequest [ REQUEST id=1, [ Capabilities: INTERNET&NOT_RESTRICTED&TRUSTED&NOT_VPN Unwanted: ] ] with score 0
04-21 11:32:32.456 D/TelephonyNetworkFactory[0]( 3648): got request NetworkRequest [ TRACK_DEFAULT id=6, [ Capabilities: INTERNET&NOT_RESTRICTED&TRUSTED Unwanted: Uid: 1000] ] with score 0
04-21 11:32:32.457 D/DebugService( 3648): DebugService DebugService:
04-21 11:32:32.462 D/GsmSMSDispatcher( 3648): GsmSMSDispatcher: subId = -2 slotId = 0
04-21 11:32:32.462 D/GsmCdmaCallTracker( 3648): Event EVENT_POLL_CALLS_RESULT Received
04-21 11:32:32.463 D/GsmCdmaCallTracker( 3648): [0] update phone state, old=IDLE new=IDLE
04-21 11:32:32.463 D/NetworkRegistrationManager( 3648): service connected.
04-21 11:32:32.463 D/DCT ( 3648): [0]SubscriptionListener.onSubscriptionInfoChanged
04-21 11:32:32.463 D/CarrierIdentifier( 3648): SubscriptionListener.onSubscriptionInfoChanged subId: -2
04-21 11:32:32.467 I/ImsManager( 3648): Creating ImsService
04-21 11:32:32.467 W/MmTelFeatureConnection( 3648): create: binder is null! Slot Id: 0
04-21 11:32:32.478 D/SubscriptionController( 3648): [getActiveSubInfoList] Sub Controller not ready
04-21 11:32:32.479 D/PhoneSwitcher( 3648): evaluating due to subChanged default 0->-1 phone[0] 0->-2
04-21 11:32:32.479 D/SST ( 3648): [0] SubscriptionListener.onSubscriptionInfoChanged
04-21 11:32:32.479 D/GsmCdmaPhone( 3648): [0] updateVoiceMail countVoiceMessages = 0 subId -2
04-21 11:32:32.479 E/Phone ( 3648): setVoiceMessageCount in sharedPreference: invalid subId -2
04-21 11:32:32.480 D/SubscriptionController( 3648): [getSlotIndex]- subId invalid
04-21 11:32:32.480 D/CellularDataService( 3648): Cellular data service created for slot 0
04-21 11:32:32.480 D/PhoneSwitcher( 3648): evaluating due to netRequest
04-21 11:32:32.480 I/chatty ( 3648): uid=1001(radio) com.android.phone identical 2 lines
04-21 11:32:32.480 D/PhoneSwitcher( 3648): evaluating due to netRequest
04-21 11:32:32.480 D/TelephonyNetworkFactory[0]( 3648): not acting - isApp=false, isAct=false NetworkRequest [ BACKGROUND_REQUEST id=2, [ Transports: CELLULAR Capabilities: INTERNET&NOT_RESTRICTED&TRUSTED&NOT_VPN Unwanted: ] ]
04-21 11:32:32.481 D/TelephonyNetworkFactory[0]( 3648): not acting - isApp=false, isAct=false NetworkRequest [ TRACK_DEFAULT id=8, [ Capabilities: INTERNET&NOT_RESTRICTED&TRUSTED Unwanted: Uid: 10029] ]
04-21 11:32:32.481 D/TelephonyNetworkFactory[0]( 3648): not acting - isApp=false, isAct=false NetworkRequest [ REQUEST id=1, [ Capabilities: INTERNET&NOT_RESTRICTED&TRUSTED&NOT_VPN Unwanted: ] ]
04-21 11:32:32.481 D/TelephonyNetworkFactory[0]( 3648): not acting - isApp=false, isAct=false NetworkRequest [ TRACK_DEFAULT id=6, [ Capabilities: INTERNET&NOT_RESTRICTED&TRUSTED Unwanted: Uid: 1000] ]
04-21 11:32:32.483 I/ImsManager( 3648): Creating ImsService
04-21 11:32:32.484 W/MmTelFeatureConnection( 3648): create: binder is null! Slot Id: 0
04-21 11:32:32.488 D/SST ( 3648): [0] EVENT_SIM_NOT_INSERTED
04-21 11:32:32.488 D/SST ( 3648): [0] cancelAllNotifications: mPrevSubId=-1
04-21 11:32:32.488 E/DcTracker( 3648): Unhandled event={ when=-8ms what=270385 obj=android.os.AsyncResult@168ad20 target=com.android.internal.telephony.dataconnection.DcTracker }
04-21 11:32:32.934 D/ImsManager( 3648): Connector: getImsService
04-21 11:32:32.935 I/ImsManager( 3648): Creating ImsService
04-21 11:32:32.935 W/MmTelFeatureConnection( 3648): create: binder is null! Slot Id: 0
04-21 11:32:32.935 E/ImsManager( 3648): Connector: Retrying getting ImsService...
04-21 11:32:33.688 D/SubscriptionController( 3648): [getActiveSubInfoList] Sub Controller not ready
04-21 11:32:33.937 D/ImsManager( 3648): Connector: getImsService
04-21 11:32:33.937 I/ImsManager( 3648): Creating ImsService
04-21 11:32:33.938 W/MmTelFeatureConnection( 3648): create: binder is null! Slot Id: 0
04-21 11:32:33.938 E/ImsManager( 3648): Connector: Retrying getting ImsService...
04-21 11:32:34.445 D/SST ( 3648): [0] SST.getAllCellInfo(): not implemented
04-21 11:32:34.445 D/SST ( 3648): [0] SST.getAllCellInfo(): X size=0 list=null
04-21 11:32:34.445 D/LocaleTracker( 3648): getCellInfo: cell info=null
04-21 11:32:34.446 D/LocaleTracker( 3648): Can't get cell info. Try again in 4 secs.
04-21 11:32:34.446 D/LocaleTracker( 3648): updateLocale: mcc = null, country =
04-21 11:32:34.708 D/WAP PUSH( 3648): Received broadcast android.intent.action.USER_UNLOCKED
04-21 11:32:34.709 D/WAP PUSH( 3648): Received broadcast android.intent.action.USER_UNLOCKED
04-21 11:32:34.709 D/SmsBroadcastUndelivered( 3648): Received broadcast android.intent.action.USER_UNLOCKED
04-21 11:32:34.710 E/WAP PUSH( 3648): bindService() for wappush manager failed
04-21 11:32:34.711 E/WAP PUSH( 3648): bindService() for wappush manager failed
04-21 11:32:34.711 D/SmsBroadcastUndelivered( 3648): scanning raw table for undelivered messages
04-21 11:32:34.803 D/SmsBroadcastUndelivered( 3648): finished scanning raw table in 91 ms
04-21 11:32:35.258 D/GsmCellBroadcastHandler( 3648): mWakeLock released
04-21 11:32:35.274 D/CellBroadcastHandler( 3648): mWakeLock released
04-21 11:32:35.287 D/CdmaServiceCategoryProgramHandler( 3648): mWakeLock released
04-21 11:32:35.940 D/ImsManager( 3648): Connector: getImsService
04-21 11:32:35.940 I/ImsManager( 3648): Creating ImsService
04-21 11:32:35.942 W/MmTelFeatureConnection( 3648): create: binder is null! Slot Id: 0
04-21 11:32:35.943 E/ImsManager( 3648): Connector: Retrying getting ImsService...
04-21 11:32:36.609 D/use-Rlog/RLOG-RIL ATC( 3098): AT> at+qcfg="aprstlevel"
04-21 11:32:36.806 D/use-Rlog/RLOG-RIL ATC( 3098): AT< +QCFG: "ApRstLevel",1
04-21 11:32:36.806 D/use-Rlog/RLOG-RIL ATC( 3098): AT< OK
04-21 11:32:36.806 D/use-Rlog/RLOG-RIL ATC( 3098): AT> at+qcfg="modemrstlevel",0
04-21 11:32:36.827 D/use-Rlog/RLOG-RIL ATC( 3098): AT< OK
04-21 11:32:36.827 D/use-Rlog/RLOG-RIL ATC( 3098): AT> at+qcfg="dbgctl",1
04-21 11:32:36.838 D/use-Rlog/RLOG-RIL ATC( 3098): AT< OK
04-21 11:32:36.839 D/use-Rlog/RLOG-RIL ATC( 3098): AT> AT+QSCLK=1
04-21 11:32:36.841 D/use-Rlog/RLOG-RIL ATC( 3098): AT< OK
04-21 11:32:38.447 D/SST ( 3648): [0] SST.getAllCellInfo(): not implemented
04-21 11:32:38.447 D/SST ( 3648): [0] SST.getAllCellInfo(): X size=0 list=null
04-21 11:32:38.447 D/LocaleTracker( 3648): getCellInfo: cell info=null
04-21 11:32:38.447 D/LocaleTracker( 3648): Can't get cell info. Try again in 8 secs.
04-21 11:32:38.447 D/LocaleTracker( 3648): updateLocale: mcc = null, country =
04-21 11:32:39.946 D/ImsManager( 3648): Connector: getImsService
04-21 11:32:39.947 I/ImsManager( 3648): Creating ImsService
04-21 11:32:39.948 W/MmTelFeatureConnection( 3648): create: binder is null! Slot Id: 0
04-21 11:32:39.948 E/ImsManager( 3648): Connector: Retrying getting ImsService...
04-21 11:32:41.647 D/SipService( 3648): SipService: started!
04-21 11:32:41.652 D/SipService( 3648): start:
04-21 11:32:41.862 D/SubscriptionController( 3648): [getActiveSubInfoList] Sub Controller not ready
04-21 11:32:41.889 I/chatty ( 3648): uid=1001(radio) Binder:3648_6 identical 8 lines
04-21 11:32:41.896 D/SubscriptionController( 3648): [getActiveSubInfoList] Sub Controller not ready
04-21 11:32:41.901 D/SubscriptionController( 3648): [getActiveSubInfoList] Sub Controller not ready
04-21 11:32:41.905 D/SubscriptionController( 3648): [getActiveSubInfoList] Sub Controller not ready
04-21 11:32:41.943 I/chatty ( 3648): uid=1001(radio) Binder:3648_6 identical 9 lines
04-21 11:32:41.950 D/SubscriptionController( 3648): [getActiveSubInfoList] Sub Controller not ready
04-21 11:32:42.910 D/SubscriptionController( 3648): [getPhoneId] asked for default subId=-1
04-21 11:32:44.731 D/SubscriptionController( 3648): [getSlotIndex]- subId invalid
04-21 11:32:44.732 D/SubscriptionController( 3648): [getSlotIndex]- subId invalid
04-21 11:32:46.430 D/SubscriptionController( 3648): [getActiveSubInfoList] Sub Controller not ready
04-21 11:32:46.453 D/SST ( 3648): [0] SST.getAllCellInfo(): not implemented
04-21 11:32:46.453 D/SST ( 3648): [0] SST.getAllCellInfo(): X size=0 list=null
04-21 11:32:46.453 D/LocaleTracker( 3648): getCellInfo: cell info=null
04-21 11:32:46.454 D/LocaleTracker( 3648): Can't get cell info. Try again in 16 secs.
04-21 11:32:46.454 D/LocaleTracker( 3648): updateLocale: mcc = null, country =
04-21 11:32:46.613 D/use-Rlog/RLOG-RIL ATC( 3098): AT> AT+CSQ
04-21 11:32:46.808 D/use-Rlog/RLOG-RIL ATC( 3098): AT< +CSQ: 23,99
04-21 11:32:46.808 D/use-Rlog/RLOG-RIL ATC( 3098): AT< OK
04-21 11:32:46.809 E/RILC ( 3098): currentSignalStrengthInd: radioService[0]->mRadioIndication == NULL
04-21 11:32:46.809 D/use-Rlog/RLOG-RIL ATC( 3098): AT> AT+CGREG?
04-21 11:32:46.810 D/use-Rlog/RLOG-RIL ATC( 3098): AT< +CGREG: 2,2
04-21 11:32:46.810 D/use-Rlog/RLOG-RIL ATC( 3098): AT< OK
04-21 11:32:46.926 D/TelephonyNetworkFactory[0]( 3648): got request NetworkRequest [ TRACK_DEFAULT id=10, [ Capabilities: INTERNET&NOT_RESTRICTED&TRUSTED Unwanted: Uid: 10071] ] with score 0
04-21 11:32:46.926 D/PhoneSwitcher( 3648): evaluating due to netRequest
04-21 11:32:46.927 D/TelephonyNetworkFactory[0]( 3648): not acting - isApp=false, isAct=false NetworkRequest [ TRACK_DEFAULT id=10, [ Capabilities: INTERNET&NOT_RESTRICTED&TRUSTED Unwanted: Uid: 10071] ]
04-21 11:32:47.217 D/SubscriptionController( 3648): [getSlotIndex]- subId invalid
04-21 11:32:47.217 D/SubscriptionController( 3648): [getSubId]- invalid slotIndex=-1
04-21 11:32:47.472 D/SubscriptionController( 3648): [getSlotIndex]- subId invalid
04-21 11:32:47.472 D/SubscriptionController( 3648): [getSubId]- invalid slotIndex=-1
04-21 11:32:47.639 D/SubscriptionController( 3648): [getActiveSubInfoList] Sub Controller not ready
04-21 11:32:47.664 D/SubscriptionController( 3648): [getSlotIndex]- subId invalid
04-21 11:32:47.950 D/ImsManager( 3648): Connector: getImsService
04-21 11:32:47.950 I/ImsManager( 3648): Creating ImsService
04-21 11:32:47.953 W/MmTelFeatureConnection( 3648): create: binder is null! Slot Id: 0
04-21 11:32:47.954 E/ImsManager( 3648): Connector: Retrying getting ImsService...
04-21 11:32:48.081 D/SubscriptionController( 3648): [getPhoneId] asked for default subId=-1

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

7,176件の閲覧回数
cmsd
Contributor III

Did you get your modem/RIL working?

I am also seeing the errors:

04-21 11:32:30.286 E/TelephonyManager( 3241): IMSI error: Subscriber Info is null

and

01-01 00:00:17.178 D/TelephonyManager( 3063): No /proc/cmdline exception=java.io.FileNotFoundException: /proc/cmdline (Permission denied)
01-01 00:00:17.178 D/TelephonyManager( 3063): /proc/cmdline=

Assuming you got your modem/RIL working:

- What did you need to do to get a signal strength indicator to appear?

- Likewise for a Settings page?

0 件の賞賛
返信

7,450件の閲覧回数
fu_qiang
Contributor II

hi Bio_TICFSL

Thank you for your reply

I don't quite catch your meaning. Now I just want to be able to surf the Internet using SIM CARDS on the board,

From my perspective, this should be similar to PPP dial-up.What you said is similar to the lack of Google communication framework

0 件の賞賛
返信

7,450件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Android BSP from NXP does not offer,  the Android Phone or the  Play Store in the package, since this required licensing from Google, so you need to contact Google in order to get Android Services, then you would get an APK to install in your customized BSP

Regards

0 件の賞賛
返信

7,174件の閲覧回数
cmsd
Contributor III

Hi Bio_TICFSL,

Are Android Services required for RIL integration?  (Android 10 / iMX8M / Quectel EM12-G in my case.)

I don't need to use a particular dialler (there is already a bare-bones dialler in the Android 10 / iMX8M build.)

I do need to see the signal strength on the top bar and to see the IMEI and other details under Settings.

Thanks, Chris.

0 件の賞賛
返信