imx8: HDMI display screen not coming up with imx8qxp android12

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx8: HDMI display screen not coming up with imx8qxp android12

3,276 次查看
SGPT31
Contributor I

Hi,

I could build & flash android12 in imx8qxp emmc. I could see image boot up via console but at the same time nothing coming up on display. I tried both ports lvds0 & lvds1 but same result. I could see some graphics composer related errors in kernel logs. Adding below kernel logs for reference, looking forward for your response asap.

mek_8q:/ # dmesg
[    0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd042]
[    0.000000] Linux version 5.15.52-dirty (agl@agl-OptiPlex-7010) (Android (8508608, based on r450784e) clang version 14.0.7 (https://android.googlesource.com/toolchain/llvm-project 4c603efb0cca074e9238af8b4106c30add4418f6), LLD 14.0.7) #1 SMP PREEMPT Tue Jan 31 20:43:42 IST 2023
[    0.000000] Machine model: Freescale i.MX8QXP MEK
[    0.000000] Stack Depot is disabled
[    0.000000] efi: UEFI not found.
[    0.000000] Reserved memory: created DMA memory pool at 0x0000000090400000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node vdevbuffer, compatible id shared-dma-pool1|mek_8q:/ # dmesg
[    0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd042]
[    0.000000] Linux version 5.15.52-dirty (agl@agl-OptiPlex-7010) (Android (8508608, based on r450784e) clang version 14.0.7 (https://android.googlesource.com/toolchain/llvm-project 4c603efb0cca074e9238af8b4106c30add4418f6), LLD 14.0.7) #1 SMP PREEMPT Tue Jan 31 20:43:42 IST 2023
[    0.000000] Machine model: Freescale i.MX8QXP MEK
[    0.000000] Stack Depot is disabled
[    0.000000] efi: UEFI not found.
[    0.000000] Reserved memory: created DMA memory pool at 0x0000000090400000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node vdevbuffer, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x0000000094300000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node vdev0buffer@94300000, compatible id shared-dma-pool
[    0.000000] NUMA: No NUMA configuration found
[    0.000000] NUMA: Faking a node at [mem 0x0000000080200000-0x00000008bfffffff]
[    0.000000] NUMA: NODE_DATA [mem 0x8bfa47640-0x8bfa49fff]
[    0.000000] kvm [0]: Reserved 22 MiB at 0x8be400000
[    0.000000] Zone ranges:
[    0.000000] DMA      [mem 0x0000000080200000-0x00000000ffffffff]
[    0.000000] DMA32    empty
[    0.000000] Normal   [mem 0x0000000100000000-0x00000008bfffffff]
[    0.000000] Movable zone start for each node
[    0.000000] Early memory node ranges
[    0.000000] node   0: [mem 0x0000000080200000-0x0000000083ffffff]
[    0.000000] node   0: [mem 0x0000000084000000-0x00000000861fffff]
[    0.000000] node   0: [mem 0x0000000086200000-0x0000000087ffffff]
[    0.000000] node   0: [mem 0x000000008a000000-0x000000008fffffff]
[    0.000000] node   0: [mem 0x0000000090c00000-0x0000000091ffffff]
[    0.000000] node   0: [mem 0x0000000092000000-0x00000000920fffff]
[    0.000000] node   0: [mem 0x0000000092100000-0x00000000923fffff]
[    0.000000] node   0: [mem 0x0000000092400000-0x0000000094afffff]
[    0.000000] node   0: [mem 0x0000000094b00000-0x00000000fdffffff]
[    0.000000] node   0: [mem 0x0000000880000000-0x000000088fffffff]
[    0.000000] node   0: [mem 0x0000000890000000-0x00000008bfffffff]
[    0.000000] Initmem setup node 0 [mem 0x0000000080200000-0x00000008bfffffff]
[    0.000000] On node 0, zone DMA: 512 pages in unavailable ranges
[    0.000000] On node 0, zone DMA: 8192 pages in unavailable ranges
[    0.000000] On node 0, zone DMA: 3072 pages in unavailable ranges
[    0.000000] On node 0, zone Normal: 8192 pages in unavailable ranges
[    0.000000] cma: Reserved 928 MiB at 0x00000000c2000000
[    0.000000] psci: probing for conduit method from DT.
[    0.000000] psci: PSCIv1.1 detected in firmware.
[    0.000000] psci: Using standard PSCI v0.2 function IDs
[    0.000000] psci: MIGRATE_INFO_TYPE not supported.
[    0.000000] psci: SMC Calling Convention v1.2
[    0.000000] percpu: Embedded 30 pages/cpu s83160 r8192 d31528 u122880
[    0.000000] pcpu-alloc: s83160 r8192 d31528 u122880 alloc=30*4096
[    0.000000] pcpu-alloc: [0] 0 [0] 1 [0] 2 [0] 3
[    0.000000] Detected VIPT I-cache on CPU0
[    0.000000] CPU features: SYS_ID_AA64MMFR1_EL1[11:8]: already set to 0
[    0.000000] CPU features: detected: GIC system register CPU interface
[    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 754184
[    0.000000] Policy zone: Normal
[    0.000000] Kernel command line: stack_depot_disable=on kasan.stacktrace=off kvm-arm.mode=protected cgroup_disable=pressure console=ttyLP0,115200 earlycon init=/init androidboot.hardware=nxp firmware_class.path=/vendor/firmware loop.max_part=7 androidboot.fbTileSupport=enable cma=928M@0x960M-0xfc0M transparent_hugepage=never androidboot.lcd_density=240 androidboot.primary_display=imx-drm androidboot.wificountrycode=CN moal.mod_para=wifi_mod_para.conf pci=nomsi video=HDMI-A-2:d androidboot.vendor.sysrq=1 buildvariant=userdebug rootwait androidboot.serialno=0818900e828fc1ee androidboot.btmacaddr=08:18:90:0e:82:8f androidboot.soc_type=imx8qxp androidboot.soc_rev=revc androidboot.boot_device_root=mmcblk0 androidboot.boottime=1BLL:0,1BLE:6099,KL:0,KD:0,AVB:432,ODT:0,SW:0 androidboot.bootreason=reboot androidboot.dtbo_idx=0 androidboot.keystore=software androidboot.verifiedbootstate=orange androidboot.flash.locked=0 androidboot.slot_suffix=_a dm="1 vroot none ro 1,0 3095928 ve
[    0.000000] cgroup: Disabling pressure control group feature
[    0.000000] device-mapper: init: will configure 1 devices
[    0.000000] Unknown kernel command line parameters "buildvariant=userdebug", will be passed to user space.
[    0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes, linear)
[    0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[    0.000000] mem auto-init: stack:all(zero), heap alloc:on, heap free:off
[    0.000000] software IO TLB: mapped [mem 0x00000000be000000-0x00000000c2000000] (64MB)
[    0.000000] Memory: 1584336K/3065856K available (22656K kernel code, 2530K rwdata, 13516K rodata, 1600K init, 652K bss, 531248K reserved, 950272K cma-reserved)
[    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[    0.000000] trace event string verifier disabled
[    0.000000] rcu: Preemptible hierarchical RCU implementation.
[    0.000000] rcu: \x09RCU event tracing is enabled.
[    0.000000] rcu: \x09RCU dyntick-idle grace-period acceleration is enabled.
[    0.000000] rcu: \x09RCU restricting CPUs from NR_CPUS=32 to nr_cpu_ids=4.
[    0.000000] \x09Trampoline variant of Tasks RCU enabled.
[    0.000000] \x09Tracing variant of Tasks RCU enabled.
[    0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[    0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[    0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[    0.000000] GICv3: 512 SPIs implemented
[    0.000000] GICv3: 0 Extended SPIs implemented
[    0.000000] GICv3: Distributor has no Range Selector support
[    0.000000] Root IRQ handler: gic_handle_irq.0063cfc43c850c778600e9fd9282e821.cfi_jt
[    0.000000] GICv3: 16 PPIs implemented
[    0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000051b00000
[    0.000000] rcu: \x09Offload RCU callbacks from CPUs: (none).
[    0.000000] kfence: initialized - using 524288 bytes for 63 objects at 0x(____ptrval____)-0x(____ptrval____)
[    0.000000] arch_timer: cp15 timer(s) running at 8.00MHz (phys).
[    0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x1d854df40, max_idle_ns: 440795202120 ns
[    0.000001] sched_clock: 56 bits at 8MHz, resolution 125ns, wraps every 2199023255500ns
[    0.001438] Calibrating delay loop (skipped), value calculated using timer frequency.. 16.00 BogoMIPS (lpj=32000)
[    0.001461] pid_max: default: 32768 minimum: 301
[    0.001869] LSM: Security Framework initializing
[    0.001988] SELinux:  Initializing.
[    0.002513] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes, linear)
[    0.002547] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes, linear)
[    0.005884] rcu: Hierarchical SRCU implementation.
[    0.006640] dyndbg: Ignore empty _ddebug table in a CONFIG_DYNAMIC_DEBUG_CORE build
[    0.007478] EFI services will not be available.
[    0.008244] smp: Bringing up secondary CPUs ...
[    0.009745] Detected VIPT I-cache on CPU1
[    0.009792] GICv3: CPU1: found redistributor 1 region 0:0x0000000051b20000
[    0.009849] CPU1: Booted secondary processor 0x0000000001 [0x410fd042]
[    0.011448] Detected VIPT I-cache on CPU2
[    0.011484] GICv3: CPU2: found redistributor 2 region 0:0x0000000051b40000
[    0.011523] CPU2: Booted secondary processor 0x0000000002 [0x410fd042]
[    0.013095] Detected VIPT I-cache on CPU3
[    0.013132] GICv3: CPU3: found redistributor 3 region 0:0x0000000051b60000
[    0.013171] CPU3: Booted secondary processor 0x0000000003 [0x410fd042]
[    0.013295] smp: Brought up 1 node, 4 CPUs
[    0.013352] SMP: Total of 4 processors activated.
[    0.013362] CPU features: detected: 32-bit EL0 Support
[    0.013370] CPU features: detected: 32-bit EL1 Support
[    0.013380] CPU features: detected: CRC32 instructions
[    0.013392] CPU features: detected: Protected KVM
[    0.013522] CPU features: emulated: Privileged Access Never (PAN) using TTBR0_EL1 switching
[    0.024431] CPU: All CPU(s) started at EL2
[    0.024552] alternatives: patching kernel code
[    0.027351] devtmpfs: initialized
[    0.055810] Registered cp15_barrier emulation handler
[    0.055846] Registered setend emulation handler
[    0.055862] KASLR disabled due to lack of seed
[    0.056151] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[    0.056195] futex hash table entries: 1024 (order: 4, 65536 bytes, linear)
[    0.086601] pinctrl core: initialized pinctrl subsystem
[    0.088522] NET: Registered PF_NETLINK/PF_ROUTE protocol family
[    0.102824] DMA: preallocated 512 KiB GFP_KERNEL pool for atomic allocations
[    0.103480] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[    0.103678] audit: initializing netlink subsys (disabled)
[    0.104071] audit: type=2000 audit(0.100:1): state=initialized audit_enabled=0 res=1
[    0.104869] thermal_sys: Registered thermal governor 'step_wise'
[    0.105417] cpuidle: using governor menu
[    0.106275] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[    0.106418] ASID allocator initialised with 65536 entries
[    0.106722] imx mu driver is registered.
[    0.106773] imx rpmsg driver is registered.
[    0.168478] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages
[    0.168509] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages
[    0.168520] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[    0.168531] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages
[    0.169218] cryptomgr_test (42) used greatest stack depth: 14096 bytes left
[    0.176594] ACPI: Interpreter disabled.
[    0.177877] iommu: Default domain type: Translated
[    0.177895] iommu: DMA domain TLB invalidation policy: strict mode
[    0.178845] SCSI subsystem initialized
[    0.179148] libata version 3.00 loaded.
[    0.179393] usbcore: registered new interface driver usbfs
[    0.179447] usbcore: registered new interface driver hub
[    0.179506] usbcore: registered new device driver usb
[    0.181292] mc: Linux media interface: v0.10
[    0.181341] videodev: Linux video capture interface: v2.00
[    0.181495] pps_core: LinuxPPS API ver. 1 registered
[    0.181505] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[    0.181530] PTP clock support registered
[    0.181618] EDAC MC: Ver: 3.0.0
[    0.183727] Advanced Linux Sound Architecture Driver Initialized.
[    0.185726] imx-scu scu: NXP i.MX SCU Initialized
[    0.208845] imx8qxp-pinctrl scu:pinctrl: Invalid fsl,pins or pins property in node /scu/pinctrl/wifi_initgrp
[    0.208924] imx8qxp-pinctrl scu:pinctrl: initialized IMX pinctrl driver
[    0.211821] clocksource: Switched to clocksource arch_sys_counter
[    0.296709] VFS: Disk quotas dquot_6.6.0
[    0.296820] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[    0.297236] pnp: PnP ACPI: disabled
[    0.325345] NET: Registered PF_INET protocol family
[    0.325610] IP idents hash table entries: 65536 (order: 7, 524288 bytes, linear)
[    0.328705] tcp_listen_portaddr_hash hash table entries: 2048 (order: 3, 32768 bytes, linear)
[    0.328827] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear)
[    0.328926] TCP established hash table entries: 32768 (order: 6, 262144 bytes, linear)
[    0.329331] TCP bind hash table entries: 32768 (order: 7, 524288 bytes, linear)
[    0.329836] TCP: Hash tables configured (established 32768 bind 32768)
[    0.330046] UDP hash table entries: 2048 (order: 4, 65536 bytes, linear)
[    0.330161] UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes, linear)
[    0.330542] NET: Registered PF_UNIX/PF_LOCAL protocol family
[    0.331280] PCI: CLS 0 bytes, default 64
[    0.332505] hw perfevents: enabled with armv8_cortex_a35 PMU driver, 7 counters available
[    0.334159] kvm [1]: IPA Size Limit: 40 bits
[    0.361655] kvm [1]: GICv3: no GICV resource entry
[    0.361686] kvm [1]: disabling GICv2 emulation
[    0.361711] kvm [1]: GIC system register CPU interface enabled
[    0.361899] kvm [1]: vgic interrupt IRQ9
[    0.362157] kvm [1]: Protected nVHE mode initialized successfully
[    0.369288] Initialise system trusted keyrings
[    0.369621] workingset: timestamp_bits=42 max_order=20 bucket_order=0
[    0.385971] fuse: init (API version 7.34)
[    0.435979] xor: measuring software checksum speed
[    0.441732] 8regs           :  1728 MB/sec
[    0.446679] 32regs          :  1997 MB/sec
[    0.451691] arm64_neon      :  1971 MB/sec
[    0.451702] xor: using function: 32regs (1997 MB/sec)
[    0.451726] Key type asymmetric registered
[    0.451737] Asymmetric key parser 'x509' registered
[    0.452044] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 239)
[    0.452059] io scheduler mq-deadline registered
[    0.452069] io scheduler kyber registered
[    0.452357] io scheduler bfq registered
[    0.459320] EINJ: ACPI disabled.
[    0.546574] mxs-dma 5b810000.dma-apbh: initialized
[    0.547771] Bus freq driver module loaded
[    0.551053] 5a060000.serial: ttyLP0 at MMIO 0x5a060010 (irq = 44, base_baud = 5000000) is a FSL_LPUART
[    1.869087] printk: console [ttyLP0] enabled
[    1.875481] 5a080000.serial: ttyLP2 at MMIO 0x5a080010 (irq = 46, base_baud = 5000000) is a FSL_LPUART
[    1.904006] brd: module loaded
[    1.925709] loop: module loaded
[    1.935157] tun: Universal TUN/TAP device driver, 1.6
[    1.942626] PPP generic driver version 2.4.2
[    1.948036] PPP BSD Compression module registered
[    1.953459] PPP Deflate Compression module registered
[    1.959250] PPP MPPE Compression module registered
[    1.964748] NET: Registered PF_PPPOX protocol family
[    1.970417] PPTP driver version 0.8.5
[    1.975120] usbcore: registered new interface driver asix
[    1.981346] usbcore: registered new interface driver ax88179_178a
[    1.988188] usbcore: registered new interface driver cdc_ether
[    1.994768] usbcore: registered new interface driver cdc_eem
[    2.001170] usbcore: registered new interface driver net1080
[    2.007599] usbcore: registered new interface driver cdc_subset
[    2.014268] usbcore: registered new interface driver zaurus
[    2.020643] usbcore: registered new interface driver cdc_ncm
[    2.027063] usbcore: registered new interface driver qmi_wwan
[    2.039263] usbcore: registered new interface driver cdc_wdm
[    2.045868] usbcore: registered new interface driver usbserial_generic
[    2.053215] usbserial: USB Serial support registered for generic
[    2.059975] usbcore: registered new interface driver option
[    2.066284] usbserial: USB Serial support registered for GSM modem (1-port)
[    2.075878] input: sc-powerkey as /devices/platform/sc-powerkey/input/input0
[    2.084620] usbcore: registered new interface driver xpad
[    2.092197] imx-sc-rtc scu:rtc: registered as rtc0
[    2.097782] imx-sc-rtc scu:rtc: setting system clock to 1970-01-01T00:00:08 UTC (8)
[    2.106363] i2c_dev: i2c /dev entries driver
[    2.119745] amphion-vpu-core 2d040000.vpu-core: [0] = decoder
[    2.129014] amphion-vpu-core 2d050000.vpu-core: [1] = encoder
[    2.138389] __power_supply_register: Expected proper parent device for 'battery'
[    2.147113] __power_supply_register: Expected proper parent device for 'usb'
[    2.157067] trusty trusty: trusty version: Project: imx8qxp, Build: build@pantakill-2, Built: 20:14:21 Aug 24 2022
[    2.168204] trusty trusty: selected api version: 5 (requested 5)
[    2.178521] trusty-log trusty:trusty-log: /dev/trusty-log0 registered
[    2.186471] trusty-log trusty:trusty-log: boot args 0x*** 0x*** 0x*** 0x0
[    2.193975] trusty-log trusty:trusty-log: initializing trusty (Project: imx8qxp, Build: build@pantakill-2, Built: 20:14:21 Aug 24 2022)
[    2.206848] trusty-log trusty:trusty-log: failed to read rpmb write counter
[    2.214511] trusty-log trusty:trusty-log: ss: block_device_tipc_init: bad static rpmb size, 2048
[    2.223997] trusty-log trusty:trusty-log: ss: proxy_connect: block_device_tipc_init failed (-1)
[    2.233679] trusty_ipc virtio0: vring0: va(id)  (____ptrval____)(ffffffc2) qsz 32 notifyid 1
[    2.242876] trusty_ipc virtio0: vring1: va(id)  (____ptrval____)(ffffffc3) qsz 32 notifyid 2
[    2.252744] trusty-virtio trusty:trusty-virtio: initializing done
[    2.253037] trusty_ipc virtio0: is online
[    2.261492] device-mapper: uevent: version 1.0.3
[    2.270195] device-mapper: ioctl: 4.45.0-ioctl (2021-03-22) initialised: dm-devel@redhat.com
[    2.283968] sdhci: Secure Digital Host Controller Interface driver
[    2.290886] sdhci: Copyright(c) Pierre Ossman
[    2.296123] sdhci-pltfm: SDHCI platform and OF driver helper
[    2.304037] ledtrig-cpu: registered to indicate activity on CPUs
[    2.312614] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[    2.319934] hid: raw HID events driver (C) Jiri Kosina
[    2.326324] usbcore: registered new interface driver usbhid
[    2.332622] usbhid: USB HID core driver
[    2.339788] ashmem: initialized
[    2.342893] mmc0: SDHCI controller on 5b010000.mmc [5b010000.mmc] using ADMA
[    2.345816] cs_system_cfg: CoreSight Configuration manager initialised
[    2.365129] Galcore version 6.4.3.p4.398061
[    2.380948] [drm] Initialized vivante 1.0.0 20170808 for 80000000.imx8_gpu0_ss on minor 0
[    2.426766] netem: version 1.3
[    2.430579] u32 classifier
[    2.433992] input device check on
[    2.438295] mmc0: new HS400 Enhanced strobe MMC card at address 0001
[    2.438360] Actions configured
[    2.446738] mmcblk0: mmc0:0001 S0J57X 29.6 GiB
[    2.451350] xt_time: kernel timezone is -0000
[    2.458990] Alternate GPT is invalid, using primary GPT.
[    2.460107] gre: GRE over IPv4 demultiplexor driver
[    2.465982] mmcblk0: p1 p2 p3 p4 p5 p6 p7 p8 p9 p10 p11 p12 p13 p14 p15 p16 p17 p18 p19 p20 p21
[    2.471487] IPv4 over IPsec tunneling driver
[    2.485569] mmcblk0boot0: mmc0:0001 S0J57X 31.5 MiB
[    2.486885] Initializing XFRM netlink socket
[    2.494120] mmcblk0boot1: mmc0:0001 S0J57X 31.5 MiB
[    2.496679] IPsec XFRM device driver
[    2.504374] mmcblk0rpmb: mmc0:0001 S0J57X 4.00 MiB, chardev (234:0)
[    2.507579] NET: Registered PF_INET6 protocol family
[    2.521503] Segment Routing with IPv6
[    2.525960] In-situ OAM (IOAM) with IPv6
[    2.530844] mip6: Mobile IPv6
[    2.536043] ip6_gre: GRE over IPv6 tunneling driver
[    2.542323] NET: Registered PF_PACKET protocol family
[    2.548158] NET: Registered PF_KEY protocol family
[    2.553980] l2tp_core: L2TP core driver, V2.0
[    2.559068] l2tp_ppp: PPPoL2TP kernel driver, V2.0
[    2.567417] registered taskstats version 1
[    2.572356] Loading compiled-in X.509 certificates
[    2.578769] kworker/u8:1 (148) used greatest stack depth: 13584 bytes left
[    2.582849] Loaded X.509 cert 'Build time autogenerated kernel key: 218a8bb39e5cfc671adfa953ff6ea5fc5bb600b5'
[    2.597368] page_owner is disabled
[    2.601826] Key type ._fscrypt registered
[    2.606549] Key type .fscrypt registered
[    2.611182] Key type fscrypt-provisioning registered
[    2.651102] mxs_phy 5b100000.usbphy: supply phy-3p0 not found, using dummy regulator
[    2.686055] pps pps0: new PPS source ptp0
[    2.698493] fec 5b040000.ethernet eth0: registered PHC device 0
[    2.709767] imx-rproc imx8x_cm4@0: mbox_request_channel_byname() could not locate channel named "txdb"
[    2.719831] imx-rproc imx8x_cm4@0: No txdb, ret -22
[    2.726056] remoteproc remoteproc0: imx-rproc is available
[    2.732345] remoteproc remoteproc0: attaching to imx-rproc
[    2.738884] remoteproc0#vdev0buffer: assigned reserved memory node vdevbuffer
[    2.747764] virtio_rpmsg_bus virtio1: rpmsg host is online
[    2.749465] virtio_rpmsg_bus virtio1: creating channel rpmsg-vehicle-channel addr 0x1
[    2.754005] remoteproc0#vdev0buffer: registered virtio1 (type 7)
[    2.762638] virtio_rpmsg_bus virtio1: creating channel rpmsg-i2c-channel addr 0x2
[    2.769394] remoteproc0#vdev1buffer: assigned reserved memory node vdevbuffer
[    2.777659] i2c-rpmsg virtio1.rpmsg-i2c-channel.-1.2: new channel: 0x400 -> 0x2!
[    2.793564] virtio_rpmsg_bus virtio2: rpmsg host is online
[    2.799793] remoteproc0#vdev1buffer: registered virtio2 (type 7)
[    2.806622] remoteproc remoteproc0: remote processor imx-rproc is now attached
[    2.816810] remoteproc remoteproc1: imx-dsp-rproc is available
[    2.827250] debugfs: File 'Playback' in directory 'dapm' already present!
[    2.834918] debugfs: File 'Capture' in directory 'dapm' already present!
[    2.846212] i2c 1-0050: Fixing up cyclic dependency with 5b130000.usb
[    2.855152] imx_rpmsg_i2c bus@5a000000:i2c-rpbus-1: add I2C adapter i2c-rpmsg-adapter successfully
[    2.869511] imx_rpmsg_i2c bus@5a000000:i2c-rpbus-5: add I2C adapter i2c-rpmsg-adapter successfully
[    2.880509] pca953x 15-001a: supply vcc not found, using dummy regulator
[    2.888174] pca953x 15-001a: using no AI
[    2.893810] pca953x 15-001d: supply vcc not found, using dummy regulator
[    2.901420] pca953x 15-001d: using no AI
[    2.906617] imx_rpmsg_i2c bus@5a000000:i2c-rpbus-15: add I2C adapter i2c-rpmsg-adapter successfully
[    2.918253] imx6q-pcie 5f010000.pcie: supply epdev_on not found, using dummy regulator
[    2.927516] imx6q-pcie 5f010000.pcie: No cache used with register defaults set!
[    2.963846] imx6q-pcie 5f010000.pcie: PCIe PLL is locked.
[    2.970063] imx6q-pcie 5f010000.pcie: iATU unroll: disabled
[    2.976362] imx6q-pcie 5f010000.pcie: Detected iATU regions: 6 outbound, 6 inbound
[    2.984673] imx6q-pcie 5f010000.pcie: host bridge /bus@5f000000/pcie@0x5f010000 ranges:
[    2.993520] imx6q-pcie 5f010000.pcie:       IO 0x007ff80000..0x007ff8ffff -> 0x0000000000
[    3.002548] imx6q-pcie 5f010000.pcie:      MEM 0x0070000000..0x007fefffff -> 0x0070000000
[    3.011571] imx6q-pcie 5f010000.pcie: iATU unroll: disabled
[    3.017876] imx6q-pcie 5f010000.pcie: Detected iATU regions: 6 outbound, 6 inbound
[    3.126233] imx6q-pcie 5f010000.pcie: Link up
[    3.131363] imx6q-pcie 5f010000.pcie: Link up
[    3.136450] imx6q-pcie 5f010000.pcie: Link up, Gen1
[    3.143993] cs42xx8 5-0048: failed to get device ID, ret = -1
[    3.150948] cs42xx8: probe of 5-0048 failed with error -1
[    3.159520] 5a070000.serial: ttyLP1 at MMIO 0x5a070010 (irq = 45, base_baud = 5000000) is a FSL_LPUART
[    3.174202] imx_mu 31580000.mu: deferred probe timeout, ignoring dependency
[    3.181929] imx_mu: probe of 31580000.mu failed with error -110
[    3.189107] imx8qxp-lpcg-clk 37620000.clock-controller: deferred probe timeout, ignoring dependency
[    3.198870] imx8qxp-lpcg-clk: probe of 37620000.clock-controller failed with error -110
[    3.208007] imx8qxp-lpcg-clk 5a4d0000.clock-controller: deferred probe timeout, ignoring dependency
[    3.217781] imx8qxp-lpcg-clk: probe of 5a4d0000.clock-controller failed with error -110
[    3.226887] imx8qxp-lpcg-clk 5ac90000.clock-controller: deferred probe timeout, ignoring dependency
[    3.236654] imx8qxp-lpcg-clk: probe of 5ac90000.clock-controller failed with error -110
[    3.247876] imx6q-pcie 5f010000.pcie: Link up
[    3.248100] debugfs: Directory 'lvds1' with parent 'pm_genpd' already present!
[    3.253246] imx6q-pcie 5f010000.pcie: PCI host bridge to bus 0000:00
[    3.261255] debugfs: Directory 'mipi1-i2c1' with parent 'pm_genpd' already present!
[    3.267976] pci_bus 0000:00: root bus resource [bus 00-ff]
[    3.276338] debugfs: Directory 'mipi1-i2c0' with parent 'pm_genpd' already present!
[    3.282527] pci_bus 0000:00: root bus resource [io  0x0000-0xffff]
[    3.290886] debugfs: Directory 'mipi1-pwm0' with parent 'pm_genpd' already present!
[    3.297765] pci_bus 0000:00: root bus resource [mem 0x70000000-0x7fefffff]
[    3.306164] debugfs: Directory 'mipi1' with parent 'pm_genpd' already present!
[    3.313739] pci 0000:00:00.0: [1957:0000] type 01 class 0x060400
[    3.328372] pci 0000:00:00.0: reg 0x10: [mem 0x00000000-0x00ffffff]
[    3.335416] pci 0000:00:00.0: reg 0x38: [mem 0x00000000-0x00ffffff pref]
[    3.335456] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[    3.342912] pci 0000:00:00.0: supports D1 D2
[    3.354020] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[    3.356330] pci 0000:00:00.0: PME# supported from D0 D1 D2 D3hot
[    3.363778] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2
[    3.376680] pci 0000:01:00.0: [1b4b:2b42] type 00 class 0x020000
[    3.379640] platform regulatory.0: Falling back to sysfs fallback for: regulatory.db
[    3.386382] pci 0000:01:00.0: reg 0x10: [mem 0x00000000-0x000fffff 64bit pref]
[    3.392307] ALSA device list:
[    3.392315] #0: bt-sco-audio
[    3.392322] #1: wm8960-audio
[    3.392336] TAP version 14
[    3.392339] 1..0
[    3.419864] pci 0000:01:00.0: reg 0x18: [mem 0x00000000-0x000fffff 64bit pref]
[    3.428136] pci 0000:01:00.0: supports D1 D2
[    3.433131] pci 0000:01:00.0: PME# supported from D0 D1 D3hot D3cold
[    3.440315] pci 0000:01:00.0: 2.000 Gb/s available PCIe bandwidth, limited by 2.5 GT/s PCIe x1 link at 0000:00:00.0 (capable of 4.000 Gb/s with 5.0 GT/s PCIe x1 link)
[    3.473289] pci 0000:00:00.0: BAR 0: assigned [mem 0x70000000-0x70ffffff]
[    3.480843] pci 0000:00:00.0: BAR 6: assigned [mem 0x71000000-0x71ffffff pref]
[    3.488790] pci 0000:00:00.0: BAR 15: assigned [mem 0x72000000-0x721fffff 64bit pref]
[    3.497345] pci 0000:01:00.0: BAR 0: assigned [mem 0x72000000-0x720fffff 64bit pref]
[    3.505836] pci 0000:01:00.0: BAR 2: assigned [mem 0x72100000-0x721fffff 64bit pref]
[    3.514328] pci 0000:00:00.0: PCI bridge to [bus 01-ff]
[    3.520272] pci 0000:00:00.0:   bridge window [mem 0x72000000-0x721fffff 64bit pref]
[    3.529184] device-mapper: init: attempting early device configuration.
[    3.537156] device-mapper: init: adding target '0 3095928 verity 1 PARTUUID=8952f864-66b7-4e21-acdc-e07f7bd8e3f2 PARTUUID=8952f864-66b7-4e21-acdc-e07f7bd8e3f2 4096 4096 386991 386991 sha256 90e6a2396165fe0c487d63dc185198b7af7db3d299f2ddcb16b8247eb23168b0 7fa6eaf80fd2bfa30901bec87b48415ddd9daffe6256027416c46214cd052d48 10 restart_on_corruption ignore_zero_blocks use_fec_from_device PARTUUID=8952f864-66b7-4e21-acdc-e07f7bd8e3f2 fec_roots 2 fec_blocks 390040 fec_start 390040'
[    3.580018] device-mapper: verity: sha256 using implementation "sha256-ce"
[    3.590371] device-mapper: init: dm-0 is ready
[    3.606453] EXT4-fs (dm-0): mounted filesystem without journal. Opts: (null). Quota mode: none.
[    3.616022] VFS: Mounted root (ext4 filesystem) readonly on device 254:0.
[    3.624305] devtmpfs: mounted
[    3.628654] Freeing unused kernel memory: 1600K
[    3.634300] Run /init as init process
[    3.638674] with arguments:
[    3.638679] /init
[    3.638683] with environment:
[    3.638687] HOME=/
[    3.638691] TERM=linux
[    3.638695] buildvariant=userdebug
[    3.664389] random: init: uninitialized urandom read (40 bytes read)
[    3.821836] random: init: uninitialized urandom read (40 bytes read)
[    3.829525] random: init: uninitialized urandom read (4 bytes read)
[    3.940218] init: init first stage started!
[    3.946310] init: Unable to open /lib/modules, skipping module loading.
[    3.963569] init: Using Android DT directory /proc/device-tree/firmware/android/
[    4.016006] init: [libfs_mgr]superblock s_max_mnt_count:65535,/dev/block/by-name/metadata
[    4.025093] init: [libfs_mgr]Filesystem on /dev/block/by-name/metadata was not cleanly shutdown; state flags: 0x1, incompat feature flags: 0x46
[    4.039416] EXT4-fs (mmcblk0p12): Ignoring removed nomblk_io_submit option
[    4.075311] EXT4-fs (mmcblk0p12): recovery complete
[    4.081638] EXT4-fs (mmcblk0p12): mounted filesystem with ordered data mode. Opts: errors=remount-ro,nomblk_io_submit. Quota mode: none.
[    4.094899] init: [libfs_mgr]check_fs(): mount(/dev/block/by-name/metadata,/metadata,ext4)=0: Success
[    4.108542] init: [libfs_mgr]umount_retry(): unmount(/metadata) succeeded
[    4.116440] init: [libfs_mgr]Running /system/bin/e2fsck on /dev/block/mmcblk0p12
[    4.126900] logwrapper: Cannot log to file /dev/fscklogs/log
[    4.129554] logwrapper: executing /system/bin/e2fsck failed: No such file or directory
[    4.133756] e2fsck: executing /system/bin/e2fsck failed: No such file or directory
[    4.143634] init (181) used greatest stack depth: 11648 bytes left
[    4.150348] e2fsck: e2fsck terminated by exit(255)\x0a
[    4.169251] EXT4-fs (mmcblk0p12): mounted filesystem with ordered data mode. Opts: discard. Quota mode: none.
[    4.196989] device-mapper: verity: sha256 using implementation "sha256-ce"
[    4.215350] EXT4-fs (dm-1): mounted filesystem without journal. Opts: barrier=1,inode_readahead_blks=8. Quota mode: none.
[    4.229870] device-mapper: verity: sha256 using implementation "sha256-ce"
[    4.247193] EXT4-fs (dm-2): mounted filesystem without journal. Opts: errors=panic. Quota mode: none.
[    4.259948] device-mapper: verity: sha256 using implementation "sha256-ce"
[    4.277773] EXT4-fs (dm-3): mounted filesystem without journal. Opts: barrier=1,inode_readahead_blks=8. Quota mode: none.
[    4.305856] printk: init: 17 output lines suppressed due to ratelimiting
[    4.424827] init: Opening SELinux policy
[    4.446064] init: Loading SELinux policy
[    4.495950] SELinux:  Permission nlmsg_getneigh in class netlink_route_socket not defined in policy.
[    4.505993] SELinux:  Permission bpf in class capability2 not defined in policy.
[    4.514103] SELinux:  Permission checkpoint_restore in class capability2 not defined in policy.
[    4.523549] SELinux:  Permission bpf in class cap2_userns not defined in policy.
[    4.531658] SELinux:  Permission checkpoint_restore in class cap2_userns not defined in policy.
[    4.541269] SELinux:  Class mctp_socket not defined in policy.
[    4.547835] SELinux: the above unknown classes and permissions will be denied
[    4.569253] SELinux:  policy capability network_peer_controls=1
[    4.576004] SELinux:  policy capability open_perms=1
[    4.581686] SELinux:  policy capability extended_socket_class=1
[    4.588318] SELinux:  policy capability always_check_network=0
[    4.594857] SELinux:  policy capability cgroup_seclabel=0
[    4.600972] SELinux:  policy capability nnp_nosuid_transition=1
[    4.607604] SELinux:  policy capability genfs_seclabel_symlinks=0
[    4.614406] SELinux:  policy capability ioctl_skip_cloexec=0
[    4.960007] audit: type=1403 audit(11.360:2): auid=4294967295 ses=4294967295 lsm=selinux res=1
[    4.969400] audit: type=1404 audit(11.360:3): enforcing=1 old_enforcing=0 auid=4294967295 ses=4294967295 enabled=1 old-enabled=1 lsm=selinux res=1
[    5.003753] selinux: SELinux: Loaded file_contexts
[    5.009348] selinux:
[    5.026334] random: init: uninitialized urandom read (40 bytes read)
[    5.059563] random: init: uninitialized urandom read (40 bytes read)
[    5.066988] random: init: uninitialized urandom read (4 bytes read)
[    5.141235] init: init second stage started!
[    5.229568] init: Using Android DT directory /proc/device-tree/firmware/android/
[    5.249022] init: Overriding previous property 'persist.sys.usb.config':'adb' with new value 'none'
[    5.259015] init: Couldn't load property file '/vendor/default.prop': open() failed: No such file or directory: No such file or directory
[    5.280643] init: Couldn't load property file '/odm_dlkm/etc/build.prop': open() failed: No such file or directory: No such file or directory
[    5.300394] init: Setting product property ro.product.brand to 'Android' (from ro.product.product.brand)
[    5.310733] init: Setting product property ro.product.device to 'mek_8q' (from ro.product.product.device)
[    5.321089] init: Setting product property ro.product.manufacturer to 'nxp' (from ro.product.product.manufacturer)
[    5.332210] init: Setting product property ro.product.model to 'MEK-MX8Q' (from ro.product.product.model)
[    5.342546] init: Setting product property ro.product.name to 'mek_8q_car' (from ro.product.product.name)
[    5.742148] linkerconfig (197) used greatest stack depth: 11120 bytes left
[    5.878748] ueventd: ueventd started!
[    5.889637] selinux: SELinux: Loaded file_contexts
[    5.895246] selinux:
[    5.898837] ueventd: Parsing file /system/etc/ueventd.rc...
[    5.908949] ueventd: Added '/vendor/etc/ueventd.rc' to import list
[    5.916159] ueventd: Added '/odm/etc/ueventd.rc' to import list
[    5.924162] ueventd: Parsing file /vendor/etc/ueventd.rc...
[    5.932594] ueventd: /vendor/etc/ueventd.rc: 42: /sys/ lines must have 5 or 6 entries
[    5.941961] ueventd: Parsing file /odm/etc/ueventd.rc...
[    5.948384] ueventd: Unable to read config file '/odm/etc/ueventd.rc': open() failed: No such file or directory
[    6.076983] random: boringssl_self_: uninitialized urandom read (40 bytes read)
[    6.085654] random: boringssl_self_: uninitialized urandom read (4 bytes read)
[    6.093743] random: boringssl_self_: uninitialized urandom read (4 bytes read)
[    6.221607] boringssl_self_ (200) used greatest stack depth: 10976 bytes left
[    6.559346] audit: type=1400 audit(12.956:4): avc:  denied  { sys_admin } for  pid=207 comm="init.insmod.sh" capability=21  scontext=u:r:init-insmod-sh:s0 tcontext=u:r:init-insmod-sh:s0 tclass=capability permissive=0
[    6.709809] mlan: loading out-of-tree module taints kernel.
[    6.722539] mlan: module verification failed: signature and/or required key missing - tainting kernel
[    6.865696] wlan: Loading MWLAN driver
[    6.871027] wlan: Register to Bus Driver...
[    6.876486] wlan_pcie 0000:01:00.0: enabling device (0000 -> 0002)
[    6.883629] Attach moal handle ops, card interface type: 0x204
[    6.893478] PCIE8997: init module param from usr cfg
[    6.899299] card_type: PCIE8997, config block: 0
[    6.904673] cfg80211_wext=0xf
[    6.908378] sta_name=wlan
[    6.911712] uap_name=wlan
[    6.915052] wfd_name=p2p
[    6.918300] max_vir_bss=1
[    6.921658] cal_data_cfg=none
[    6.925367] ps_mode = 1
[    6.928554] auto_ds = 1
[    6.931718] host_mlme=enable
[    6.935354] fw_name=pcieuart8997_combo_v4.bin
[    6.940499] rx_work=1 cpu_num=4
[    6.944455] Attach mlan adapter operations.card_type is 0x204.
[    6.955949] Request firmware: pcieuart8997_combo_v4.bin
[    7.376946] Registered swp emulation handler
[    7.404634] random: logd: uninitialized urandom read (40 bytes read)
[    7.547969] logd.auditd: start
[    7.552087] logd.klogd: 7547976375
[    7.566630] FW download over, size 592732 bytes
[    7.578091] watchdogd: watchdogd started (interval 10, margin 20)!
[    8.048396] pb_decode failed
[    8.052258] this type is not correct!
[    8.068885] send message failed!
[    8.165608] wait_for_keymaster: Waiting for Keymaster device
[    8.279900] WLAN FW is active
[    8.283612] on_time is 8279811875
[    8.314600] fw_cap_info=0x187c7fa3, dev_cap_mask=0xffffffff
[    8.321016] max_p2p_conn = 8, max_sta_conn = 8
[    8.333397] wlan: wlan0 set max_mtu 2000
[    8.344527] wlan: wlan1 set max_mtu 2000
[    8.352584] wlan: p2p0 set max_mtu 2000
[    8.361131] wlan: version = PCIE8997--16.92.21.p55.3-MM5X16344.p3-GPL-(FP92)
[    8.372371] wlan: Register to Bus Driver Done
[    8.377515] wlan: Driver loaded successfully
[    8.386094] insmod (212) used greatest stack depth: 9424 bytes left
[    8.827963] imx8_media_dev: module is from the staging directory, the quality is unknown, you have been warned.
[    9.177845] ServiceManager: Waited one second for android.system.keystore2.IKeystoreService/default (is service started? are binder threads started and available?)
[   10.194271] ServiceManager: Waited one second for android.system.keystore2.IKeystoreService/default (is service started? are binder threads started and available?)
[   10.211172] init: Control message: Could not find 'aidl/android.system.keystore2.IKeystoreService/default' for ctl.interface_start from pid: 221 (/system/bin/servicemanager)
[   10.407836] random: crng init done
[   10.411970] random: 168 urandom warning(s) missed due to ratelimiting
[   10.852249] init: Control message: Could not find 'android.hardware.graphics.composer@2.1::IComposer/default' for ctl.interface_start from pid: 222 (/system/bin/hwservicemanager)
[   11.210552] ServiceManager: Waited one second for android.system.keystore2.IKeystoreService/default (is service started? are binder threads started and available?)
[   11.227459] wait_for_keymaster: Keymaster device ready
[   11.236762] binder: undelivered transaction 227, process died.
[   11.243685] init: Service 'wait_for_keymaster' (pid 262) exited with status 0 waiting took 3.147000 seconds
[   11.254271] init: Sending signal 9 to service 'wait_for_keymaster' (pid 262) process group...
[   11.263889] libprocessgroup: Successfully killed process cgroup uid 0 pid 262 in 0ms
[   11.278329] init: [libfs_mgr]Invalid ext4 superblock on '/dev/block/by-name/userdata'
[   11.287394] init: [libfs_mgr]mount_with_alternatives(): skipping mount due to invalid magic, mountpoint=/data blk_dev=/dev/block/mmcblk0p18 rec[4].fs_type=ext4
[   11.304083] init: Calling: /system/bin/vdc cryptfs mountFstab /dev/block/by-name/userdata /data
[   11.352046] vdc: Waited 0ms for vold
[   11.396652] EXT4-fs (dm-4): Ignoring removed nomblk_io_submit option
[   11.403789] EXT4-fs (dm-4): Using encoding defined by superblock: utf8-12.1.0 with flags 0x0
[   11.505720] EXT4-fs (dm-4): recovery complete
[   11.511584] EXT4-fs (dm-4): mounted filesystem with ordered data mode. Opts: errors=remount-ro,nomblk_io_submit. Quota mode: journalled.
[   11.601534] e2fsck: e2fsck 1.45.4 (23-Sep-2019)
[   11.630155] e2fsck: Pass 1: Checking inodes, blocks, and sizes
[   11.729887] e2fsck: Pass 2: Checking directory structure
[   11.984659] e2fsck: Pass 3: Checking directory connectivity
[   11.991100] e2fsck: Pass 4: Checking reference counts
[   12.026328] e2fsck: Pass 5: Checking group summary information
[   12.144445] e2fsck: /dev/block/dm-4: 5258/298368 files (1.8% non-contiguous), 77498/1192448 blocks
[   12.175283] EXT4-fs (dm-4): Using encoding defined by superblock: utf8-12.1.0 with flags 0x0
[   12.189901] EXT4-fs (dm-4): mounted filesystem with ordered data mode. Opts: noauto_da_alloc,errors=panic. Quota mode: journalled.
[   12.219784] init: Userdata mounted using /vendor/etc/fstab.nxp result : 7
[   12.227542] init: Keyring created with id 328736684 in process 1
[   12.374256] type=1400 audit(18.772:5): avc: denied { sys_admin } for comm="android.hardwar" capability=21 scontext=u:r:hal_power_default:s0 tcontext=u:r:hal_power_default:s0 tclass=capability permissive=0
[   12.393984] type=1400 audit(18.792:6): avc: denied { sys_admin } for comm="android.hardwar" capability=21 scontext=u:r:hal_power_default:s0 tcontext=u:r:hal_power_default:s0 tclass=capability permissive=0
[   12.407507] vdc: Waited 0ms for vold
[   12.443940] fscrypt: AES-256-CTS-CBC using implementation "cts-cbc-aes-ce"
[   12.455889] fscrypt: AES-256-XTS using implementation "xts-aes-ce"
[   12.660464] apexd: This device does not support updatable APEX. Exiting
[   12.667977] apexd: Marking APEXd as activated
[   12.874569] vdc: Waited 0ms for vold
[   13.236479] apexd: This device does not support updatable APEX. Exiting
[   13.243904] apexd: Marking APEXd as ready
[   13.391355] logd: logd reinit
[   13.397661] logd: FrameworkListener: read() failed (Connection reset by peer)
[   13.881245] update_verifier: Started with arg 1: nonencrypted
[   13.892957] update_verifier: Booting slot 0: isSlotMarkedSuccessful=1
[   13.900191] update_verifier: Leaving update_verifier.
[   14.047496] using random self ethernet address
[   14.052824] using random host ethernet address
[   14.062814] using random self ethernet address
[   14.068568] using random host ethernet address
[   14.075956] file system registered
[   14.689866] healthd: batteryCapacityLevelPath not found
[   14.706820] healthd: batteryChargeTimeToFullNowPath. not found
[   14.769669] healthd: batteryFullChargeDesignCapacityUahPath. not found
[   14.841504] healthd: battery none chg=au
[   14.907372] type=1400 audit(21.304:7): avc: denied { integrity } for comm="init" lockdown_reason="debugfs access" scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=lockdown permissive=0
[   14.936225] type=1400 audit(21.312:8): avc: denied { integrity } for comm="init" lockdown_reason="debugfs access" scontext=u:r:init:s0 tcontext=u:r:init:s0 tclass=lockdown permissive=0
[   15.082878] type=1400 audit(21.372:9): avc: denied { read } for comm="android.hardwar" name="u:object_r:boot_status_prop:s0" dev="tmpfs" ino=81 scontext=u:r:hal_audiocontrol_default:s0 tcontext=u:object_r:boot_status_prop:s0 tclass=file permissive=0
[   15.358778] init: Service 'boringssl_self_test_apex32' (pid 410) exited with status 0 waiting took 0.255000 seconds
[   15.381195] init: Sending signal 9 to service 'boringssl_self_test_apex32' (pid 410) process group...
[   15.391921] libprocessgroup: Successfully killed process cgroup uid 0 pid 410 in 0ms
[   15.424099] init: processing action (apexd.status=ready && ro.product.cpu.abilist64=*) from (/system/etc/init/hw/init.rc:96)
[   15.462867] init: starting service 'boringssl_self_test_apex64'...
[   15.471067] amphion-vpu-core 2d040000.vpu-core: decoder firmware version : 1.8.5
[   15.480816] init: SVC_EXEC service 'boringssl_self_test_apex64' pid 425 (uid 0 gid 0+0 context default) started; waiting...
[   15.494574] init: starting service 'bootanim'...
[   15.513629] init: Control message: Processed ctl.start for 'bootanim' from pid: 260 (/system/bin/surfaceflinger)
[   15.524696] amphion-vpu-core 2d050000.vpu-core: encoder firmware version : 1.3.1
[   15.590284] init: Service 'boringssl_self_test_apex64' (pid 425) exited with status 0 waiting took 0.115000 seconds
[   15.601754] init: Sending signal 9 to service 'boringssl_self_test_apex64' (pid 425) process group...
[   17.140031] read descriptors
[   17.145695] read strings
[   18.039318] android_work: sent uevent USB_STATE=CONNECTED
[   18.190776] android_work: sent uevent USB_STATE=CONFIGURED
[   19.265869] logd: logdr: UID=1036 GID=1007 PID=436 b tail=0 logMask=bf pid=0 start=24395968000ns deadline=0ns
[   20.040277] type=1400 audit(26.436:10): avc: denied { read } for comm="android.hardwar" name="u:object_r:boot_status_prop:s0" dev="tmpfs" ino=81 scontext=u:r:hal_audiocontrol_default:s0 tcontext=u:object_r:boot_status_prop:s0 tclass=file permissive=0
[   22.914155] type=1400 audit(29.312:11): avc: denied { read } for comm="main" name="u:object_r:vendor_default_prop:s0" dev="tmpfs" ino=287 scontext=u:r:zygote:s0 tcontext=u:object_r:vendor_default_prop:s0 tclass=file permissive=0
[   25.080613] type=1400 audit(31.480:12): avc: denied { read } for comm="android.hardwar" name="u:object_r:boot_status_prop:s0" dev="tmpfs" ino=81 scontext=u:r:hal_audiocontrol_default:s0 tcontext=u:object_r:boot_status_prop:s0 tclass=file permissive=0
[   26.167684] type=1400 audit(32.564:13): avc: denied { read } for comm="Binder:243_2" name="wakeup8" dev="sysfs" ino=37195 scontext=u:r:system_suspend:s0 tcontext=u:object_r:sysfs:s0 tclass=dir permissive=0
[   30.127331] type=1400 audit(36.524:14): avc: denied { read } for comm="android.hardwar" name="u:object_r:boot_status_prop:s0" dev="tmpfs" ino=81 scontext=u:r:hal_audiocontrol_default:s0 tcontext=u:object_r:boot_status_prop:s0 tclass=file permissive=0
[   31.262541] init: Control message: Processed ctl.start for 'idmap2d' from pid: 522 (system_server)
[   31.372968] healthd: battery none chg=au
[   32.094245] init: processing action (sys.sysctl.extra_free_kbytes=*) from (/system/etc/init/hw/init.rc:1206)
[   34.202757] read descriptors
[   34.206877] read strings
[   34.220123] read descriptors
[   34.239696] read strings
[   34.317737] type=1400 audit(1675260459.600:15): avc: denied { search } for comm="usb@1.3-service" name="usb" dev="sysfs" ino=28346 scontext=u:r:hal_usb_impl:s0 tcontext=u:object_r:sysfs_batteryinfo:s0 tclass=dir permissive=0
[   35.064912] Qualcomm Atheros AR8031/AR8033 5b040000.ethernet-1:00: attached PHY driver (mii_bus:phy_addr=5b040000.ethernet-1:00, irq=POLL)
[   35.186657] type=1400 audit(1675260460.468:16): avc: denied { read } for comm="android.hardwar" name="u:object_r:boot_status_prop:s0" dev="tmpfs" ino=81 scontext=u:r:hal_audiocontrol_default:s0 tcontext=u:object_r:boot_status_prop:s0 tclass=file permissive=0
[   35.485528] type=1400 audit(1675260460.768:17): avc: denied { read } for comm="main" name="u:object_r:vendor_default_prop:s0" dev="tmpfs" ino=287 scontext=u:r:zygote:s0 tcontext=u:object_r:vendor_default_prop:s0 tclass=file permissive=0
[   35.593465] type=1400 audit(1675260460.872:18): avc: denied { search } for comm="usb@1.3-service" name="usb" dev="sysfs" ino=28346 scontext=u:r:hal_usb_impl:s0 tcontext=u:object_r:sysfs_batteryinfo:s0 tclass=dir permissive=0
[   39.035975] send message failed!
[   39.168126] send message failed!
[   39.173790] receive power state report with value 0
[   39.181533] send message failed!
[   39.286632] receive power state report with value 0
[   39.292303] send message failed!
[   39.357884] send message failed!
[   39.991009] init: processing action (boot.car_service_created=1) from (/system/etc/init/com.android.car.procfsinspector.rc:7)
[   40.008919] init: starting service 'com.android.car.procfsinspector'...
[   40.030451] init: processing action (boot.car_service_created=1) from (/system/etc/init/init.bootstat.car.rc:6)
[   40.045644] init: starting service 'exec 18 (/system/bin/bootstat -r car_service_created)'...
[   40.055968] send message failed!
[   40.074195] init: SVC_EXEC service 'exec 18 (/system/bin/bootstat -r car_service_created)' pid 993 (uid 1000 gid 1007+0 context default) started; waiting...
[   40.108212] init: Command 'exec - system log -- /system/bin/bootstat -r car_service_created' action=boot.car_service_created=1 (/system/etc/init/init.bootstat.car.rc:7) took 63ms and succeeded
[   40.149892] init: Service 'exec 18 (/system/bin/bootstat -r car_service_created)' (pid 993) exited with status 0 waiting took 0.082000 seconds
[   40.163641] init: Sending signal 9 to service 'exec 18 (/system/bin/bootstat -r car_service_created)' (pid 993) process group...
[   40.178082] libprocessgroup: Successfully killed process cgroup uid 1000 pid 993 in 0ms
[   40.835322] selinux: SELinux: Skipping restorecon on directory(/data/system_ce/0)
[   44.880449] vehicle_rpmsg virtio1.rpmsg-vehicle-channel.-1.1: new channel: 0x401 -> 0x1!
[   44.901081] debugfs: Directory 'img-pdma1' with parent 'pm_genpd' already present!
[   44.920001] debugfs: Directory 'img-pdma2' with parent 'pm_genpd' already present!
[   44.930080] debugfs: Directory 'img-pdma3' with parent 'pm_genpd' already present!
[   44.940126] debugfs: Directory 'img-pdma4' with parent 'pm_genpd' already present!
[   44.952456] debugfs: Directory 'img-pdma5' with parent 'pm_genpd' already present!
[   44.964017] debugfs: Directory 'img-pdma6' with parent 'pm_genpd' already present!
[   44.973439] debugfs: Directory 'img-pdma7' with parent 'pm_genpd' already present!
[   45.062088] init: Command 'setprop persist.device_config.attempted_boot_count 0' action=sys.boot_completed=1 (/system/etc/init/flags_health_check.rc:8) took 153ms and succeeded
[   45.085154] init: Service 'exec 20 (/system/bin/bootstat --record_boot_complete --record_boot_reason --record_time_since_factory_reset -l)' (pid 1305) exited with status 0 oneshot service took 0.180000 seconds in background
[   45.121822] init: Sending signal 9 to service 'exec 20 (/system/bin/bootstat --record_boot_complete --record_boot_reason --record_time_since_factory_reset -l)' (pid 1305) process group...
[   45.161557] libprocessgroup: Successfully killed process cgroup uid 1000 pid 1305 in 0ms
[   45.180625] init: processing action (sys.boot_completed=1) from (/system/etc/init/logd.rc:33)
[   45.203323] init: starting service 'logd-auditctl'...
[   45.226029] imx-lpi2c 56226000.i2c: use pio mode
[   45.235663] init: processing action (sys.boot_completed=1 && sys.wifitracing.started=0) from (/system/etc/init/wifi.rc:28)
[   45.236350] i2c 16-004c: Fixing up cyclic dependency with bus@56220000:ldb@562210e0
[   45.287220] it6263 16-004c: Probe failed. Remote port 'lvds-channel@0' disabled
[   45.312782] i2c i2c-16: LPI2C adapter registered
[   45.353370] imx-lpi2c 56246000.i2c: use pio mode
[   45.366891] i2c 17-004c: Fixing up cyclic dependency with bus@56220000:ldb@562410e0
[   45.379001] it6263 17-004c: Probe failed. Remote port 'lvds-channel@0' disabled
[   45.389417] i2c i2c-17: LPI2C adapter registered
[   45.658482] dpu-core 56180000.dpu: driver probed
[   45.683402] imx-drm display-subsystem: bound imx-drm-dpu-bliteng.2 (ops dpu_bliteng_ops)
[   45.724549] imx-drm display-subsystem: bound imx-dpu-crtc.0 (ops dpu_crtc_ops)
[   45.744411] imx-drm display-subsystem: bound imx-dpu-crtc.1 (ops dpu_crtc_ops)
[   45.775265] imx-drm display-subsystem: bound bus@56220000:ldb@562210e0 (ops imx8qxp_ldb_ops)
[   45.796725] imx8qxp-lpcg-clk 585a0000.clock-controller: deferred probe timeout, ignoring dependency
[   45.808412] imx-drm display-subsystem: bound bus@56220000:ldb@562410e0 (ops imx8qxp_ldb_ops)
[   45.809324] imx8qxp-lpcg-clk: probe of 585a0000.clock-controller failed with error -110
[   45.821241] [drm] Initialized imx-drm 1.0.0 20120507 for display-subsystem on minor 1
[   45.861263] imx-lpi2c 58226000.i2c: use pio mode
[   45.870782] i2c i2c-18: LPI2C adapter registered
[   45.897519] mxc-md bus@58000000:camera: deferring cap_device registration
[   45.902090] init: Command 'mkdir /sys/kernel/debug/tracing/instances/wifi 711' action=sys.boot_completed=1 && sys.wifitracing.started=0 (/system/etc/init/wifi.rc:30) took 646ms and succeeded
[   45.925095] init: Service 'logd-auditctl' (pid 1311) exited with status 0 oneshot service took 0.694000 seconds in background
[   45.926871] isi-capture 58100000.isi:cap_device: deferring 58100000.isi:cap_device device registration
[   45.938619] init: Sending signal 9 to service 'logd-auditctl' (pid 1311) process group...
[   45.957845] isi-m2m 58100000.isi:m2m_device: deferring 58100000.isi:m2m_device device registration
[   45.980009] mxc-isi 58100000.isi: mxc_isi.0 registered successfully
[   45.991130] mxc-md bus@58000000:camera: deferring cap_device registration
[   45.991901] isi-capture 58110000.isi:cap_device: deferring 58110000.isi:cap_device device registration
[   46.004070] isi-m2m 58100000.isi:m2m_device: Register m2m success for ISI.0
[   46.009653] mxc-isi 58110000.isi: mxc_isi.1 registered successfully
[   46.029639] isi-capture 58120000.isi:cap_device: deferring 58120000.isi:cap_device device registration
[   46.032540] mx8-img-md: Registered mxc_isi.0.capture as /dev/video3
[   46.040180] mxc-isi 58120000.isi: mxc_isi.2 registered successfully
[   46.052303] mxc-md bus@58000000:camera: deferring cap_device registration
[   46.057843] isi-capture 58130000.isi:cap_device: deferring 58130000.isi:cap_device device registration
[   46.074163] mxc-isi 58130000.isi: mxc_isi.3 registered successfully
[   46.077265] mx8-img-md: Registered mxc_isi.0.capture as /dev/video3
[   46.082620] platform 58227000.csi: Fixing up cyclic dependency with 18-006a
[   46.102142] mx8-img-md: Registered mxc_isi.1.capture as /dev/video4
[   46.119942] mxc-mipi-csi2 58227000.csi: lanes: 4, name: mxc-mipi-csi2.0
[   46.143857] mxc-jpeg 58400000.jpegdec: decoder device registered as /dev/video6 (81,6)
[   46.144599] mx8-img-md: Registered mxc_isi.2.capture as /dev/video5
[   46.165658] mxc-md bus@58000000:camera: deferring cap_device registration
[   46.173879] mxc-jpeg 58450000.jpegenc: encoder device registered as /dev/video7 (81,7)
[   46.208056] max9286_mipi 18-006a: max9286_read_reg:read reg error: reg=1e
[   46.217998] max9286 is not found, chip id reg 0x1e = 0x(ffffffff)
[   46.245790] mx8-img-md: Registered mxc_isi.0.capture as /dev/video3
[   46.254408] mx8-img-md: Registered mxc_isi.1.capture as /dev/video4
[   46.263941] mx8-img-md: Registered mxc_isi.2.capture as /dev/video5
[   46.277504] mx8-img-md: Registered mxc_isi.3.capture as /dev/video8
[   46.287446] unregister ISI channel: mxc_isi.0
[   46.301893] unregister ISI channel: mxc_isi.1
[   46.319467] unregister ISI channel: mxc_isi.2
[   46.325844] unregister ISI channel: mxc_isi.3
[   46.350208] type=1400 audit(1675260471.632:19): avc: denied { sys_admin } for comm="init.insmod.sh" capability=21 scontext=u:r:init-insmod-sh:s0 tcontext=u:r:init-insmod-sh:s0 tclass=capability permissive=0
[   46.656283] type=1400 audit(1675260471.936:20): avc: denied { sys_admin } for comm="init.insmod.sh" capability=21 scontext=u:r:init-insmod-sh:s0 tcontext=u:r:init-insmod-sh:s0 tclass=capability permissive=0
[   46.768492] type=1400 audit(1675260472.052:21): avc: denied { search } for comm="HWC-Poll-Thread" name="data" dev="dm-4" ino=120961 scontext=u:r:hal_graphics_composer_default:s0 tcontext=u:object_r:system_data_file:s0:c512,c768 tclass=dir permissive=0
[   46.768871] audit: audit_lost=1 audit_rate_limit=5 audit_backlog_limit=64
[   46.799323] audit: rate limit exceeded
[   46.828628] type=1400 audit(1675260472.052:22): avc: denied { search } for comm="HWC-Poll-Thread" name="data" dev="dm-4" ino=120961 scontext=u:r:hal_graphics_composer_default:s0 tcontext=u:object_r:system_data_file:s0:c512,c768 tclass=dir permissive=0
[   46.856411] type=1400 audit(1675260472.052:23): avc: denied { search } for comm="HWC-Poll-Thread" name="data" dev="dm-4" ino=120961 scontext=u:r:hal_graphics_composer_default:s0 tcontext=u:object_r:system_data_file:s0:c512,c768 tclass=dir permissive=0
[   46.881803] type=1400 audit(1675260472.052:24): avc: denied { search } for comm="HWC-Poll-Thread" name="data" dev="dm-4" ino=120961 scontext=u:r:hal_graphics_composer_default:s0 tcontext=u:object_r:system_data_file:s0:c512,c768 tclass=dir permissive=0
[   46.907245] type=1400 audit(1675260472.052:25): avc: denied { search } for comm="HWC-Poll-Thread" name="data" dev="dm-4" ino=120961 scontext=u:r:hal_graphics_composer_default:s0 tcontext=u:object_r:system_data_file:s0:c512,c768 tclass=dir permissive=0
[   46.932643] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[   46.933027] type=1400 audit(1675260472.052:26): avc: denied { search } for comm="HWC-Poll-Thread" name="data" dev="dm-4" ino=120961 scontext=u:r:hal_graphics_composer_default:s0 tcontext=u:object_r:system_data_file:s0:c512,c768 tclass=dir permissive=0
[   46.964486] type=1400 audit(1675260472.052:27): avc: denied { search } for comm="HWC-Poll-Thread" name="data" dev="dm-4" ino=120961 scontext=u:r:hal_graphics_composer_default:s0 tcontext=u:object_r:system_data_file:s0:c512,c768 tclass=dir permissive=0
[   47.197323] ci_hdrc ci_hdrc.0: EHCI Host Controller
[   47.203150] ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 1
[   47.235981] ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00
[   47.248146] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 5.15
[   47.257264] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[   47.276253] usb usb1: Product: EHCI Host Controller
[   47.282061] usb usb1: Manufacturer: Linux 5.15.52-dirty ehci_hcd
[   47.288833] usb usb1: SerialNumber: ci_hdrc.0
[   47.307017] hub 1-0:1.0: USB hub found
[   47.312222] hub 1-0:1.0: 1 port detected
[   47.428558] insmod (1361) used greatest stack depth: 6048 bytes left
[   47.529847] usbcore: registered new interface driver usb-storage
[   51.648300] binder_alloc: 1402: binder_alloc_buf, no vma
[   51.654546] binder: 522:539 transaction failed 29189/-3, size 1332-0 line 3101
[   52.423365] selinux: SELinux: Skipping restorecon on directory(/data/system_ce/10)
[   52.431793] selinux:
[   52.441855] selinux: SELinux: Skipping restorecon on directory(/data/vendor_ce/10)
[   52.450414] selinux:
[   52.460639] selinux: SELinux: Skipping restorecon on directory(/data/misc_ce/10)
[   52.469093] selinux:
[   54.064310] init: DM_DEV_STATUS failed for system: No such device or address
[   54.074094] init: DM_DEV_STATUS failed for system: No such device or address
[   54.083934] init: DM_DEV_STATUS failed for system: No such device or address
[   54.092418] init: DM_DEV_STATUS failed for system: No such device or address
[   59.241888] type=1400 audit(1675260484.524:43): avc: denied { search } for comm="RenderThread" name="data" dev="dm-4" ino=120961 scontext=u:r:platform_app:s0:c522,c768 tcontext=u:object_r:system_data_file:s0:c512,c768 tclass=dir permissive=0
[   59.241998] audit: audit_lost=16 audit_rate_limit=5 audit_backlog_limit=64
[   59.272555] audit: rate limit exceeded
[   59.285479] type=1400 audit(1675260484.524:44): avc: denied { search } for comm="RenderThread" name="data" dev="dm-4" ino=120961 scontext=u:r:platform_app:s0:c522,c768 tcontext=u:object_r:system_data_file:s0:c512,c768 tclass=dir permissive=0
[   59.370096] type=1400 audit(1675260484.524:45): avc: denied { search } for comm="RenderThread" name="data" dev="dm-4" ino=120961 scontext=u:r:platform_app:s0:c522,c768 tcontext=u:object_r:system_data_file:s0:c512,c768 tclass=dir permissive=0
[   59.442623] type=1400 audit(1675260484.524:46): avc: denied { search } for comm="RenderThread" name="data" dev="dm-4" ino=120961 scontext=u:r:platform_app:s0:c522,c768 tcontext=u:object_r:system_data_file:s0:c512,c768 tclass=dir permissive=0
[   59.466738] type=1400 audit(1675260484.524:47): avc: denied { search } for comm="RenderThread" name="data" dev="dm-4" ino=120961 scontext=u:r:platform_app:s0:c522,c768 tcontext=u:object_r:system_data_file:s0:c512,c768 tclass=dir permissive=0
[   62.239976] init: Sending signal 9 to service 'idmap2d' (pid 1362) process group...
[   62.298050] libprocessgroup: Successfully killed process cgroup uid 1000 pid 1362 in 49ms
[   62.309936] init: Control message: Processed ctl.stop for 'idmap2d' from pid: 522 (system_server)
[   62.320417] init: Service 'idmap2d' (pid 1362) received signal 9
[   74.840980] healthd: battery none chg=au
[   85.403634] binder: undelivered transaction 179811, process died.
[  134.841421] healthd: battery none chg=au

Thanks & Regards,

Sandeep

0 项奖励
回复
2 回复数

3,257 次查看
SGPT31
Contributor I

Hi,

Thanks!

Any suggestion on this? Looking forward to hearing from you asap.

Regards,

Sandeep

0 项奖励
回复

501 次查看
ycheng
Contributor III
man, your post gives me eye sore. The dmesg dump is deterring others to help you.

To add some value to this reply: the composer service error is not important as long as it does not spam. The service isn't available at the beginning, but once it's up and the error stops being emitted.

If you need help ASAP, you will need to open a support case instead of asking on a community forum.
0 项奖励
回复