imx7ulp RAM error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx7ulp RAM error

2,054 Views
kayiyeh
Contributor II

Hi there,

I used my imx7ulpevk and replaced the DRAM to a new 4Gb LPDDR3. After changing some code, I can bootup Linux and run "memtester" for DRAM burn in. Then I Run into an error. The error message is kind of lengthy and messy, please refer to the attached file and give some comments for direction of debug.

Regards,

Ka-Yi Yeh

Labels (1)
0 Kudos
Reply
1 Reply

1,980 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ka-Yi

memtester errors description can be found on

Micromat :: Topic: Memory test failing solid bits (1/1) 

ram - What can I do with the output of memtester when it shows bad memory? - Unix & Linux Stack Exch... 

For new memory it is necessary to run ddr test i.MX6/7 DDR Stress Test Tool V3.00 

and update ddr settings found from test in uboot

imximage.cfg\mx7ulp_evk\freescale\board - uboot-imx - i.MX U-Boot 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply