imx7d power up sequence issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx7d power up sequence issue

909 Views
felixhsu
Contributor III

Hi All

Platform: i.MX7D with PF3000

Software: Linux 4.1.15.2.0.0

When power up the VLDO3V3 will have abnormal signal then pull high, why reason will bring abnormal signal?

How to fixed abnormal signal?

Thanks.

i.MX7D EVB

power up nxp evb.jpg

Customer board

power up svh.jpg

Labels (3)
0 Kudos
Reply
1 Reply

746 Views
art
NXP Employee
NXP Employee

There is nothing abnormal here. The small initial voltage on the VLDO3V3 power rail is most likely caused by some current back leakage somewhere in the hardware. It should not affect the hardware functionality.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply