imx7d external clock source voltage range

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx7d external clock source voltage range

1,974件の閲覧回数
felixhsu
Contributor III

Hi All

Could you tell me the imx7d external clock source voltage range is 1.8V or 3.3V or other voltage range?

PS: the external clock means EXT_CLK1 or EXT_CLK2 ...etc.

CCM.png

Thanks.

ラベル(3)
0 件の賞賛
返信
3 返答(返信)

1,784件の閲覧回数
twhsueh
Contributor I

Hi Carlos,

    If "SD1_DATA1(pin D6)" is set to "CCM_EXT_CLK2" and NVCC_SD1 : 3.3V. 

    OSC clock input can not exceed 1.8V too?

    擷取0111.PNG

thanks,

0 件の賞賛
返信

1,784件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi Felix,

When the pad is configured to SD card functionality, it will be tight to 3.3V rail; however, when using the pin as CCM_EXT_CLK, it will be tight to 1.8V rail.

As a final note, all of the CCM CLK pins are outputs (the N/P are differential outputs, and the other are single-ended).

Hope this will be useful for you.

Best regards!

/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,784件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi Felix,

You could refer to section 5.3.2 of the i.MX7D Reference Manual, where it is mentioned oscillator pads should be supplied to 1.8V, and higher voltages must not be applied:

https://www.nxp.com/docs/en/reference-manual/IMX7DRM.pdf

Hope this will be useful for you.

Best regards!

/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信