imx7d external clock source voltage range

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx7d external clock source voltage range

2,017 Views
felixhsu
Contributor III

Hi All

Could you tell me the imx7d external clock source voltage range is 1.8V or 3.3V or other voltage range?

PS: the external clock means EXT_CLK1 or EXT_CLK2 ...etc.

CCM.png

Thanks.

Labels (3)
0 Kudos
Reply
3 Replies

1,827 Views
twhsueh
Contributor I

Hi Carlos,

    If "SD1_DATA1(pin D6)" is set to "CCM_EXT_CLK2" and NVCC_SD1 : 3.3V. 

    OSC clock input can not exceed 1.8V too?

    擷取0111.PNG

thanks,

0 Kudos
Reply

1,827 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Felix,

When the pad is configured to SD card functionality, it will be tight to 3.3V rail; however, when using the pin as CCM_EXT_CLK, it will be tight to 1.8V rail.

As a final note, all of the CCM CLK pins are outputs (the N/P are differential outputs, and the other are single-ended).

Hope this will be useful for you.

Best regards!

/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,827 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Felix,

You could refer to section 5.3.2 of the i.MX7D Reference Manual, where it is mentioned oscillator pads should be supplied to 1.8V, and higher voltages must not be applied:

https://www.nxp.com/docs/en/reference-manual/IMX7DRM.pdf

Hope this will be useful for you.

Best regards!

/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply