imx7S Pinmux Tool Question?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx7S Pinmux Tool Question?

1,300 Views
hazar_mutgan
Contributor I

Hello,


I have noticed that CCM_CLKO2 signal is not available on GPIO_IO3 or SD1_WP pad for  MCIMX7S3EVK08SC device at Pins for iMX Tool V5. Is it only missing from the tool or the device itself doesn't support it?

Thank you in advance,


Regards,


Hazar

Tags (3)
0 Kudos
Reply
1 Reply

1,244 Views
igorpadykov
NXP Employee
NXP Employee

Hi Hazar

yes processor supports it as described in sect.8.1 External Signals

and Pin Multiplexing i.MX7S Reference Manual

http://cache.nxp.com/files/32bit/doc/ref_manual/IMX7SRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply