imx7S Pinmux Tool Question?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx7S Pinmux Tool Question?

1,292件の閲覧回数
hazar_mutgan
Contributor I

Hello,


I have noticed that CCM_CLKO2 signal is not available on GPIO_IO3 or SD1_WP pad for  MCIMX7S3EVK08SC device at Pins for iMX Tool V5. Is it only missing from the tool or the device itself doesn't support it?

Thank you in advance,


Regards,


Hazar

タグ(3)
0 件の賞賛
返信
1 返信

1,236件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Hazar

yes processor supports it as described in sect.8.1 External Signals

and Pin Multiplexing i.MX7S Reference Manual

http://cache.nxp.com/files/32bit/doc/ref_manual/IMX7SRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信