imx7 vs imx8 unexpected difference in performance

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx7 vs imx8 unexpected difference in performance

2,636 Views
mikyago
Contributor I
Good morning,
we're performing a performance test on our 2 platforms, imx7d and imx8 mmini, to investigate an issue we're facing.
The test is based in a basic communication between 2 threads, implemented with the pthread library, and it works as follow:
1) One thread is in waiting with a conditional wait
2) the other thread wakes it up
3) elapsed time computation
4) threads exchange roles
5) cycle restarts
Fact is: we see very different performance with this test between imx7 and imx8 platforms.
To make a deeper analysis, we make these measurements in 3 different conditions:
  • threads on the same core
  • threads on different cores
  • OS decides on its own
The most critical condition, the one in which the 2 platforms perform very differently is when threads are in different cores. We even tried to put 2 cores offline in the imx8 platform, but as it is possible to see below, nothing changes. Can someone help us with this situation? Are we missing something?

Further details:
We tried to use this system settings to get a better system stability for all the tests:
  • scaling_governor: performance
  • dynamic frequency scaling driver: disabled
(i.e. on imx8: echo 0 > /sys/bus/platform/drivers/imx_busfreq/busfreq/enable)
Data

imx7d
uname -r:  4.9.11+gf1a31cc

Forcing threads on different cores
[T1] Average is 10 us;
[T2] Average is 14 us;

Forcing threads on same core
[T1] Average is 10 us;
[T2] Average is 14 us;

OS scheduler decides thread-core affinity
[T1] Average is 11 us;
[T2] Average is 15 us;
imx8mmini (all cores online)
uname -r: 4.14.78-imx_4.14.78_1.0.0_ga_dev+g991fec2

Forcing threads on different cores
[T1] Average is 493 us;
[T2] Average is 458 us;

Forcing threads on same core
[T1] Average is 10 us;
[T2] Average is 10 us;

OS scheduler decides thread-core affinity
[T1] Average is 507 us;
[T2] Average is 448 us;
imx8mmini (only 2 cores online)
uname -r: 4.14.78-imx_4.14.78_1.0.0_ga_dev+g991fec2

Forcing threads on different cores
[T1] Average is 474 us;
[T2] Average is 379 us;

Forcing threads on same core
[T1] Average is 10 us;
[T2] Average is 10 us;

OS scheduler decides thread-core affinity
[T1] Average is 480 us;
[T2] Average is 384 us;
As it is possible to see the difference is sensible. We're available for any further useful test, just let us know.
Any help would be appreciated, thanks!
0 Kudos
Reply
1 Reply

2,360 Views
igorpadykov
NXP Employee
NXP Employee

Hi Miky

nxp provides linux bsps described on below link, which are optimized for

demonstration all processor (as much as possible) capabilities

i.MX Software | NXP 

For specific customer needs may be recommended to proceed with help

of extended support of NXP Professional Services | NXP 

so necessary adjustments were made for improving performance

for specific customer use cases.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply