imx7 mfgtool error Verifying Checksum ...Bad Data CRC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx7 mfgtool error Verifying Checksum ...Bad Data CRC

1,770 Views
delauratfrançoi
Contributor II

Hello

I work with imx7d.

I use mfgtool to update my board. I use the L4.9.11_1.0.0 mfgtool. I tested the timing of the ddr. It is OK.

But I have an error whan the u boot mfgtool verify the fsl-image-mfgtool-initramfs-imx_mfgtools.cpio.gz.u-boot. The error is "Verifying Checksum ...Bad Data CRC".

The size of  fsl-image-mfgtool-initramfs-imx_mfgtools.cpio.gz.u-boot is bigger than 8Moctet.

If I use a old  fsl-image-mfgtool-initramfs-imx_mfgtools.cpio.gz.u-boot with a size smaller than 8Moctet it is ok.

I saw that only 8Moctet was loaded if the size was bigger than 8Moctet

I don't understand.

Can you help me please.

Best regards.

François

0 Kudos
Reply
2 Replies

1,761 Views
igorpadykov
NXP Employee
NXP Employee

Hi François

 

one can try to decrease size of   fsl-image-mfgtool-initramfs-imx_mfgtools.cpio.gz.u-boot

rebuilding it (remove unused drivers from image) using sect. 6.2 Manufacturing Tool Yocto Guide

included in  Documentation

 

Best regards
igor

 

 

0 Kudos
Reply

1,753 Views
delauratfrançoi
Contributor II

Hi

Yes I decreased the size of  fsl-image-mfgtool-initramfs-imx_mfgtools.cpio.gz.u-boot. I remove the package mtd. And there is not mode error crc.

But I would have liked to know why I am limited to a size of 8M.

Best Regards

François

0 Kudos
Reply