Hi,
I have a pico imx7 board, normally cortex M4 debug console is on UART 6 defined in dts as
pinctrl_uart6: uart6grp {
 fsl,pins = <
 MX7D_PAD_EPDC_DATA08__UART6_DCE_RX 0x79
 MX7D_PAD_EPDC_DATA09__UART6_DCE_TX 0x79
 MX7D_PAD_EPDC_DATA10__UART6_DCE_RTS 0x79
 MX7D_PAD_EPDC_DATA11__UART6_DCE_CTS 0x79
 >;
 };
&uart6 {
 pinctrl-names = "default";
 pinctrl-0 = <&pinctrl_uart6>;
 assigned-clocks = <&clks IMX7D_UART6_ROOT_SRC>;
 assigned-clock-parents = <&clks IMX7D_OSC_24M_CLK>;
 fsl,uart-has-rtscts;
 status = "okay";
};
I have change the debug console to UART 2, for this I have disable the LCD so I can use UART 2 function on some of the LCD pads, I have done this by adding to m4 dts the following
&lcdif {
 status = "disabled";
};
In M4 I have include code for initialize UART 2 as debug console instead of UART6
IOMUXC_SW_MUX_CTL_PAD_LCD_CLK = IOMUXC_SW_MUX_CTL_PAD_LCD_CLK_MUX_MODE(4);
 IOMUXC_SW_MUX_CTL_PAD_LCD_ENABLE = IOMUXC_SW_MUX_CTL_PAD_LCD_ENABLE_MUX_MODE(4);
 IOMUXC_SW_MUX_CTL_PAD_LCD_HSYNC = IOMUXC_SW_MUX_CTL_PAD_LCD_HSYNC_MUX_MODE(4);
 IOMUXC_SW_MUX_CTL_PAD_LCD_VSYNC = IOMUXC_SW_MUX_CTL_PAD_LCD_VSYNC_MUX_MODE(4);
IOMUXC_SW_PAD_CTL_PAD_LCD_CLK = IOMUXC_SW_PAD_CTL_PAD_LCD_CLK_PE_MASK |
 IOMUXC_SW_PAD_CTL_PAD_LCD_CLK_PS(3) |
 IOMUXC_SW_PAD_CTL_PAD_LCD_CLK_HYS_MASK |
 IOMUXC_SW_PAD_CTL_PAD_LCD_CLK_DSE(1);
IOMUXC_SW_PAD_CTL_PAD_LCD_ENABLE = IOMUXC_SW_PAD_CTL_PAD_LCD_ENABLE_PE_MASK |
 IOMUXC_SW_PAD_CTL_PAD_LCD_ENABLE_PS(3) |
 IOMUXC_SW_PAD_CTL_PAD_LCD_ENABLE_HYS_MASK |
 IOMUXC_SW_PAD_CTL_PAD_LCD_ENABLE_DSE(1);
IOMUXC_SW_PAD_CTL_PAD_LCD_HSYNC = IOMUXC_SW_PAD_CTL_PAD_LCD_HSYNC_PE_MASK |
 IOMUXC_SW_PAD_CTL_PAD_LCD_HSYNC_PS(3) |
 IOMUXC_SW_PAD_CTL_PAD_LCD_HSYNC_HYS_MASK |
 IOMUXC_SW_PAD_CTL_PAD_LCD_HSYNC_DSE(1);
IOMUXC_SW_PAD_CTL_PAD_LCD_VSYNC = IOMUXC_SW_PAD_CTL_PAD_LCD_VSYNC_PE_MASK |
 IOMUXC_SW_PAD_CTL_PAD_LCD_VSYNC_PS(3) |
 IOMUXC_SW_PAD_CTL_PAD_LCD_VSYNC_HYS_MASK |
 IOMUXC_SW_PAD_CTL_PAD_LCD_VSYNC_DSE(1);
IOMUXC_UART2_RX_DATA_SELECT_INPUT = IOMUXC_UART2_RX_DATA_SELECT_INPUT_DAISY(0); // LCD_HSYNC Mode: ALT4 for UART2_RTS_B
It works, but there is a moment during boot that the output become undefined and start printing garbage until M4 is loaded in memory and init the uart port, after that everything works, for example
wwwwwwwwwwwwwwwwwwwwwwwwwwwwwwwwwwwwwwwwwwwwwwww�
Hardware initialized UART2
This was not happening with uart6.
How can I fix this in software?
Seems to be the same problem as i.MX7 M4 UART change the speed during linux booting
Hi Igor,
Thanks for the advice,
Unfortunately it didn't work, here is what I did.
I set in u-boot the mmcargs variable as this
mmcargs=setenv bootargs uart_from_osc console=${console},${baudrate} root=${mmcroot}
same result, until the M4 is not loading I got printing garbage forever.
Do I missing something here? The only difference I notice between UART2 and UART6 is that UART6 is always defined , i.e. defined in imx7d.dts file but disable there such as,
| uart6: serial@30a80000 { | |
| compatible = "fsl,imx7d-uart", | |
| "fsl,imx6q-uart", "fsl,imx21-uart"; | |
| reg = <0x30a80000 0x10000>; | |
| interrupts = <GIC_SPI 16 IRQ_TYPE_LEVEL_HIGH>; | |
| clocks = <&clks IMX7D_UART6_ROOT_CLK>, | |
| <&clks IMX7D_UART6_ROOT_CLK>; | |
| clock-names = "ipg", "per"; | |
| dmas = <&sdma 32 4 0>, <&sdma 33 4 0>; | |
| dma-names = "rx", "tx"; | |
| status = "disabled"; | |
| }; | 
Then under pico dts (imx7d-pico.dts) enable it
&uart6 {
 pinctrl-names = "default";
 pinctrl-0 = <&pinctrl_uart6>;
 assigned-clocks = <&clks IMX7D_UART6_ROOT_SRC>;
 assigned-clock-parents = <&clks IMX7D_OSC_24M_CLK>;
 fsl,uart-has-rtscts;
 status = "okay";
};
And the final M4 dts loaded (imx7d-pico_hobbit-m4.dts) disable it.
&uart6 {
 status = "disabled";
};
For my UART2 case similar thing happen but with LCD interface and UART2 never appear in DTS since it will be use by M4 only.
Will appreciate your comments,
Hi Manuel
one can try on nxp i.MX7D Sabre board with Demo Images on
Issues with pico imx7 board can be posted on its vendor forum or meta-fsl-arm mailing list
https://lists.yoctoproject.org/listinfo/meta-freescale
Best regards
igor
Hi Manuel
one can try uart_from_osc kernel boot parameter described
in Table 11. Common kernel boot parameters attached Release Notes.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------