imx7 GPIO pullup on pin used for special function

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx7 GPIO pullup on pin used for special function

1,285件の閲覧回数
eoin_oconnell
Contributor I

 

Hi all,

I am using the following pins for the SIM functionality in my IMX7d.

 

  1. pinctrl_sim1: sim-grp {
  2. fsl,pins = <
  3. MX7D_PAD_EPDC_DATA00__SIM1_PORT2_TRXD 0x30 /* SODIMM 111 5k pullup*/
  4. MX7D_PAD_EPDC_DATA01__SIM1_PORT2_CLK 0x00 /* SODIMM 113*/
  5. MX7D_PAD_EPDC_DATA02__SIM1_PORT2_RST_B 0x00 /* SODIMM 115*/
  6. MX7D_PAD_EPDC_DATA03__SIM1_PORT2_SVEN 0x00 /* SODIMM 117*/
  7. MX7D_PAD_EPDC_DATA04__SIM1_PORT2_PD 0x50 /* SODIMM 119 47k pull up*/
  8. >;
  9. };
 

I would like to know if even though the pin is being used for SIM special function if my 5k pull-up will still be activated? I do not have any option to put a pullup on my PCB, so this is my last resort

ラベル(2)
0 件の賞賛
返信
1 返信

1,280件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Eoin

 

>I would like to know if even though the pin is being used for SIM special

>function if my 5k pull-up will still be activated?

 

yes it is activated.

 

Best regards
igor

0 件の賞賛
返信