[imx6ulstarter] Mfgtools does not work with Digi embedded yocto 3.2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[imx6ulstarter] Mfgtools does not work with Digi embedded yocto 3.2

1,392 Views
Rakesh0815
Contributor I

I have been using Digi embedded yocto 2.6 version and I was able to successfully flash and load the images using Mfgtools.

Default DEY-2.6 firmware images are placed @ https://ftp1.digi.com/support/digiembeddedyocto/2.6/r3/images/ccimx6ulstarter/fb/ 

I have upgraded to Digi embedded yocto 3.2 version and to my surprise device doesn't boot with the default images provided by Digi @ https://ftp1.digi.com/support/digiembeddedyocto/3.2/r1/images/ccimx6ulstarter/fb/ 

Logs of Dey3.2 version:

**********************************************************************************************************************

U-Boot dub-2020.04-r4.2+gb94328749d (Jul 08 2021 - 12:22:48 +0000)

 

CPU:   i.MX6UL rev1.2 528 MHz (running at 396 MHz)

CPU:   Industrial temperature grade (-40C to 105C) at 43C

Reset cause: POR

I2C:   ready

DRAM:  256 MiB

MCA:   HW_VER=1  FW_VER=1.02

PMIC:  PFUZE3000 DEV_ID=0x30 REV_ID=0x11

NAND:  256 MiB

MMC:   FSL_SDHC: 0

In:    serial

Out:   serial

Err:   serial

Model: Digi International ConnectCore 6UL Starter Board.

ConnectCore 6UL SOM variant 0x02: Industrial Ultralite 528MHz, 256MB NAND, 256MB DDR3, -40/+85C, Wireless, Bluetooth

  Board version 2, ID 129

Boot device:  USB

   WARNING: Dummy default MAC in 'ethaddr'

   WARNING: Dummy default MAC in 'eth1addr'

   WARNING: Dummy default MAC in 'wlanaddr'

   WARNING: Dummy default MAC in 'btaddr'

Net:   FEC0 [PRIME]

Fastboot: Normal

Boot from USB for uuu

Run bootcmd_mfg: fastboot 0

Hit any key to stop autoboot:  0

**********************************************************************************************************************

The highlighted text "Boot from USB for uuu", it is looking for uuu utility. It should look for mfgtools with text "Boot from USB for mfgtools".

Could you please let me know if I am missing anything here and help resolve this issue.

Best Regards

Rakesh Kumar

0 Kudos
Reply
3 Replies

1,382 Views
Rakesh0815
Contributor I

Linux kernel based on version 5.4 and customized for ConnectCore DIgi products.

0 Kudos
Reply

1,380 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

When you use the  UUU to download you need to modify the UUU script according to your own board.

0 Kudos
Reply

1,387 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Which version of BSP are you using?

0 Kudos
Reply