imx6ullevl mfg build fsl-image-mfgtool-initramfs

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6ullevl mfg build fsl-image-mfgtool-initramfs

1,243件の閲覧回数
vladimirchernin
Contributor III

hi!

 am trying to build MFG support image for ref. board imx6ullevk

i work with FSL community master branch

I have  next problem with  bitbake fsl-image-mfgtool-initramfs

>>>MACHINE=imx6ullevk DISTRO=fslc-x11 source setup-environment buildtest

and i run next commad

VirtualBox:/work/work/fsl-community-bsp/buildtest$ bitbake fsl-image-mfgtool-initramfs
NOTE: Your conf/bblayers.conf has been automatically updated.
WARNING: Host distribution "linuxmint-18" has not been validated with this version of the build system; you may possibly experience unexpected failures. It is recommended that you use a tested distribution.
Parsing recipes: 100% |########################################################################################################################################################################################################| Time: 0:00:58
Parsing of 1654 .bb files complete (0 cached, 1654 parsed). 2280 targets, 191 skipped, 0 masked, 0 errors.
NOTE: Resolving any missing task queue dependencies
ERROR: Nothing PROVIDES 'virtual/mfgtool-arm-fslc-linux-gnueabi-binutils'. Close matches:
virtual/arm-fslc-linux-gnueabi-binutils
virtual/arm-fslc-linux-gnueabi-libc-initial
virtual/arm-fslc-linux-gnueabi-gcc-initial
ERROR: Required build target 'fsl-image-mfgtool-initramfs' has no buildable providers.
Missing or unbuildable dependency chain was: ['fsl-image-mfgtool-initramfs', 'linux-mfgtool', 'virtual/mfgtool-arm-fslc-linux-gnueabi-binutils']

Summary: There was 1 WARNING message shown.
Summary: There were 2 ERROR messages shown, returning a non-zero exit code

Please help me to find it out?

Thanks

Vladimir

ラベル(3)
0 件の賞賛
返信
2 返答(返信)

847件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Vladimir,

That's mean that you don't have the dependencies you have to install it: BTW you are using a linux distro not supported by yocto in VM, I encourage you to change to a machine with Linux ubuntu.

0 件の賞賛
返信

847件の閲覧回数
vladimirchernin
Contributor III

thanks for the reply!

linuxmint-18  its ubuntu 14 

if run build > bitbake core-image-minimals 

it's successful built  

0 件の賞賛
返信