imx6ul

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6ul

3,322件の閲覧回数
srinu_inaganti
Contributor III

1. How uboot changes to the new partition when kernel fails to start.

2. kernel changes any boot arguments to notify the uboot ? 

ラベル(1)
3 返答(返信)

2,654件の閲覧回数
radhikasomaiya
Senior Contributor II

Hi [email protected] ,

For roll back to another kernel in case of failure/crash of current kernel, you can do below things(just a raw idea):

1) Create two partition scheme both will have zImage and dtb.

2) Change the boot partition from u-boot. (change mmcdev and mmcpart env variables)

3) To automatically detect the kernel failure you can use the bootcount and bootlimit variables in u-boot and implement the mechanism to switch automatically.

For further understanding of the same in detail please refer to the SWUpdate: software update for embedded system — Embedded Software Update Documentation 2019.11 docum... .

Regards,

Radhika Somaiya.

2,654件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Have you download images success to your board? Here you can send us your fail log.

0 件の賞賛
返信

2,654件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Could you tell us which version of BSP are you using?

0 件の賞賛
返信