imx6ul soft reset

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6ul soft reset

2,543 次查看
yangguichuan
Contributor I

Hello, when I applied the software reset function of IMx6UL, I set SRC_SCR register to 1, and found that it must enable the watchdog to work. I want to know the principle of this software reset.Is it to reset the chip directly or stop feeding the dog to reset the watchdog by stopping the internal code running?

0 项奖励
回复
3 回复数

2,538 次查看
jimmychan
NXP TechSupport
NXP TechSupport

SRC_SCR is used to control the resets on the chip. Please read the Reference Manual Chapter 49.7.1 for the meaning of the settings in this register. 

 

Please download the Reference Manual from here:

i.MX 6UltraLite Applications Processor Reference Manual 

https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/i-mx-applications-proces...

0 项奖励
回复

2,530 次查看
yangguichuan
Contributor I

The 21, 17 and 13 bits of SRC_SCR register are all software reset. Is there any difference between them? There are no further details in the manual.

0 项奖励
回复

2,535 次查看
yangguichuan
Contributor I

But if I don't enable the watchdog and just set the 21st bit of the SRC_SCR register alone, it won't reset successfully. Only when the watchdog is enabled and the 21 bit of SRC_SCR register is set, will the reset be successful. Since it is a direct reset chip, may I ask why there is associated with the phenomenon that watchdog can only work?

0 项奖励
回复