imx6ul soft reset

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6ul soft reset

2,476 Views
yangguichuan
Contributor I

Hello, when I applied the software reset function of IMx6UL, I set SRC_SCR register to 1, and found that it must enable the watchdog to work. I want to know the principle of this software reset.Is it to reset the chip directly or stop feeding the dog to reset the watchdog by stopping the internal code running?

0 Kudos
Reply
3 Replies

2,471 Views
jimmychan
NXP TechSupport
NXP TechSupport

SRC_SCR is used to control the resets on the chip. Please read the Reference Manual Chapter 49.7.1 for the meaning of the settings in this register. 

 

Please download the Reference Manual from here:

i.MX 6UltraLite Applications Processor Reference Manual 

https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/i-mx-applications-proces...

0 Kudos
Reply

2,463 Views
yangguichuan
Contributor I

The 21, 17 and 13 bits of SRC_SCR register are all software reset. Is there any difference between them? There are no further details in the manual.

0 Kudos
Reply

2,468 Views
yangguichuan
Contributor I

But if I don't enable the watchdog and just set the 21st bit of the SRC_SCR register alone, it won't reset successfully. Only when the watchdog is enabled and the 21 bit of SRC_SCR register is set, will the reset be successful. Since it is a direct reset chip, may I ask why there is associated with the phenomenon that watchdog can only work?

0 Kudos
Reply