imx6ul qt5 programming compile

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6ul qt5 programming compile

Jump to solution
2,722 Views
fresxc
Contributor I

Hi All

    I want to compile a programming of HelloQt for imx6ul, the compiler is built by yocto. I use the way of https://community.nxp.com/docs/DOC-333580?commentID=40909#comment-40909 . When I compile helloqt program, the error following: 

  /opt/fsl-imx-wayland/4.1.15-2.0.1/sysroots/cortexa7hf-neon-poky-linux-gnueabi/usr/include/qt5/QtCore/qglobal.h:39:21: fatal error: cstddef: no such file or directory.

   How can i fix it?  thanks!

    Best Regards

Labels (3)
0 Kudos
Reply
1 Solution
2,308 Views
joanxie
NXP TechSupport
NXP TechSupport

it seems the G++ issu, pls check if you configure the toolchain correctly or not

View solution in original post

0 Kudos
Reply
2 Replies
2,309 Views
joanxie
NXP TechSupport
NXP TechSupport

it seems the G++ issu, pls check if you configure the toolchain correctly or not

0 Kudos
Reply
2,308 Views
fresxc
Contributor I

It works after I rechecked the configuration, thanks!

0 Kudos
Reply