imx6ul from qspi-flash boot firmware need to use qspi a?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6ul from qspi-flash boot firmware need to use qspi a?

Jump to solution
1,307 Views
shauew
Contributor I

hello,

       I saw the passage from the imx6ul manual (IMX6ULRM.pdf section 8.6.3)

“The QuadSPI Configuration Parameters Table is built in boot image at fixed offset 0x400 from QSPI NOR A1 base address (368 bytes).”

       Does that means qspi-flash boot need qspi a? Could i only use the qspi b ?

Labels (3)
0 Kudos
Reply
1 Solution
1,015 Views
igorpadykov
NXP Employee
NXP Employee

Hi

port a is always available, port b is configurable.

1.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,016 Views
igorpadykov
NXP Employee
NXP Employee

Hi

port a is always available, port b is configurable.

1.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply