imx6ul from qspi-flash boot firmware need to use qspi a?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

imx6ul from qspi-flash boot firmware need to use qspi a?

跳至解决方案
1,282 次查看
shauew
Contributor I

hello,

       I saw the passage from the imx6ul manual (IMX6ULRM.pdf section 8.6.3)

“The QuadSPI Configuration Parameters Table is built in boot image at fixed offset 0x400 from QSPI NOR A1 base address (368 bytes).”

       Does that means qspi-flash boot need qspi a? Could i only use the qspi b ?

标签 (3)
0 项奖励
回复
1 解答
990 次查看
igorpadykov
NXP Employee
NXP Employee

Hi

port a is always available, port b is configurable.

1.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
991 次查看
igorpadykov
NXP Employee
NXP Employee

Hi

port a is always available, port b is configurable.

1.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复