imx6ul from qspi-flash boot firmware need to use qspi a?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6ul from qspi-flash boot firmware need to use qspi a?

ソリューションへジャンプ
1,288件の閲覧回数
shauew
Contributor I

hello,

       I saw the passage from the imx6ul manual (IMX6ULRM.pdf section 8.6.3)

“The QuadSPI Configuration Parameters Table is built in boot image at fixed offset 0x400 from QSPI NOR A1 base address (368 bytes).”

       Does that means qspi-flash boot need qspi a? Could i only use the qspi b ?

ラベル(3)
0 件の賞賛
返信
1 解決策
996件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi

port a is always available, port b is configurable.

1.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
997件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi

port a is always available, port b is configurable.

1.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信