imx6ul ecspi4 w25q32

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6ul ecspi4 w25q32

4,699 次查看
xinjianlu
Contributor II

在imx6ul下设置挂载W25Q32FV(备注支持SPI nor)

设备树配置如下:

&ecspi4 {
 fsl,spi-num-chipselects = <4>;
 cs-gpios = <&gpio2 15 0>;
 pinctrl-names = "default";
 pinctrl-0 = <&pinctrl_ecspi4_1 &pinctrl_ecspi4_cs_1>;
 status = "okay";
 flash: m25p80@0 {
  compatible = "sst,w25q32","spi-nor";
  spi-max-frequency = <30000000>;
  reg = <0>;
 };

};

烧写完启动如下信息

m25p80 spi3.0: unrecognized JEDEC id bytes: 00,  0,  0

应该是 JEDEC ID 没有识别,请问设备树是否配置正确?

ecspi3下挂载的spi nor芯片的空间如何挂载 到mtd下

&ecspi4 {
 fsl,spi-num-chipselects = <4>;
 cs-gpios = <&gpio2 15 0>;
 pinctrl-names = "default";
 pinctrl-0 = <&pinctrl_ecspi4_1 &pinctrl_ecspi4_cs_1>;
 status = "okay";
 flash: m25p80@0 {
  compatible = "sst,w25q32","spi-nor";
  spi-max-frequency = <30000000>;
  reg = <0>;

   partition@6 {
  label = "w25q32";
  reg = <0x20000000 0x800000>;
 };

/*

在原512Mbyte的NAND FLASH下扩8Mbyte的spi nor空间

*/
 };

};

请帮指导!!!!

标签 (2)
0 项奖励
回复
3 回复数

4,260 次查看
igorpadykov
NXP Employee
NXP Employee

Hi

for jedec spi please check documentation linux/Documentation/devicetree/bindings/mtd/jedec,spi-nor.txt

http://git.freescale.com/git/cgit.cgi/imx/linux-imx.git/tree/Documentation/devicetree/bindings/mtd/j... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

4,261 次查看
xinjianlu
Contributor II

这个已看过,也参考这个,请有方面经验的人帮忙一下

0 项奖励
回复

4,260 次查看
igorpadykov
NXP Employee
NXP Employee

you can debug it using sect.3.8 SPI NOR Flash Memory Technology Device (MTD)

attached Linux Manual and AN4553 Using Open Source Debugging Tools for Linux on i.MX Processors
http://www.nxp.com/assets/documents/data/en/application-notes/AN4553.pdf

Best regards
igor

0 项奖励
回复