imx6ul ecspi generating signal cs

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6ul ecspi generating signal cs

1,984 次查看
2669889282
Contributor I

hi:

There is currently a peripheral spi regmap API used for read and write operations,  in ecspi3 bus connection,The cs pin is configured as required cs function which automatically generates a CS signal, not configured GPIO function to generate a CS signal manually .

dts configuration is as follows:
                pinctrl_ecspi3: ecspi3grp {
                        fsl,pins = <
                                MX6UL_PAD_UART2_RTS_B__ECSPI3_MISO        0x100b1  /* MISO*/
                                MX6UL_PAD_UART2_CTS_B__ECSPI3_MOSI        0x100b1  /* MOSI*/
                                MX6UL_PAD_UART2_RX_DATA__ECSPI3_SCLK      0x100b1  /* CLK*/
                                MX6UL_PAD_UART2_TX_DATA__ECSPI3_SS0       0x100b1  /* CS*/
                        >;
                };

However, the automatic generation CS / SS signals are as follows:

pastedImage_1.png

But my spi peripherals required CS / SS signals, as follows

pastedImage_2.png

How do I modify the kernel and dts?
linux kernel version is linux-4.9.88

标签 (2)
标记 (4)
0 项奖励
回复
3 回复数

1,838 次查看
igorpadykov
NXP Employee
NXP Employee

Hi lincheng

one can try below patch :

[v4,1/3] spi: imx: GPIO chip select DT property should not be required - Patchwork 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,838 次查看
2669889282
Contributor I

hi igorpadykov

patch does not solve my problem

SPI requires native chip select lines which automatically generates a CS signal ,instead of using the GPIO  generates  signal CS manually

ths

0 项奖励
回复

1,838 次查看
MicMoba
Contributor V

Hi lincheng,

did you find a solution for your problem? I have the same issue. I need that the CS stays low during a transmission of one command byte and receive three data bytes.

Currently I solved this by using the CS manually as GPIO but this is not very satisfy.

0 项奖励
回复