imx6ul clock stretching

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6ul clock stretching

3,087 Views
bocky
Contributor I

Does imx6ul's i2c bus support clock stretching function?

How to set?

I was affected by clock stretching when communicating with mcp9600.

How can I match it well? 

0 Kudos
Reply
4 Replies

2,939 Views
karangajjar
Senior Contributor II

Hi Yu Bocky,

Referring to the RM of imx6UL:

Screenshot from 2019-08-13 14-48-51.png

You can download the documents related to imx6UL from below link:

i.MX 6UltraLite Applications Processor | Single Arm® Cortex®-A7 @ 696 MHz | NXP 

Regards,

Karan Gajjar

0 Kudos
Reply

2,939 Views
bocky
Contributor I

Thx

0 Kudos
Reply

2,939 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yu

also some additional details can be found on

i2c baudrate 

Best regards
igor

0 Kudos
Reply

2,939 Views
bocky
Contributor I

Thx

0 Kudos
Reply