imx6ul: Uboot initializes LCDIF exceptions

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6ul: Uboot initializes LCDIF exceptions

1,851 Views
244143298
Contributor I

Board:imx6ul  When UBOOT resets LCDIF block, what is the reason for clkgate setting failure

  • When the LCDIF register is normal, the status is c0000000

  • When the LCDIF register is abnormal, the state is 80000000

 

Labels (1)
0 Kudos
Reply
2 Replies

1,702 Views
igorpadykov
NXP Employee
NXP Employee

Hi 我的钱 去玩儿群无

LCD clocks are enabled in CCM_CCGR2 register described in

sect.18.6.25 CCM Clock Gating Register 2 (CCM_CCGR2)

i.MX 6UltraLite Applications Processor Reference Manual

clocks can be enabled in dcd header:

imximage.cfg\mx6ullevk\freescale\board - uboot-imx - i.MX U-Boot 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,702 Views
244143298
Contributor I

Current situation: Why does the CLkgate bit not set 1 when UBOOT resets the LCDIF block device

0 Kudos
Reply