imx6ul LCD min clock

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6ul LCD min clock

5,864 Views
efancier
Contributor I

Hi NXP support,

I am using a MYiR imx6ul core board for my product, it is going to be in production, but still facing an issue, which is I could not change the LCD pixel clock to any number below about 8.9MHZ, Have communicated to  MYiR engineer but couldn't get a correct answer, following is the LCD part in my dts file, the clock driver I got from MYiR's kernel package is also included here, any suggestion or idea what need to check ?

 

Thanks in advance!

&lcdif {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_lcdif_dat_16bits
&pinctrl_lcdif_ctrl
&pinctrl_lcdif_reset>;
display = <&display0>;
status = "okay";

display0: display0 {
bits-per-pixel = <16>;
bus-width = <16>;

display-timings {
native-mode = <&timing0>;
timing0: timing0 {
clock-frequency = <6300000>;
hactive = <240>;
vactive = <320>;
hfront-porch = <4>;
hback-porch = <8>;
hsync-len = <41>;
vback-porch = <4>;
vfront-porch = <2>;
vsync-len = <10>;

hsync-active = <0>;
vsync-active = <0>;
de-active = <1>;
pixelclk-active = <0>;
};

Labels (1)
0 Kudos
Reply
2 Replies

5,841 Views
efancier
Contributor I

Thank you igor, I will try it on my board

0 Kudos
Reply

5,851 Views
igorpadykov
NXP Employee
NXP Employee

Hi cis llc | robin

 

one can look at similar case on

https://community.nxp.com/t5/i-MX-Processors/Changing-eLCDIF-clock-source-on-i-MX6ULL/m-p/984871

 

Best regards
igor

0 Kudos
Reply