imx6solo DDR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6solo DDR

4,907 Views
1182614726
Contributor III

Dear all,

my board is imx6solo, now i'm using DDR_Stress_Tester_V1.0.3 tools to calibrate DDR, but now the tool seems to dead.

please see the attachment for more information.
when i input the DDR frequence for 400 MHz, the tool will be dead.
wo now use two DDR, each DDR is 256MB, the type is
MT41K128M16JT-125:K
can you help me? thank you very much
Labels (1)
0 Kudos
Reply
4 Replies

4,684 Views
igorpadykov
NXP Employee
NXP Employee

Hi qiang

one can try latest revision of tools

i.MX6/7 DDR Stress Test Tool V3.00 

please pay attention to FAQ section, it explains some issues.

Also may be useful to check tutorial below

DRAM Controller Optimization for i.MX Application Processors 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

4,684 Views
1182614726
Contributor III

Hi igorpadykov,

   the problem has been solved, the releason is not  revison, thank you very much

0 Kudos
Reply

4,684 Views
srikittu34
Contributor II

hello [email protected] can you please give me guidance about how to do ddr3 stress test for imx6 solo board..i am new to this field..

thanks and regards

srikirshna

0 Kudos
Reply

4,684 Views
1182614726
Contributor III

you can do this refer to the ddr3 stress tool guidance, do you have the specific question?

0 Kudos
Reply