imx6sl u-boot HWFLOW, has some one updated the serial_imx.c with HWFLOW option?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6sl u-boot HWFLOW, has some one updated the serial_imx.c with HWFLOW option?

817 次查看
RobertCorrellus
Contributor II

I have a systems using a Freewave Radio in Point-to-Point mode for a console connection.  I am working system debug and would like to be able to interrupt u-boot with a keystroke, so I can bypass booting into my application.  However at the application level flow control was added to eliminate an issue I was having transferring files.  With Flow control on  I can no longer break into the  u-boot sequence and change the start-up options, boot to application vs boot to os.

My current u-boot does not support hwflow,  it apperar to be a stubbed out function in the serial_imx.c file.  Has any one added the code to enable handshaking with a u-boot bootarg?

标签 (1)
0 项奖励
回复
0 回复数