Hello
I use imx6sololite's gpio interrupts in our custom board. I meet some probloms as follow:
configuration:
PIN: GPIO2_16 :
temp = 0;
temp = readl(GPIO2_GDIR);
temp &= (~(1 << 16));
writel(temp, GPIO2_GDIR);
temp = 0;
temp = readl(GPIO2_ICR2);
temp |= (1 << 0) | (1 << 1);
writel(temp, GPIO2_ICR2);
temp = readl(GPIO2_IMR);
temp |= (1 << 16);
writel(temp, GPIO2_IMR);
PIN:GPIO3_15
temp = 0;
temp = readl(GPIO3_GDIR);
temp &= (~(1 << 15));
writel(temp, GPIO3_GDIR);
temp = 0;
temp = readl(GPIO3_ICR1);
temp |= (1 << 31) | (1 << 30);
writel(temp, GPIO3_ICR1);
temp = 0;
temp = readl(GPIO3_IMR);
temp |= (1 << 15);
writel(temp, GPIO3_IMR);
GPIO3_15 can enter interrupt funcution,working normal,but GPIO2_16 not working,could you give me some advice...
Thanks........
 
					
				
		
 igorpadykov
		
			igorpadykov
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi wei
please check if this pin is not used in other way (for example by other module
or in uboot), also one can attach jtag and check its register settings.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks for your answer,but i only regeister gpio function and read back,i under uboot read gpio2_16 and gpio3_15
gpio2_16: 020a0004: 00000000
020a0010: 00000003
020a0014: 00010000
gpio3_15:
020a4004: 00000000
020a400c: c0000000
020a4014: 00008000
gpio only regeister interrupt function,but gpio3 working nornal ,gpio2 not working,please help me.......
Thanks