imx6qdl time interval at SCLK.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6qdl time interval at SCLK.

Jump to solution
1,098 Views
dahyunkim
Contributor I

Hello, 

I had a problem in imx6qdl and I have to reduce the interval of the SCLK(spi clock).

Actually, I have to get no interval in spi clock like this.(Yello is SCLK)

pastedImage_1.png

But i.mx6qdl SCLK is like this.

pastedImage_2.png

There is 1us interval time. I use 4.5Mhz spi transfer speed.

I am wondering the way can modify the interval of the spi clock.

Do you know the way control of the spi clock?

Is the interval time related in Clock Controller Module? 

Thank you.

Labels (2)
Tags (2)
0 Kudos
Reply
1 Solution
983 Views
igorpadykov
NXP Employee
NXP Employee

Hi Dahyun

>I am wondering the way can modify the interval of the spi clock.

>Do you know the way control of the spi clock?

interval is caused by processor internal buses delays and can not be changed, sorry.

>Is the interval time related in Clock Controller Module? 

no

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
984 Views
igorpadykov
NXP Employee
NXP Employee

Hi Dahyun

>I am wondering the way can modify the interval of the spi clock.

>Do you know the way control of the spi clock?

interval is caused by processor internal buses delays and can not be changed, sorry.

>Is the interval time related in Clock Controller Module? 

no

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply