Hi!
Having a custom board with IMX6Q I'm trying to bring up NAND сhip (MT29F2G08ABAEA).
I've already compiled a few u-boot versions from different vendors and repositories including Freescale, Boundary and Denx mainline. I have to mention that in all repositories I use nitrogen6x board as reference because it has similar design and very convenient set of files to fill in DDR3 registers. I need to modify DDR settings because DDR3 calibration tools shows different values.
So what I achieved so far:
1) Freescale uboot-imx->imx_v2013.04_3.10.17_1.0.0_ga
boots fine, NAND detected, NAND erase hangs:
U-Boot 2013.04-04989-g6bb0820-dirty (Apr 06 2016 - 09:46:52)
CPU: Freescale i.MX6Q rev1.5 at 792 MHz
CPU: Temperature 37 C, calibration data: 0x5824ec69
Reset cause: POR
Board: Nitrogen6X
I2C: ready
DRAM: 1 GiB
NAND: 256 MiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1
MMC: no card present
MMC init failed
Using default environment
No panel detected: default to HDMI
unsupported panel HDMI
In: serial
Out: serial
Err: serial
Net: Phy not found
using phy at 4
PHY reset timed out
FEC [PRIME]
Warning: failed to set MAC address
Boot from USB for mfgtools
Use default environment for mfgtools
Run bootcmd_mfg: run mfgtool_args;bootm ${loadaddr} ${initrd_addr} ${fdt_addr};
Hit any key to stop autoboot: 0
Wrong Image Format for bootm command
ERROR: can't get kernel image!
U-Boot > nand info
Device 0: nand0, sector size 128 KiB
Page size 2048 b
OOB size 64 b
Erase size 131072 b
U-Boot > nand erase.chip
NAND erase.chip: device 0 whole chip
<<<here nothing happens and the board hangs
2) Denx u-boot mainline, branch v2016.03
git clone https://github.com/u-boot/u-boot
cd u-boot/
git checkout v2016.03 -b tmp
Results: boots fine, NAND detected, NAND erase hangs with lots of DMA errors:
U-Boot 2016.03-dirty (Apr 06 2016 - 10:07:27 +0300)
CPU: Freescale i.MX6Q rev1.5 at 792 MHz
Reset cause: POR
Board: Cruis-V ver.1 (Debug)
I2C: ready
DRAM: 1 GiB
NAND: 256 MiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1
SF: Unsupported flash IDs: manuf 00, jedec 0000, ext_jedec 0000
*** Warning - spi_flash_probe() failed, using default environment
No panel detected: default to HDMI
Display: HDMI (1024x768)
In: serial
Out: serial
Err: serial
Net: Board Net Initialization Failed
No ethernet found.
Hit any key to stop autoboot: 0
=> nand info
Device 0: nand0, sector size 128 KiB
Page size 2048 b
OOB size 64 b
Erase size 131072 b
subpagesize 2048 b
options 0x 200
bbt options 0x 8000
=> nand erase.chip
NAND erase.chip: device 0 whole chip
MXS NAND: DMA read error
MXS NAND: Error sending command
MXS NAND: Error sending command
MXS NAND: DMA read error
MXS NAND: Error sending command
MXS NAND: Error sending command
MXS NAND: DMA read error
Please check the attached patch of my changes to 2016 u-boot. It is based on this patch http://lists.denx.de/pipermail/u-boot/2014-November/194898.html
Somebody please help me to enable NAND support in u-boot!
Original Attachment has been moved to: myboard.patch.zip
Hi Maxim
please look at
NAND FLASH support for i.MX6 U-Boot
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor!
That really helped!
Just to keep it for other users:
git clone https://github.com/u-boot/u-boot
cd u-boot
git checkout v2013.10
make ARCH=arm titanium_config
make ARCH=arm CROSS_COMPILE=/opt/gcc-linaro-arm-linux-gnueabihf-4.7-2013.04-20130415_linux/bin/arm-linux-gnueabihf- -j4