imx6q spidev_test loopback test no RX

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6q spidev_test loopback test no RX

3,494 次查看
jongjyhhsieh
Contributor I

my goal is run a loopback test on the spi device. 

So far, I configured pin map for SPI1 and SPI3 and enabled them on the board-specific file. 

I can see spi1.0 and spi3.0 device node under /dev/. 

I connected the SPI3's MISO to MOSI to run the loopback. 

For the testing application used spidev_test.c which is under kernel document and just modified the device name to spidev3.0.

when I run the test app, below is what I get, 

spi mode: 0
bits per word: 8
max speed: 500000 Hz (500 KHz)

00 00 00 00 00 00
00 00 00 00 00 00
00 00 00 00 00 00
00 00 00 00 00 00
00 00 00 00 00 00
00 00 00 00 00 00
00 00

I am expecting to get the same tx data for rx but I get 0 as above.

Let me know if anythig I have missed.

Thanks in advance, 

标签 (1)
0 项奖励
回复
3 回复数

3,029 次查看
zengyi7761
Contributor I

Hi,

    Have you solved this problem? I meet the same problem now......

0 项奖励
回复

3,029 次查看
pavleb
Contributor I

There was a bug in the pinctrl definitions in the mainline kernel.

Checkout this commit: 5040feb00c624e18c3a41c600883ab848c1f1f53

0 项奖励
回复

3,029 次查看
jimmychan
NXP TechSupport
NXP TechSupport

We have documentation for different version of Linux BSP.

i.MX 6 Series Software and Development Tool|NXP 

for example :            

In the documentation, there is i.MX_Linux_Reference_Manual.pdf

For the ECSPI, please read the Chapter 36. And 36.4 Unit Test for the test details.

0 项奖励
回复