imx6q spdif issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6q spdif issue

5,357 次查看
joubertshe
Contributor I

hi

Now I want to recive hdmi audio input data via spdif interface , and i add the spdif device in device tree and also can see the imx-spdif in alsa devices list in log,  but now we encounter   the issue that we cannot get any data from the interface , I use the command that arecord -D plughw:1,0  test.wav -v , and i have attach the images which contain the log , pls help check thanks 

Joubert

标签 (1)
0 项奖励
回复
2 回复数

5,166 次查看
joubertshe
Contributor I

hi igor

now when I play an music source on PC via spdif to output to imx6q , the spdif card can do record thing but the value of the captured wav file is all 0x00 except the wav head.

the spdif register value is 

00 00140620

04 00000000

08 00000098

0c 001047ec

10 00038012

14 00000000

18 00000000

1c 00100000

20 00280089

24 00c88088

28 00000000

34 00000000

38 00000000

44 00371e9f

50 00020f00

please help check thanks

0 项奖励
回复

5,165 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Joubert

one can try to test using procedures described in sect.7.4.2 S/PDIF Tx Driver, 7.4.3 S/PDIF Rx Driver

attached Linux Manual using Demo Image

https://www.nxp.com/webapp/Download?colCode=L4.9.88_2.0.0_MX6QDLSOLOX&appType=license&location=null&... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复