imx6q secureboot not always bring up

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6q secureboot not always bring up

1,394 次查看
liuhao1
Contributor II

I work on the imx6q,and burn the pulic key to fuse and open the secure boot function

before  I use  "fuse prog 0 6 0x2"

=> hab_status                                                                                               
                                                                                                            
Secure boot disabled                                                                                        
                                                                                                            
HAB Configuration: 0xf0, HAB State: 0x66                                                                    
No HAB Events Found! 

After I use the command on uboot "fuse prog 0 6 0x2"

But it not always bring up sucessfully

When it bring up sucessfully,I enter "hab_status",it show message as following

Secure boot enabled                                                                                         
                                                                                                            
HAB Configuration: 0xcc, HAB State: 0x99                                                                    
No HAB Events Found!

what is the reason about this

0 项奖励
回复
3 回复数

1,275 次查看
igorpadykov
NXP Employee
NXP Employee

Hi y liuhao

one can recheck hardware (clocks and power supplies) using

i.MX6 System Development User’s Guide

https://www.nxp.com/docs/en/user-guide/IMX6DQ6SDLHDG.pdf

and memory

https://community.nxp.com/docs/DOC-105652 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,275 次查看
liuhao1
Contributor II

But I work on the same board and with same uboot

The uboot can bring up sucessfully everytime

But If I use the command fuse prog 0 6 0x2

It only bring up 1 or 2 times in 20

In my mind it may be depend on the boot mode or fuse config

0 项奖励
回复

1,275 次查看
igorpadykov
NXP Employee
NXP Employee

if - "It only bring up 1 or 2 times in 20" - this may be caused

by hardware problems too.

0 项奖励
回复