I have a imx6q-sabresd based board with wayland weston (also another image that uses xwayland). I'm able to start and use weston, but only when using pixman (CPU graphics). When I try to start weston with the default settings (ie with --use-g2d=1) which uses the GL rendering, I get the following error:
[21:29:08.220] Command line: weston ---debug --tty=1 --device=/dev/fb0 --use-g2d=1 --log=/tmp/weston.log
[21:29:08.220] OS: Linux, 6.1.36-custom-machine+gfd5321d928cc, #1 SMP PREEMPT Mon Nov 27 17:22:40 PST 2023, armv7l
[21:29:08.221] Flight recorder: enabled
[21:29:08.221] Using config file '/etc/xdg/weston/weston.ini'
[21:29:08.221] Output repaint window is 7 ms maximum.
[21:29:08.221] Loading module '/usr/lib/libweston-10/fbdev-backend.so'
[21:29:08.227] initializing fbdev backend
[21:29:08.227] warning: the fbdev backend is deprecated, please migrate to the DRM backend
[21:29:08.228] Trying weston_launch launcher...
[21:29:08.228] could not get launcher fd from env
[21:29:08.228] Trying direct launcher...
[21:29:08.236] Loading module '/usr/lib/libweston-10/g2d-renderer.so'
[21:29:08.249] g2d_open fail.
[21:29:08.249] g2d_renderer_create failed.
Upon further investigation, I tried to run the provided imx-g2d-samples starting with just /opt/g2d_samples/g2d_basic_test but I'm always met with the following error:
[ 1] HAL user version: 6.4.11.658245
[ 2] HAL kernel version: 6.4.11.684571
g2d_open: fail with status -24
g2d_open fail.
Since the G2D library is NXP proprietary (source code not provided), we were unable to dig into the error which seems to be coming from the library.
---
Additionally, if I disable g2d, I get an ELG error instead. See below:
[21:36:29.690] Command line: weston ---debug --tty=1 --device=/dev/fb0 --use-g2d=0 --log=/tmp/weston.log
[21:36:29.690] OS: Linux, 6.1.36-custom-machine+gfd5321d928cc, #1 SMP PREEMPT Mon Nov 27 17:22:40 PST 2023, armv7l
[21:36:29.690] Flight recorder: enabled
[21:36:29.690] Using config file '/etc/xdg/weston/weston.ini'
[21:36:29.690] Output repaint window is 7 ms maximum.
[21:36:29.691] Loading module '/usr/lib/libweston-10/fbdev-backend.so'
[21:36:29.697] initializing fbdev backend
[21:36:29.697] warning: the fbdev backend is deprecated, please migrate to the DRM backend
[21:36:29.697] Trying weston_launch launcher...
[21:36:29.697] could not get launcher fd from env
[21:36:29.697] Trying direct launcher...
[21:36:29.697] Loading module '/usr/lib/libweston-10/gl-renderer.so'
[21:36:29.710] EGL client extensions: EGL_EXT_client_extensions
EGL_EXT_platform_base EGL_KHR_platform_wayland
EGL_EXT_platform_wayland EGL_EXT_device_query
[21:36:29.710] warning: either no EGL_EXT_platform_base support or specific platform support; falling back to eglGetDisplay.
[21:36:29.710] failed to initialize display
[21:36:29.710] EGL error state: EGL_NOT_INITIALIZED (0x3001)
[21:36:29.710] gl_renderer_create failed.
[21:36:29.785] BUG: layer_list is not empty after shutdown. Calls to weston_layer_fini() are missing somwhere.
I also see
[ 1] HAL user version: 6.4.11.658245
[ 2] HAL kernel version: 6.4.11.684571
free(): double free detected in tcache 2
In the terminal after running the weston command, but not in the weston log file.
Keep in mind that if I use `--use-pixman`, then weston is able to start and run fine.
---
I have added the `kernel-module-imx-gpu-viv` package to my image, and enabled
`CONFIG_MXC_GPU_VIV=y`
in my defconfig.
I've tried adding many different packages based on reference images (such as
mesa,
imx-gpu-g2d,
imx-gpu-viv,
packagegroup-fsl-tools-gpu,
packagegroup-fsl-gstreamer1.0,
etc)
but I have been unable to get graphics acceleration to work.
Can anyone provide any insight into this issue or what I might be missing?
Please check the GPU setting in dts and kernel driver. You can refer the EVK dts and kernel.
This error more likely relates to driver
As far as I'm aware, I have the necessary DTS entries. I used the imx6q-sabresd.dts as a reference.
I do have the following entries (this is everything that should be related to graphics/display that I have):
#include "imx6q.dtsi"
#include <dt-bindings/clock/imx6qdl-clock.h>
...
...
/ {
mxcfb1: fb@0 {
compatible = "fsl,mxc_sdc_fb";
disp_dev = "ldb";
interface_pix_fmt = "RGB666";
default_bpp = <16>;
int_clk = <0>;
late_init = <0>;
status = "okay";
};
...
...
};
&dcic1 {
dcic_id = <0>;
dcic_mux = "dcic-hdmi";
status = "disabled";
};
&dcic2 {
dcic_id = <1>;
dcic_mux = "dcic-lvds1";
status = "okay";
};
&ldb {
status = "okay";
lvds-channel@0 {
status = "okay";
fsl,data-mapping = "spwg";
fsl,data-width = <18>;
crtc = "ipu2-di0";
primary;
display-timings {
/* default display timings */
native-mode = <&timing1>;
/* display timings */
timing1: ourdisplay {
.....
.....
};
};
};
lvds-channel@1 {
crtc = "ipu2-di1";
status = "disabled";
};
};
&gpc {
fsl,ldo-bypass = <1>;
};
®_arm {
vin-supply = <&sw1a_reg>;
};
®_pu {
vin-supply = <&sw1c_reg>;
};
®_soc {
vin-supply = <&sw1c_reg>;
};
®_vdd1p1 {
vin-supply = <&vgen5_reg>;
};
®_vdd2p5 {
vin-supply = <&vgen5_reg>;
};
&clks {
assigned-clocks = <&clks IMX6QDL_CLK_LDB_DI0_SEL>,
<&clks IMX6QDL_CLK_LDB_DI1_SEL>;
assigned-clock-parents = <&clks IMX6QDL_CLK_PLL2_PFD0_352M>,
<&clks IMX6QDL_CLK_PLL2_PFD0_352M>;
};
...
...
Is there anything that seems to be missing? As far as I can tell, I have everything important.
I had exactly the same problem after I mixed-and-matched yocto layers. For me the problem was a mismatch between the g2d / imx-gpu-viv libs and the "galcore" kernel driver. After I made sure that g2d_basic_test spits out the same version for 'user' and 'kernel' everything worked.
It is a pity that the error messages of these closed source libs are basically worthless for non-nxp employees. Nobody knows what error -24 is supposed to mean - how about a more deccriptive message...
I checked the current settings you shared, there is no obvious error.
Can you share the kernel log when you test g2d?
And check the information under /sys/kernel/debug/gc.
Enabling more debug using `dmesg -n 8`, and then running `/opt/g2d_samples/g2d_basic_test`, I get no new dmesg logs.
Same base error though:
root@product:/# /opt/g2d_samples/g2d_basic_test
---------------- g2d_open/close stress test ----------
[ 1] HAL user version: 6.4.11.658245
[ 2] HAL kernel version: 6.4.11.684571
g2d_open: fail with status -24
g2d_open/close stress test fail.
Under /sys/kernel/debug/gc, I got this info:
root@product:/sys/kernel/debug/gc# ls
clients database64x info poweroff_timeout vidmem64x
clk dump_trigger load version
database idle meminfo vidmem
root@product:/sys/kernel/debug/gc# cat info
gpu : 0
model : 2000
revision : 5108
product : 0
eco : 0
gpu : 16
model : 320
revision : 5007
product : 0
eco : 0
gpu : 20
model : 355
revision : 1215
product : 0
eco : 0
root@product:/sys/kernel/debug/gc# cat meminfo
VIDEO MEMORY:
POOL SYSTEM:
Free : 134199280 B
Used : 18448 B
MinFree : 134199280 B
MaxUsed : 18448 B
Total : 134217728 B
POOL VIRTUAL:
Used : 0 B
MaxUsed : 0 B
root@product:/sys/kernel/debug/gc# cat version
6.4.11.p2.684571 built at daharingwitekio-ubuntu
Platform path: drivers/mxc/gpu-viv/hal/os/linux/kernel/platform/freescale/gc_hal_kernel_platform_imx.c
root@product:/sys/kernel/debug/gc# cat vidmem
root@product:/sys/kernel/debug/gc# cat clients
PID NAME
------------------------
root@product:/sys/kernel/debug/gc# cat database
GPU Idle: 0 ns
root@product:/sys/kernel/debug/gc# cat load
core : 0
load : 0%
One thing I noticed that might be of interest in the kernel boot logs is this:
[ 1.778654] imx-gpc 20dc000.gpc: Failed to create device link (0x180) with 20c8000.anatop:regulator-v
ddpu
[ 1.812171] imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
Are you using custom machine and just import meta-imx from github?
Did you import meta-freescale layer?
Or you are using the Yocto project we release?
Here's the layers I'm using:
${BSPDIR}/sources/poky/meta \
${BSPDIR}/sources/poky/meta-poky \
${BSPDIR}/sources/meta-openembedded/meta-oe \
${BSPDIR}/sources/meta-openembedded/meta-filesystems \
${BSPDIR}/sources/meta-openembedded/meta-multimedia \
${BSPDIR}/sources/meta-openembedded/meta-python \
${BSPDIR}/sources/meta-freescale \
${BSPDIR}/sources/meta-freescale-distro \
${BSPDIR}/sources/meta-arm/meta-arm \
${BSPDIR}/sources/meta-arm/meta-arm-toolchain \
${BSPDIR}/sources/meta-imx/meta-bsp \
${BSPDIR}/sources/meta-my-custom-layer \And this is the NXP manifest I used as my base: https://github.com/nxp-imx/imx-manifest/blob/imx-linux-mickledore/imx-6.1.22-2.0.0.xml
My machine conf is based on `meta-imx/meta-bsp/conf/machine/imx6qsabresd.conf`. I changed to my own dts/defconfig, added firmware, etc. My kernel config is based on the same one they were using.
My distro is based on `meta-freescale-distro/conf/distro/fsl-wayland.conf`. Only real difference here is I'm using busybox/sysvinit as my virtual_runtime/init_manager
You are using L6.1.36 kernel and firmware not L6.1.22.
I think you should can this previous error log about regulator-vddpu, the gpu power domain not work.
pd_pu: power-domain@1 {
reg = <1>;
#power-domain-cells = <0>;
power-supply = <®_pu>;
clocks = <&clks IMX6QDL_CLK_GPU3D_CORE>,
<&clks IMX6QDL_CLK_GPU3D_SHADER>,
<&clks IMX6QDL_CLK_GPU2D_CORE>,
<&clks IMX6QDL_CLK_GPU2D_AXI>,
<&clks IMX6QDL_CLK_OPENVG_AXI>,
<&clks IMX6QDL_CLK_VPU_AXI>;
};
gpu_3d: gpu@130000 {
compatible = "vivante,gc";
reg = <0x00130000 0x4000>;
interrupts = <0 9 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&clks IMX6QDL_CLK_GPU3D_AXI>,
<&clks IMX6QDL_CLK_GPU3D_CORE>,
<&clks IMX6QDL_CLK_GPU3D_SHADER>;
clock-names = "bus", "core", "shader";
power-domains = <&pd_pu>;
#cooling-cells = <2>;
status = "disabled";
};
Could you clarify what you meant by this? I did try enabling gpu_3d and gpu_2d but running the basic G2D test still failed with the same error.
From the error , seems that regulator-vddpu used by GPU has link issue.
imx-gpc 20dc000.gpc: Failed to create device link (0x180) with 20c8000.anatop:regulator-vddpu
Can you also test L5.15.71 BSP?
Update:
This is warning message in L6.1.36, here is my test on imx6qpdlsolox which is similiar withe imx6q.Please re-check your porting steps.
imx6qpdlsolox login: root
root@imx6qpdlsolox:~# cd /opt/g2d_samples/
root@imx6qpdlsolox:/opt/g2d_samples# ./g2d_basic_test
---------------- g2d_open/close stress test ----------
Width 1920, Height 1088
---------------- g2d_alloc stress test ---------------
---------------- test dst YUV feature ----------------
RGBA to YUY2 time 12514us, 79fps, 166Mpixel/s ........
YUY2 to NV12 time 7005us, 142fps, 298Mpixel/s ........
---------------- g2d blit performance ----------------
RGBA->RGBA time 3704us, 269fps, 563Mpixel/s ........
g2d blending time 9338us, 107fps, 223Mpixel/s ........
---------------- g2d clear performance ----------------
g2d clear time 1837us, 544fps, 1137Mpixel/s ........
^C
root@imx6qpdlsolox:/opt/g2d_samples# dmesg | grep imx-gpc
[ 2.366450] imx-gpc 20dc000.gpc: Failed to create device link (0x180) with 20c8000.anatop:regulator-vddpu
root@imx6qpdlsolox:/opt/g2d_samples#