imx6q multiple display issue with same IPU

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6q multiple display issue with same IPU

1,723 次查看
jignesh1
Contributor I

Hello All,

We are using custom board of imx6q(part number MCIMX6Q6AVT10AD) with two display 1. LCD(800x480) primary 2. HDMI(1920x1080@60) secondary. Both LCD working correct and we are using kernel 3.14.28.

We are facing issue that when HDMI output is working and if we restart LCD preview several times then we get following errors continuously on console. This result into that both LCD and HDMI stop working.

imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00080000

imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_5 = 0x00800000

imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00080000

mxc_sdc_fb fb.24: timeout when waiting for flip irq

imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_5 = 0x00800000

imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00080000

imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_5 = 0x00800000

imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00080000

mxc_sdc_fb fb.24: timeout when waiting for flip irq

imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_5 = 0x00800000

Please  help us to resolve above issue.

Thanks,

Jignesh Patel

标签 (2)
0 项奖励
回复
1 回复

1,417 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi jignesh,

Most probable cause for this issue is huge load on the DDR memory bus.  One can adjust this by configuring IPU priorities in IOMUXC_GPR6 or NIC-301 (Chapter 46 Network Interconnect Bus System (NIC-301) i.MX6DL RM) 

or by optimizing custom application. However. these errors mean that IPU/LCD is not configured properly, please look at

below link for various LCD configurations

 

http://boundarydevices.com/configuring-i-mx6-machines-different-screens-nitrogen6x-sabre-lite/

0 项奖励
回复