imx6q fec BUG NAPI

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6q fec BUG NAPI

1,616 次查看
linw
Contributor I

1:power on boot will not cause this issue

2: type reboot in uart console will not cause this issue

3: adb shell reboot,or adb shell# reboot will cause the issue, the log is below

there is no bug on my imx6dl board by the way!!

this this bug about the NAPI feature???

kernel BUG at include/linux/netdevice.h:520!

Unable to handle kernel NULL pointer dereference at virtual address 00000000

pgd = d0614000

[00000000] *pgd=00000000

Internal error: Oops: 805 [#1] PREEMPT SMP

Modules linked in:

CPU: 1    Tainted: G    B   W    (3.0.35 #10)

PC is at __bug+0x1c/0x28

LR is at __bug+0x18/0x28

pc : [<c004efec>]    lr : [<c004efe8>]    psr: 600b0013

sp : d04f1df8  ip : 00000000  fp : 00000001

r10: d04f0000  r9 : d418d380  r8 : 00000000

r7 : d46f4044  r6 : 00000000  r5 : c06a0a8c  r4 : d46f4000

r3 : 00000000  r2 : c0909ebc  r1 : 600b0093  r0 : 00000033

Flags: nZCv  IRQs on  FIQs on  Mode SVC_32  ISA ARM  Segment user

Control: 10c53c7d  Table: 2061404a  DAC: 00000015

PC: 0xc004ef6c:

ef6c  e1a04000 e24dd010 e590003c eb01ca10 e3500000 0594003c 0a00000d e2841034

ef8c  e594002c e891000e e88d000f ea000003 e59d000c eb01ca06 e3500000 0a000006

U-Boot 2009.08-dirty (Oct 10 2015 - 13:55:35)

标记 (3)
0 项奖励
回复
2 回复数

1,445 次查看
igorpadykov
NXP Employee
NXP Employee

Hi lin

seems reboot can not be performed with adb, suggest also

to post it on

Android Community | Android Open Source Project

since there may be restrictions from adb

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,445 次查看
linw
Contributor I

yep, It did seems reboot in adb shell is different from reboot in console shell.

so I just unconfig the NAPI feature to avoid that issue. any good idears?

0 项奖励
回复