imx6q ext4 file system

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6q ext4 file system

ソリューションへジャンプ
3,833件の閲覧回数
yilingxu
Contributor III

Hi, my rootfs is put in SD card, and is not packaged, specifically, there are /bin, /boot, /dev, /user ... in my second partition of SD card. The linux kernel can mount this rootfs and it works well.

Now I want to sign my rootfs, so I want to make the rootfs as an image. Specifically, I want to make the rootfs as imx-imx6qsabresd.ext4, and put imx-imx6qsabresd.ext4 in my second partition of SD card. How can linux kernel work with this type of rootfs?

I am new with rootfs, can anyone give me some suggestions? thanks a lot.

Yiling Xu

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
3,650件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Are you talking about copying the root file system?

Attached is the Linux User's guide. please refer to the 4.3.5. for more details.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
3,651件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Are you talking about copying the root file system?

Attached is the Linux User's guide. please refer to the 4.3.5. for more details.

0 件の賞賛
返信