imx6q eim problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6q eim problem

985件の閲覧回数
xjy198903
Contributor IV

 

The EIM module of imx6q uses a 16-bit address line (AD0~AD15),16-bit data line (DA16~DA31), asynchronous mode, the module is connected to FPGA, no matter it is read or write, the information on the data line is valid, but there is always no valid data on the address line, the module is connected to FPGA, no matter it is read or write, the information on the data line is valid, but there is always no valid data on the address line.

 
タグ(1)
0 件の賞賛
返信
0 返答(返信)