Drive strength of GPIO in IMX8M Plus

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Drive strength of GPIO in IMX8M Plus

1,019件の閲覧回数
dvkhetia
Contributor I

Greetings,
My system has 6, 8:1 Multiplexer, I wish to short the 3 select lines of all 6 Mux together. The 3 select lines of mux are connected to GPIO pins  & then those 3 GPIOs would change states & would result in selection of corresponding channel input from all individual multiplexers. I have seen that drive strength of the GPIO can be increased (x6) by programming a register. I wanted to know that by doing so, will the GPIO be able to drive all mux select lines

 

Regards,
Devang Khetia

0 件の賞賛
返信
1 返信

977件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Please refer :i.MX 8M Plus Applications Processor Datasheet for Industrial Products

The max output current for 3.3V is 12mA and 9.6mA for 1.8V 

Zhiming_Liu_0-1703479389011.png