Hi
We use LPDDR2 on imx6q-dl platform for developing ,but cannot wakeup system using power key and alarm.
When using power key wake up system , it reboot displaying watch dog as follows:
Please give me some suggestion .
Thanks !
request_suspend_state: sleep (0->3) at 46522649338 (1970-01-01 00:02:25.215163671 UTC)
active wake lock PowerManagerService.Display
PM: suspend entry 1970-01-01 00:02:25.228328004 UTC
Freezing user space processes ... (elapsed 0.031 seconds) done.
Freezing remaining freezable tasks ... (elapsed 0.001 seconds) done.
PM: suspend of devices complete after 144.482 msecs
PM: suspend devices took 0.150 seconds
PM: late suspend of devices complete after 0.508 msecs
PM: noirq suspend of devices complete after 0.581 msecs
Disabling non-boot CPUs ...
CPU1: shutdown
U-Boot 2014.04 (Sep 05 2016 - 18:21:07)
CPU: Freescale i.MX6D rev1.5 at 792 MHz
CPU: Temperature 28 C, calibration data: 0x5554c569
Reset cause: WDOG
Board: MX6-Yilian
I2C: ready
DRAM: 2 GiB
 
					
				
		
 igorpadykov
		
			igorpadykov
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		plase check
Schematics (1)
Quick Start Board Design Files (REV 0) 
http://www.nxp.com/products/single-chip-modules/quick-start-board-for-scm-i.mx-6dq:QWKS-SCM-IMX6DQ?f...
Best regards
igor
 
					
				
		
 igorpadykov
		
			igorpadykov
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		there is no IMX6Q reference board with LPDDR2,
so no bsp/git. You can port SCM patches to this kernel.
Best regards
igor
 
					
				
		
 igorpadykov
		
			igorpadykov
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi clsn
please check lpddr2 patches (SCM_Linux_Patch_meta-fsl-scm.tar.gz)
for i.MX6DQ SCM board
SCM-i.MX 6Dual/6Quad Linux Patch not able to bitbake
Quick Start Board for SCM-i.MX 6DQ|NXP
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------