imx6q, communication problems between MIPI-CSI and IPU CSI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6q, communication problems between MIPI-CSI and IPU CSI

2,383件の閲覧回数
yeyuan1
Contributor III

ipucsi.PNG

 

Hello,

     The development board I use is IMX6Q.

     The yellow circle in the figure above is the part where mipi-CSI connects with IPU-CSI.

      Have the following questions:

      When using the MIpi-CSI camera, imX6Q should receive data using the MIpi-CSI interface.Mipi-csi receives the data and passes it to the IPU-CSI module.Ipu-csi working modes include Gated Clock Mode, non-gated Clock Mode, CCIR656 Interlace Mode and CCIR656 Progressive Mode. In this case, which mode should IPU-CSI work in?

 

Thanks

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

2,374件の閲覧回数
Ednnafeners
Contributor I

Help us  Monkey App

0 件の賞賛
返信

2,377件の閲覧回数
yeyuan1
Contributor III

please help me

0 件の賞賛
返信