Hi @VicKrawciw ,
In fact, the .FLM driver which I share with you already works with Segger JLINK debugger, which we have tested previously.
Now, when you download the code to the octal flash, can you boot works normal or not? Just don't use the debugger at first.
You also can use the MCUbootUtility tool download code to the octal flash in serial download mode, whether that method boot works OK or not?
If serial download boot works OK, and the .FLM download also works OK, just debugger can't work, it should still related to your ULINK pro debugger. Don't debug the code with SDRAM at first, just test the led_blinky project.
Best Regards,
kerry